1. Introduction
This page describes how to quickly handle an On/Off Light Device with On/Off Light Switch.
This project generates basic node (Light Device) supporting Router features and End Devices (Light Switch).
It is a good introduction to handle and have a first approach of ST Zigbee mesh solution.
2. Functioning
This example demonstrates STM32WB applications using the ST Zigbee network to connect switch and Light bulb together in different cases.
From a basic example with one switch is connected to one light bulb, it is possible to connect multi-switch at the same light bulb or to connect one switch to multiple light bulbs and all other combinations to test the Zigbee functionalities.
3. Getting started
This project implements a Zigbee mesh supporting Coordinator (ZC), Router (ZR) and End Device (ZED) features. These features are sufficient to set up a first mesh network, see Zigbee network wiki page.
Software and system requirements
For more information, please visit STM32WB Build Zigbee project - stm32mcu
Hardware requirements
P-NUCLEO-WB55[1] is required to set up the demonstration.
For more information, please visit STM32WB Development ecosystem
Log via UART Interface
4. On Off Cluster
In this example, the topology used is a Light bulb used as ZR to relay messages in the Zigbee network and switches as ZED. In addition, the ZR and ZED will use the cluster "On/Off". So, the basis topology uses 1 ZC, 2 ZR and 4 ZED, both ZR bound to 2 ZED each. It is possible to extend devices with the clusters “Level control”, “Color changes”… to add features.
- Client point of view
The client command (switch) sends a message (On/Off/Toggle) to the server (light bulb). The implementation is straightforward and high-level, allowing you to choose the messages delivery method: broadcast, group or unicast. In this example, the message has sent in unicast mode, which requires binding the devices together. This approach enables configuring the reporting process and receiving an acknowledge from server.
- Server point of view
After reception of a command from a client, an appropriate callback function is executed by the server. If attribute modification, the server sends this modification to each client according to the report configuration in the local binding table.
5. Binding and report process
To manage many configurations, attribute reports are used to troubleshoot issues. To do this, each time a client binds to a server, a configuration report is created to notify the client of the attribute modification.
Please find below the Binding process.
In case of multi-client, the report attribute is using to maintain a coherence between each client when the state of light is changed on the server.
Please find below the Report attribute process for two clients:
6. Retry process
To make it more reliable, a “retry” process has created when a Zigbee command form client failed. As explained before, for all applications, all the command are sent in unicast. Once the command is sent, the server responds with an acknowledgement, if this one includes a failure message, the message will resend to the server.
Please find below the retry process and the flow chart inplemented in source code:
These are three possible situations:
- The client doesn’t receive any response from server, indicating a communication issue.
- The client receives an acknowledgement from server, but it implies a failure in processing the command.
- Everything works fine, and the client receives successful acknowledgement from server.
By implementing this mechanism, the number of failed commands has significantly decreased.