This article gives an overview of the OEMiRoT solution integrated in STM32U0.
How to use it, step by step, is described in wiki pages How to start with OEMiRoT on STM32U0.
1. OEMiRoT presentation
1.1. Overview
OEMiRoT stands for OEM immutable (unchangeable) Root of Trust and acts as a first boot stage. OEMiRoT is an example based on the MCUboot open-source software (refer to mcuboot.com) provided with STM32CubeU0. OEMiRoT offers two services:
- The Secure Boot (root of trust service) is an immutable code, which is always executed after a system reset. It checks static protections (Options Bytes), activates runtime protections and then verifies the authenticity and integrity of the user application code before every execution.
- The Secure Firmware Update application is an immutable code that detects new firmware image candidate. It checks its version (version downgrade prevention), authenticity and integrity before installing it after decryption.
1.2. Protection measures and security strategy
Cryptography ensures integrity, authentication, and confidentiality. However, the use of cryptography alone is not enough: a set of measures and system-level strategies are needed for protecting critical operations and sensitive data (such as a secret key), and the execution flow, in order to resist against possible attacks. On STM32U0, the security strategy is based on (see also STM32U0 Reference manual for more description):
- RDP: Read protection level 2 achieves the highest protection level. Read protection level 2 with OEM2 password capability is used to ensure that a JTAG debugger cannot access the device, except to inject the OEM2 password. In RDP level 2, when the OEM2 password is injected on the JTAG port, the RDP level is regressed to level 1. The OEM2 password must first have been provisioned when the RDP level is 0. Refer to RDP for U0 wiki article for more details.
- Boot lock: BOOT_LOCK option byte is set to establish a chain of trust, by forcing the system to boot from the user flash memory in 0x08000000.
- Antitamper protection: the antitamper protection is used to protect sensitive data from physical attacks. The antitamper protection is activated at the start of OEMiRoT_Boot project and remains active during OEMiRoT_Appli execution. In case of tamper detection, sensitive data in backup SRAM are immediately erased, and a reboot is forced. Both external active tamper pins and internal tamper events are used.
- MPU: The MPU is a memory protection mechanism that allows specific access rights to be defined for any memory-mapped resources of the device: flash memory, SRAM, and peripheral registers. The MPU is configured to limit the execution surface to the code section of OEMiRoT_Boot project during its execution then extended to the application code section after verifying its integrity and its authenticity. This protection is dynamically managed at runtime.
- HDP: when the HDP secure hide protection is activated, any accesses to the protected flash memory area (fetch, read, programming, erase) are rejected. All the code and secrets located inside the protected flash memory area are fully hidden. In the OEMiRoT_Boot project example, the system is configured to hide the OEMiRoT_Boot code, the OEMiRoT_Boot personalized data (secrets) and the OEMiRoT_Boot nonvolatile counters area located in flash memory (Refer to the Memory layout for more details on HDP area) just before launching the verified user application.
- WRP: write protection is used to protect OEMiRoT_Boot code from external attacks or even internal modifications such as unwanted writings/erase operations on critical code/data. In the OEMiRoT_Boot project, the system has been configured to make the OEMiRoT_Boot code, the OEMiRoT_Boot personalized data (secrets), and the OEMiRoT_Loader code as immutable data.
Secure software coding techniques such as doubling critical tests, doubling critical actions, random delay, checking parameter values, and flow control mechanism, are implemented to resist to double synchronized fault-injection attacks.
1.3. Cryptography operations
The OEMiRoT_Boot application example is delivered with the following cryptographic scheme:
- ECDSA-P256 asymmetric cryptography for image authentication.
- AES-CTR-128 symmetric cryptography with key ECIES-P256 encrypted for image confidentiality.
- SHA256 cryptography for image integrity check.
All cryptography operations are done in software (no hardware acceleration).
1.4. OEMiRoT activation
The following figure illustrates the secure boot and the secure update process by showing all the steps required to boot the user application code image:
- At reset, boot is forced on OEMiRoT when BOOT_LOCK set to 1.
- OEMiRoT checks if a new user application code and /or data image are stored in the download slot. If any, OEMiRoT decrypts it then controls its integrity, its authenticity and the antirollback version.
- If successful, the image is decrypted and copied in the user application installation slot. The SHA256 calculated to control the integrity (new reference hash) is stored in the Hash Ref region. The version of the new image is stored in the NV counters region for the antirollback verification. Refer to the Memory layout for more details on OEMiRoT flash memory regions.
- OEMiRoT controls the integrity and the authenticity of the user application code and data images from the installation slot. If successful, OEMiRoT executes it. The jump to the user application code is done using a service from bootloader located in the system flash memory. This service activates the HDP (HDP1_ACCDIS different from 0xA3 and HDP1EN different from 0xB4) are set out of the HDP area. See also STM32U0 Reference manual). In case of control failure the local loader is started to provide the capability to download of a new image.
File:Security U0 OEMiRoT boot.png
Note: To avoid any risk of attack, when OEMiRoT jumps into the user application, the MPU is configured to ensure that only the user application code area is allowed to be executed (execution surface controlled via MPU configuration). It is the user application responsibility to reconfigure the MPU to fit with its security needs.
2. Features list
The main features of the OEMiRoT are:
- ECDSA-P256 asymmetric cryptography for image authentication.
- SHA256 cryptography for image integrity check.
- AES-CTR-128 cryptography for image encryption with symmetric key encrypted in ECIES-P256 provided in the image itself. Refer to Image generation for more details.
- Accelerated boot thanks to image SHA256 reference management. Image verification mainly consists of verifying the SHA256 of the image (integrity check) and then verifying the signature of this SHA256 (authentication check). If successful, the SHA256 is stored as reference for next boot. At next boot, the signature verification is skipped if the SHA256 of the image match the reference stored in user flash. This feature brings performance optimization (under the MCUBOOT_USE_HASH_REF compilation switch).
- Anti rollback version check based on image version counters in user flash.
- Configurable slots mode:
- Single primary slot mode, which enables maximizing image size. The downloaded image is in the same memory slot as the installed image. The new downloaded image overwrites the previous installed image.
- Primary and secondary slots mode, which enables safe image programming. The downloaded image and installed image are in different memory slots.
- Image installation resistant to asynchronous power down and reset.
- Data image: an optional data image can be activated/deactivated through MCUBOOT_DATA_IMAGE_NUMBER define.
- Integration of the full entropy TRNG source (RNG hardware peripheral) for random numbers generation (boot seed generation, tamper protection) or random delays.
- Configurable firmware image upgrade strategy, for primary and secondary slots mode:
- Overwrite strategy, for which the image in the secondary slot overwrites the image in the primary slot.
- Swap strategy, for which the image in primary and secondary slots are swapped. After the swap, the new image in the primary slot must be confirmed by the user application, else, at the next boot, the images are swapped back.
- Memory configuration: all slots are located inside internal user flash (primary and secondary slots for code and data images).
- Integration of hardware security peripherals and mechanisms in order to implement a root of trust. RDP, BOOT_LOCK, MPU, WRP, HDP, and TAMPER are combined to achieve the highest security level. When connected on the HW board, external tamper can be activated with OEMIROT_TAMPER_ENABLE define.
- Image generation with STM32TrustedPackageCreator tool delivered within STM32CubeProgrammer.
Features configurability:
Feature | OEMiRoT |
---|---|
Image upgrade strategy |
|
Slots mode |
|
Flash memory configuration |
|
Antitamper |
|
3. Flash memory layout
The STM32CubeU0OEMiRoT relies on flash memory layout defining several regions:
- HASF REF region: region where the SHA256 references are stored (one reference per image).
- NV counters region: region where OEMiRoT_Boot gets nonvolatile information about last installed images (code and data) versions for the anti rollback feature.
- SCRATCH region: region used by OEMiRoT_Boot to store the image data temporarily during the image swap process (not used in overwrite-only mode).
- Integrator personalized data region: region to personalize OEMiRoT secrets (authentication and encryption keys).
- OEMiRoT_Boot code region: region to program the OEMiRoT_Boot code binary that manages the functions "Secure Boot" and "Secure Firmware Update”.
- Application installation (primary) slot region: region to program the image code and data after installation.
- Application download (secondary) slot region: region to program the "new" image code and data, candidate for installation.
- Loader code region: region to program the OEMiRoT_Loader code binary.
The flash memory layout is fixed but can be updated especially when:
- there is no data image,
- the image upgrade strategy is overwrite,
- the local loader is not required.
If the flash memory layout is modified, the MPU regions configuration must be updated taking into account the constraints on Cortex M0+ MPU (refer to ARM documentation for more details):
- region start address is multiple of the region size
- each region can be divided in 8 sub-regions
- a maximum of 8 regions can be defined
Flash memory layout is as follow:
4. Provisioning process
The product provisioning to activate and configure OEMiRoT is done following the four steps below:
- Select the RDP level.
- Build the OEMiRoT_Boot and OEMiRoT_Loader projects.
- Generation of the user application code and data images.
- Programing of the option bytes, the OEMiRoT_Boot binary, the OEMiRoT_Lodaer binary and the application images in the device
Note: A set of scripts is provided in Firmware/Projects/NUCLEO-U083RC/ROT_Provisioning/OEMiRoT folder. It guides the user all along the provisioning process. Refer to How to start with OEMiRoT on STM32U0 article.
5. Images generation
OEMiRoT manages images at MCUBoot format including:
- a header,
- the encrypted firmware binary,
- some metadata information (TLV format: Tags Length Value) allowing the control of the image (SHA256, ECDSA signature, encryption key …), and
- a magic to trigger the installation.
Further information about the MCUBoot open-source software is available at mcuboot.com.
A PC tool STM32TrustedPackageCreator is provided to generate both code and data images. These images are encrypted and signed using the keys configured. OEMiRoT_Code_Image.xml / OEMiRoT_Data_Image.xml contains all the parameters driving the image generation such as:
- The authentication and encryption keys.
- The version.
- The dependency with code or data image if a synchronized installation is required.
OEMiRoT_Code_Image.xml / OEMiRoT_Code_Data.xml can be edited with STM32TrustedPackageCreator in order to modify the version and the dependency parameters.
The following figure shows the code image generation (same applied for data image):
6. Appendix
6.1. OEMiRoT start-up sequence
Performance measured @ xx MHz:
32 KBytes | 64 KBytes | 128 KBytes | |
---|---|---|---|
Boot time | x ms | x ms | x ms |
6.2. Application development phase
During development phase, it is recommended to compile OEMiRoT_Boot project with DEV_MODE defined and to select RDP level0 during provisioning process :
- When DEV_MODE is defined:
- additional logs are displayed in tera term during OEMiRoT_Boot project execution.
- an infinite loop is executed instead of a reset in Error_Handler() function .
- tamper event is cleared at startup when required. No need to power off/on the board to clear this event.
- OPEN product state can be selected during provisioning process.
At the end of the development phase, DEV_MODE must be disabled and the RDP level2 must be selected during provisioning process to achieve the highest security level.
6.3. OEMiRoT_Code_image xml file format
Parameter | Updatable | Description |
---|---|---|
Authentication key | Automatic | Private key inherited from OEMiROT_Config.xml file. |
Write Option | Automatic | Image upgrade strategy: Overwrite, Swap. This value is updated during the postbuild operation based on MCUBOOT_OVERWRITE_ONLY definition from flash_layout.h |
Encryption key | Automatic | Public key inherited from OEMiROT_Config.xml file. |
Endianness | No | Little endian. |
Padding | No | Add an installation magic value at the end of the image to trigger image installation. Padding with 0xFF when required. |
Firmware/Data area size | Automatic | Firmware/Data area size. This value is updated during the postbuild operation based on slot configuration from flash_layout.h. |
Header Size | No | 0x400 bytes |
Padding Header | No | Padding the header with 0xFF to fulfil the 0x400 bytes. |
Dependency with data image | No | This parameter must be enabled when the installation of both data and code images must be synchronized. |
Version | Yes | x.y.z firmware image version. |
Security Counter | No | Security counter value automatically generated based on version information. |
Align | No | 16 bytes alignment |
Firmware binary input file | Automatic | Location of the firmware binary file. This parameter is updated during the provisioning process based on information from env.bat file. |
Image output file | Yes | Location of the encrypted image generated. If changed, provisioning scripts must be updated accordingly. |
Same applied for OEMiRoT_Data_Image.xml
6.4. Troubleshooting
Problem | Possible solution |
---|---|
Provisioning errors in ob_flash_programming.bat script | PC com port is connected to tera term application |
Provisioning errors. No JTAG connection. |
|