STiRoT for STM32H7S

Revision as of 10:07, 20 October 2023 by Registered User

STiRoT stands for ST Immutable (unchangeable) Root of Trust. This is a ROM code developed by STMicroelectronics, which targets a SESIP level 3 certified implementation. Since STiRoT requires hardware cryptographic features, it is only available on STM32H7Sxx product lines.

One of the major specificity of this series is that STM32H7xx integrates only 64 KBytes of user flash. As a consequence, the user applications will be most of the time stored in the external memory selected by the OEM.

A detailed description of STiRoT is provided in AN6034

1. STiRoT services

STiRoT provides two services.

  • The Secure Boot (root of trust services) is an immutable code, which is always executed after a system reset. It activates runtime protections and then, it verifies the authenticity and integrity of the application code before every execution.
  • The Secure Firmware Update application is an immutable code that detects that a new firmware image is available. It checks its authenticity, then checks the integrity of the code before installing it after decryption.

2. STiRoT activation

STiRoT is activated in two different use cases:

  • One boot stage: STiRoT directly manages the user application.

Security STiRoT 1bootstage.png

  • Two boot stages: STiRoT manages an updatable boot stage (OEMuRoT) which manages the user application. The updatable boot stage can be customized to fit customer needs.

Security STiRoT 2bootstages.png

In both cases, STiRoT never access the external flash memory. The control of the authenticity and the integrity as well as the execution of the user application or the OEMuRoT is always done in internal RAM memory. To do this, STiRoT relies on iLoader application to copy the user application or the OEMuRoT from external flash memory to internal RAM memory.

Please refer to AN6034 to get all the details on on the STiRoT activation use cases.

An example of one boot stage configuration is provided through How_to_start_with_STiRoT_on_STM32H7S article.

An example of two boot stages configuration is provided through How_to_start_with_STiRoT_OEMuRoT_on_STM32H7S article.

3. STiRoT configuration

STiROT configuration provides the possibility to:

  • Define the RAM and the external flash memory mapping: select the location and the size of each area.
  • Configure the authentication and encryption keys.
  • Allow the jump in the bootloader (external access) when no valid image is installed.

The product provisioning to activate and configure STiRoT is done following the four steps below:

0.Generation of iLoader binary.
1.Configuration of STiROT. At this stage, the location of the image, and the cryptographic keys are defined.
2.Generation of the code image.
3.Programming of the OBKeys, the option bytes, the iLoader and the image in the device.

Note: A set of scripts is provided in the STM32CubeH7RS MCU package (Firmware/Projects/Board/ ROT_Provisioning/STiROT folder). It guides the user all along the provisioning process.

Security STiRoT privisioning.png

Please refer to AN6034 to get all the details on the STiROT provisioning process including OBkeys configuration files and image generation.