STiRoT stands for ST Immutable (unchangeable) Root of Trust. This is a ROM code developed by STMicroelectronics, which targets a SESIP level 3 certified implementation. Since the STiRoT requires hardware cryptographic features, it is only available on STM32H7Sxx product lines.
A detailed description of STiRoT is provided in ANXXXX.
1. STiRoT services
The STiRoT provides two services.
- The Secure Boot (root of trust services) is an immutable code, which is always executed after a system reset. It activates runtime protections and then, it verifies the authenticity and integrity of the application code before every execution.
- The Secure Firmware Update application is an immutable code that detects that a new firmware image is available. It checks its authenticity, then checks the integrity of the code before installing it after decryption.
2. STiRoT activation
STiRoT is activated in two different use cases:
- One boot stage: The STiRoT integrated inside the STM32H7Sxx directly manages the user application.
- Two boot stages: The STiRoT integrated inside the STM32H7Sxx manages an updatable boot stage (OEMuRoT) which manages the user application. The updatable boot stage can be customized to fit customer needs.
In both cases, STiRoT never access the external flash memory. STiRoT relies on iLoader to copy the user application or the OEMuRoT from external flash memory to internal RAM memory.
Please refer to ANXXXX to get all the details on on the STiRoT activation use cases.
An example of one boot stage configuration is provided through How_to_start_with_STiRoT_on_STM32H7S article.
3. STiRoT configuration
STiROT configuration provides the possibility to:
- Define the RAM and the external flash memory mapping: select the location and the size of each area.
- Configure the authentication and encryption keys.
- Allow the jump in the bootloader (external access) when no valid image is installed. This parameter is hidden by default.
The product provisioning to activate and configure STiRoT is done following the four steps below:
- 0.Generation of iLoader binary.
- 1.Configuration of the STiROT. At this stage, the location of the image, and the cryptographic keys are defined.
- 2.Generation of the code image.
- 3.Programming of the OBKeys, the option bytes, the iLoader and the image in the device.
Note: A set of scripts is provided in the STM32CubeH7RS MCU package (Firmware/Projects/Board/ ROT_Provisioning/STiROT folder). It guides the user all along the provisioning process. Refer to [4] for more information.
Please refer to ANXXXX to get all the details on the STiROT provisioning process including OBkeys configuration files and image generation.