STM32WB Build Zigbee Project

Revision as of 15:13, 17 October 2023 by Registered User (→‎Cube IDE)

1. Presentation

This page describes how to easily build and install a STM Zigbee example application.
Project examples can be found on STM32CubeWB MCU Package[1], and are available for different platforms.

ST Zigbee project example directory
Connectivity zigbee projects.png



2. Requirements

2.1. Software and system requirements

The software requirements are as follows.
The minimum IDE versions:

  • IAR embedded workbench for ARM (EWARM) toolchain V8.20.2
  • RealView microcontroller development kit (MDK-ARM) toolchain V5.31
  • STM32CubeIDE toolchain V1.7.0 [2]

Programmer:

  • STM32CubeProgrammer[3]: to flash the board with an already generated binary

2.2. Hardware requirements

A Nucleo board[4], an STM32WB USB dongle[4], or an STM32WB discovery kit[5] is necessary to install the application.

Platforms illustration
Connectivity hardware-presentation.png


More details about the board and other hardware requirements are available in the Bluetooth® Low Energy SIG and 802.15.4 Nucleo pack user manual[6].

3. Build and install the application

This section describes the build process using IAR and STM32CubeIDE.

3.1. IAR IDE

Select the application that you want to build, open the IAR (EWARM) dedicated directory and launch the project.eww IAR file to open the demonstration project on IDE.

IAR project directory
Connectivity Zigbee IAR.png



Ensure that your project is correctly visible into the project explorer view.

Build your project by reproducing the following steps:

IAR: build
Connectivity Zigbee Build Project.png


You can build and flash the project on your board by clicking on the button as illustrated below:

IAR: build and flash
Connectivity Zigbee BuildProject.png

3.2. STM32CubeIDE

Select the application that you want to build, open the STM32CubeIDE dedicated directory. Launch the STM32CubeIDE, and select the folder .project of the demonstration.

CubeIDE project folder
Connectivity Zigbee IDE.png




Ensure that your project is correctly visible into the project explorer view.
Build your project by reproducing the following steps:

CubeIDE: build
Connectivity Zigbee CubeIDE.png


Flash it on the board:

CubeIDE: flash
Connectivity Zigbee Flash CubeIDE.png

3.3. Install the application from STM32CubeProgrammer

It is possible either to flash the previously build binary using STM32CubeProgrammer software[7].

Select your device and connect to it:

CubeProgrammer: platform connection
Connectivity Zigbee Build CubeProgrammer.png


Once connected, the device information is displayed on the Cube programmer interface. Click on the programming icon, in the left column, and select the project binary to flash (could be .hex, .elf, or .bin):

  • [...]\Projects\[...]\Applications\Zigbee\Zigbee_Find_Bind_Coord\[...]\ Zigbee_Find_Bind_Coord.elf

Then, click on the Start programming button:

CubeProgrammer: flash project
Connectivity Zigbee CubeProgrammer.png


When the programming is complete, the following logs are displayed:

CubeProgrammer: logs
Connectivity Zigbee log.png

4. References


[[Category:Zigbee|30]]


No categories assignedEdit