![]() |
Coming soon |
1. LC3 Codec
The LC3 codec is an algorithm allowing to compress audio data for transmitting over the air.
This codec must be supported by any application build over the Generic Audio Framework and BLE 5.2 isochronous feature. It runs channel independently, has a complexity similar to Opus, and can be used for either voice and music with a better quality.
1.1. LC3 configuration
BLE profile configures an LC3 session defined by:
- The sampling frequency : 8, 16, 24, 32 ,44.1 or 48 kHz
- The frame duration : 7.5 or 10ms
The frame duration varies a little with 44.1 kHz, refers to LC3 specification [1] for details
Then it also configures each channels referring to the session with additional information:
- The mode : encoding or decoding
- The PCM sample width : 16, 24 or 32 bits
- The bitrate within a list of recommended bitrates
The LC3 supports bitrate updates, but BLE profiles don't use this feature
Also, the ST LC3 codec embed a Packet Loss Concealment algorithm based on the annex B of the LC3 specification. This algorithm ensure signal continuity and reduced glitches in cases of corrupted/missing packet and is triggered by either an external indicator BFI or an internal frame analysis.
Picture data flow
At the encoder side, the data flow if the following
- Data Input
- PCM signal buffered into an Nf samples per channel, this size is linked to the frame duration and frequency.
- For example, 10ms frame at 32kHz leads to 320 samples
- Data Output
- An encoded buffer per frame per channel of size Nbytes, this size is directly linked to the bitrate and is within the range of 20 to 400 bytes.
- In our example, 64kbps leads to 80 bytes, so compression factor of 8 for 16bits/sample
1.2. LC3 requirement
Our LC3 implementation is based of floating point numbers and needs to access the FPU for fast computation as well as the support of DSP instructions. Also, since it's an heavy process, it is recommenced to use high core clock with Instruction Cache enabled. The library provided is compiled for cortex M33 with speed optimization.
Provided by the application, the following RAM must be allocated for running the full feature LC3:
- 604 bytes per session
- 4820 bytes per encoding channel
- 8340 bytes per decoding channel
Also, at least 7000 bytes are allocated by the encoder over the stack, or 4700 bytes if the only decoder is used.
The flash footprint of the full codec represents around 120 kBytes and can be reduced at the linking time if only one mode is used.
Finally here is an overview of the CPU load required Picture of CPU load
This LC3 implementation is SIG certified with the QDID : XXXXX
2. Audio path architecture
2.1. Clock synchronization
2.1.1. Genelarities
The Bluetooth specification says when use unframed PDU, the upper layer must synchronize generation of its data to the effective transport timings. In BLE, transports timings are defined by the link layer master and upper layers (including audio peripheral) from both slave and master side have to synchronize to the that timings. This statement has also sense when using framed PDU for avoiding glitch generation and having the same data rate from the audio source to the audio sink.
Picture clocks domain
The most constraining role is BLE slave, meaning the device has to synchronize it's audio peripheral clock to the remote link layer. Being slave on the audio peripheral brings a constraint impossible to respect.
RF Role | Audio Role | Sleep Clock Source | Synchronization method |
---|---|---|---|
Master | Master | LSE | PLL Loop control |
HSE/1000 | Direct synchronization | ||
LSI | PLL Loop control (not recommended) | ||
Slave | Any | None | |
Slave | Master | Any | PLL Loop control |
Slave | Any | None |
2.1.2. Implementation
Drift measurement can be done through the link layer and adjustment of the frequency can be done on the fly by updating the fractional N value of the PLL. For that, the PLL corrector provided needs an an approximately 1MHz free running timer, clocked by the PLL output, to measure drifts.