How to perform people counting using FP-AI-VISION1 and STM32H747XI

Revision as of 02:21, 14 October 2023 by Registered User

Some recent STM32H747I-DISCO kits are shipping with MB1166-A09 LCD daughterboards. This daughterboard uses an updated LCD controller, NT35510. This article describes how to run FP-AI-VISION1 projects kits with the updated LCD daughterboard, with a focus on incorporating the updated LCD driver into existing projects.

1. Prerequisites:

  1. . STM32H747I-DISCO with LCD daughterboard "MB1166-A09"

Note: This guide is not suitable for MB1166-A08 and MB1166-A10 LCD revisions. Follow the instructions given in FP-AI-VISION1 / TODO for these revisions.

  1. . Computer with STM32CubeIDE installed (v1.13.1 or higher)


2. Steps:

  1. . Download and unzip NT35510 drivers from this zip file. Alternatively, up-to-date drivers can be downloaded directly from the STM32CubeH7 GitHub repo.
  2. . Copy the entire nt35510 directory to

..\FP-AI-VISION1_V3.1.0\Drivers\BSP\Components\ <\code>

  1. . Copy

stm32h747i_discovery_lcd.c <\code>

and ```stm32h747i_discovery_lcd.h``` , and paste them into ```..\FP-AI-VISION1_V3.1.0\Drivers\BSP\STM32H747I-Discovery\```
  1. . Use a text editor to open ```..\FP-AI-VISION1_V3.1.0\Projects\STM32H747I-DISCO\Applications\Common\CM7\Inc\stm32h747i_discovery_conf.h```. On line 34, make the following changes:
/* LCD controllers defines */ <br />
#define USE_LCD_CTRL_NT35510                1U <br />
#define USE_LCD_CTRL_OTM8009A               0U <br />
#define USE_LCD_CTRL_ADV7533                0U <br />
  1. . TODO: Drag/drop nt355510 to components directory in CubeIDE
  2. . Compile and flash
No categories assignedEdit