This message will disappear after all relevant tasks have been resolved.
Semantic MediaWiki
There are 1 incomplete or pending task to finish installation of Semantic MediaWiki. An administrator or user with sufficient rights can complete it. This should be done before adding new data to avoid inconsistencies.1. Introduction
It is advised to start by reading the New product state article.
From the development phase until the maintenance phase a product can be configure under many product states ( also called lifecycle states).
The lifecycle controls the access to code and data.
This article lists in which product states a STM32H5 can be configured.
2. Product states
2.1. Product state : Open
- This state is mainly used during the development phase since the device is fully open.
- Debug is fully open.
- The Trust Zone can be disabled or enabled (TZEN option byte programming).
- Bootloader is usable.
- This state is mainly used during the development phase since the device is fully open.
2.2. Product state : provisioning
- This state is used during the provisioning.
- The debug is only available when executing a nonsecure user application.
- The Trust Zone can be disabled or enabled (TZEN option byte programming).
- Bootloader is usable.
- Secure Firmware install can be launched in this state (not anymore possible in the following states).
- This state is used during the provisioning.
2.3. Product state : Provisioned
- In this state, the OEMiRoT or STiRoT code and datas are provisioned.
- Debug is available only when executing a nonsecure user application.
- Debug Authentication can be launched : Debug access for secure applications can be available by launching the Debug Authentication (see Debug Authentication setting).
- The OEMiROT or STiRoT can launch the bootloader if the verification of the code located in the next isolation level is failing (authentication, integrity, or missing code)
- In this state, the OEMiRoT or STiRoT code and datas are provisioned.
2.4. Product state : TZ-Closed
- The TZ-Closed state corresponds to an intermediate state of the product. All the secure firmware is installed, the non secure application can be developed, or loaded in a second instance.
- The iROT + uROT (optional) + Secure-OS code and data are provisioned.
- uROT(optional) can launch the bootloader if the verification of the code located in the next isolation level is failing (authentication, integrity, or missing code).
- The debug is only available when executing a nonsecure user application.
- Debug Authentication can be launched : Debug access for secure applications can be available by launching the Debug Authentication.
- From this state, the non secure application can be updated using the firmware update mechanism, or directly programmed through the flash loader (embedded in the IDE).
2.5. Product state : Closed
- This state occurs with the fully provisioned product.
- Debug Authentication is allowed : The debug is fully closed but can be opened by launching the Debug Authentication (see Debug Authentication setting).
- This state occurs with the fully provisioned product.
2.6. Product state : Locked
- This state is used with the fully provisioned product without any more changes.
- Locked is a final unchangeable product state. No method can modify the embedded firmware and product configuration.
- The debug is definitively closed and cannot be reopened through debug authentication.
- No regression is possible anymore
- This state is used with the fully provisioned product without any more changes.