Certification guideline/Bluetooth Qualification Process example with STM32WBx

Revision as of 17:56, 20 July 2023 by Registered User


We will follow the 7 different steps described in Launch studio webpage but before going through this process, let's see the information of our STM32WB55RG & his associated BLE stack.

1. STM32WB55RG Component (Tested) & its associated BLE stack information

https://launchstudio.bluetooth.com/Listings/Search

1.1. STM32WB55RG Component (Tested)

In this windows, you will find the QDID number for the STM32WB55 127495. Notice that you have different STM32WB55 versions depending on the flash size. In our example, let use the STM32WB55RG (512kB flash)


This RF PHY has been qualified in 2019, with Core specification 5.0


You can notice that this component has been qualified with Test Case reference List version 2023 -1
the details of the TCRL Test list are there TCRL information

1.2. STM32WB_BLE_STACK



You can see that the STM32WB _BLE stack has been qualified with core BT5.3 & BT 5.4. This STM32WB_BLE_STACK_Full_Ext include new BT5.4 features such as Encrypted advertising data and LE GATT security levels characteristics along with GAP/GATT/SM & L2CAP layers on M0+.
If you start to develop your platform, ST recommends using BLE STACK supporting latest BT version 5.4 even if your RF PHY has been only qualified with lower BT core version.

2. Qualification process

You can find different links on Bluetooth website detailing the different steps.

https://www.bluetooth.com/develop-with-bluetooth/qualification-listing/
/https://launchstudio.bluetooth.com/ProjectBasics/

2.1. Project Basics


you must select 1 RF_PHY & 1 HOST stack at least for your end project.
the HOST stack is linked to a SK version. In our case (STM32WL55RG), you will find the latest SDK version in our ST webiste.
https://www.st.com/en/embedded-software/stm32cubewb.html


after having selected your project as End Product, we must select the Controller & Host core configuration as LE controller. Indeed, ST RF-PHY & Host stack previously selected are BLE only oriented.
Then select Layer Selection step

2.2. Layer Selection


All different layers have been pre-checked based on component features.
However, no Standard Profile have been qualified for STM32WBx. If you need any, we must select it and provide your own test evidence.
then, you can continue to next section ICS selection

2.3. ICS Selection

this section could be confusing because you must solve all potential inconsistencies.
capabilities of each layer are pre selected, but depending on the TCRL version used for qualification of the RF PHY & Host stack, some inconsistencies could appear.

to evaluate the inconsistencies, you must click on consistency check button on top right.



You must check all different inconsistencies highlighted & correct the pre-selected features, See, for example, the inconsistency related to your Product & Controller Core Specification.


Your End Project should support only 1 Core specification. However, by default, since the RF-RHY has been qualified with Core 5.0 & the Host stack with Core 5.4, the tool has selected these 2 Core specifications ( 5.0 to 5.4). Since you use ST BLE stack 5.4, you must unselect all previous Core specification.


You must proceed like this, for all inconsistencies. When all inconsistencies have been fixed, you can proceed to next section.

2.4. Testing

2.5. Test Documentation

2.6. Product Declaration

2.7. Declaration ID

2.8. Review & Submit