Getting started with STM32H5 security

Revision as of 11:01, 4 July 2023 by Registered User


A set of practical examples is proposed to get an overview and to understand the STM32H5 security solutions.
These practical examples are based on the boards, tools and code examples provided by ST.
This article gives an overview of these proposed examples.
For the examples listed below, each step to be done is described in detail.
It is advised to start with these examples before making your own trials or using other security related examples available in the STM32Cube_H5.

Product Serie STM32H503 picto.png STM32H563 picto.png STM32H573 picto.png Prerequisite Introduction article
Ecosystem NUCLEO-H503RB (MB1814) NUCLEO-H563ZI(MB1404) STM32H573I-DK(discovery)
STM32CubeMX OEMiROT example on STM32H573/563 Link to How To Link to How To STM32CubeMx_V6.9.0 or later Link
STM32CubeMX STiROT example on STM32H573 Link to How To STM32CubeMx_V6.9.0 or later Link
STM32CubeMX Secure Manager example Link to How To STM32CubeMx_V6.9.0 or later Link
Debug Authentication on STM32H573/563/503 (TZ disabled) example Link to How To Link to How To Link to How To STM32CubeH5 Link
OEMiROT on STM32H573/563 (TZ enabled) example Link to How To Link to How To STM32CubeH5 Link
OEMiROT on STM32H503 example Link to How To STM32CubeH5 Link
STiROT on STM32H573 example Link to How To STM32CubeH5 Link
Secure Manager on STM32H573 Link to How To STM32CubeH5_V1.1.1 or later; X-CUBE-SEC-M-H5_v1.0.0 or later Link

1. Secure Boot

The Secure Boot and related Root of Trust is implicitly used in all the proposed " How to start" step by step examples.
But a bootpath can be defined from scratch and a related firmware frame is generated using the STM32CubeMx.
The proposed example on this topic is based on STM32CubeMx

2. Debug Authentication

It is key to well understand how to set the Debug Authentication (DA) in order to define the wanted rights to reopen the debugger once closed.

3. OEMiROT

An OEM can develop his own customized Immutable Root Of Trust (OEMiROT).
It is advised to read the Secure Boot for STM32H5 wiki article to understand the different possible Root of Trust.

4. STiROT

An immutable root of trust defined by ST is included natively for the STM32H57x serie.
It's an embedded firmware stored in the system flash and that can't be modified.
It is advised to read the Secure Boot for STM32H5 wiki article to understand the different possible Root of Trust.

5. Secure Manager

ST provides a solution enhancing the security offer and is easy to install and to use.
This solution is called the Secure Manager and provides secure boot, updatable root of trust, PSA secure services available at run time of the application, and a secure module management.
The secure manager is only supported for the STM32H573xx product line.