1. Introduction
This wiki describes to an application developer how to integrate the STM32WBAxx Bluetooth® LE stack library.
It covers only the Bluetooth® LE stack library integration, and it does not include the Link Layer integration aspects.
Acronyms definitions | ||||||||
---|---|---|---|---|---|---|---|---|
|
2. Bluetooth® LE Stack Overview
2.1. Release contents
2.1.1. Folder structure
The Bluetooth® LE stack delivery contains 3 folders as following:
Bluetooth® LE library folder structure |
---|
- “doc” folder contains the current document and “STM32WBA_BLE_Wireless_Interface.html” which describes the Bluetooth® LE Application Commands Interface (ACI) and the Host Commands Interface (HCI).
- “include” folder contains the header files of the Bluetooth® LE stack library interface. These files contain some definitions of constants and types and the declarations of ACI and HCI functions. It also contains the declarations of some external modules’ functions used by the Bluetooth® LE stack (for more details see section 4.2)
- “lib” folder contains the 4 Bluetooth® LE stack library variants described in the following section.
2.1.2. Library variants
The Bluetooth® LE stack library is delivered in 4 variants:
- 2 variants containing the Bluetooth® LE host stack:
- Full stack (stm32wba_ble_stack_full.a)
- Basic stack (stm32wba_ble_stack_basic.a)
- 2 variants without the Bluetooth® LE host stack (controller only):
- Link Layer Only stack (stm32wba_ble_stack_llo.a)
- Link Layer Only Basic stack (stm32wba_ble_stack_llobasic.a)
Here are the 4 Bluetooth® LE stack variants details:
- Full stack (stm32wba_ble_stack_full.a) includes the LE Controller and the Host Stack, and contains all the legacy stack supported features plus the extended advertising, GATT caching, ACI HCI flow control, isochronous support for audio, L2CAP connection oriented channels.
Note: This Bluetooth® LE stack variant can be configured to run in controller only mode (host stack is bypassed).
See the parameter “options” of the initialization structure BleStack_init_t parameters in [3.1] to enable/disable the controller only mode.
- Basic stack (stm32wba_ble_stack_basic.a) contains only basic supported features or Bluetooth® LE legacy features without extended advertising, neither GATT caching, nor ACI HCI flow control, nor isochronous support, nor L2CAP connection oriented channels. The Host Stack is included, and it supports all the basic GATT, GAP and L2CAP features.
- Link Layer Only stack (stm32wba_ble_stack_llo.a) contains all the features supported by the full stack but doesn’t include the Host Stack (GATT, GAP and L2CAP features).
- Link Layer Only Basic stack (stm32wba_ble_stack_llobasic.a) contains all the features supported by the basic stack but doesn’t include the Host Stack (GATT, GAP and L2CAP features).
For more information, please refer to “STM32WBA_BLE_Wireless_Interface.html” to know which ACI and HCI command/event is supported by each stack configuration.
The table below details the supported features for each Bluetooth® LE stack variants:
2.2. Real-Time environment
2.3. Library dependencies
2.4. Library compilation options
2.5. Application compilation options
3. Bluetooth® LE stack user interface
3.1. Bluetooth® LE stack initialization
3.2. Bluetooth® LE stack process
3.3. Bluetooth® LE stack modes
4. Bluetooth® LE Stack Porting
4.1. Stack Porting
4.2. Bluetooth® LE platform functions
4.2.1. NVM functions
4.2.2. Timer functions
4.2.3. AES functions
4.2.4. PKA functions
4.2.5. RNG functions
5. References
6. Wiki syntax examples
Header text | Header text | Header text |
---|---|---|
Example | Example | Example |
Example | Example | Example |
Example | Example | Example |
Bluetooth® LE Health Thermometer Service specification | ||||||||||||||||||||||||||||||||||||||||||||||||||||
---|---|---|---|---|---|---|---|---|---|---|---|---|---|---|---|---|---|---|---|---|---|---|---|---|---|---|---|---|---|---|---|---|---|---|---|---|---|---|---|---|---|---|---|---|---|---|---|---|---|---|---|---|
|
ST Bluetooth® LE example project directory |
---|
ST Bluetooth® LE example project directory |
---|
Bluetooth®
texte - “doc” folder contains the current document and “STM32WBA_BLE_Wireless_Interface.html” which describes the BLE Application Commands Interface (ACI) and the Host Commands Interface (HCI).
- “include” folder contains the header files of the BLE stack library interface. These files contain some definitions of constants and types and the declarations of ACI and HCI functions. It also contains the declarations of some external modules’ functions used by the BLE stack (for more details see section 4.2)
- “lib” folder contains the 4 BLE stack library variants described in the following section.
BLA BLA BLA
ST Bluetooth® LE pour Nidhal |
---|
/**
******************************************************************************
* @file STM32WB_P2P_Server.ino
* @author WBL BLE Application Team
* @brief Arduino STM32WB P2P Server Application (Custom STM)
******************************************************************************