Introduction to Secure boot and Secure firmware update

Revision as of 17:34, 3 May 2023 by Registered User

1. What is the Secure Boot and Secure Firmware Update

Secure Boot and Secure Firmware Update ensure that only authorized software is executed on the device.
  • Secure Boot is the first firmware running after a STM32 reset. It activates the security mechanisms, and verifies the authenticity and the integrity of the code executed on the platform after the boot stage (Application). Secure Boot is the foundation of the device security, also known as the Root of Trust (RoT) of the device.
  • This foundation is extended by the Secure Firmware Update functionality, allowing to securely update the Application.

2. Secure Boot

Secure Boot uses cryptography to verify (Authentication + Integrity) the Application code and metadata.
Secure Boot only grants Application execution if verifications on both the code and the metadata are successful. Metadata may contain version information, hardware configuration, boot conditions, and many more.
Secure Boot must be an immutable code launched at reset. Immutability is a mandatory requirement for Secure boot.
ROMCode technology -or any other mechanism allowing the code to be immutable- ensures the immutability. In STM32 microcontrollers, the write protection mechanism on the flash memory typically supports immutability.
The immutable code must be concise, simple and verifiable. This minimizes the risk of a vulnerability that cannot be corrected. Complex steps are handled at the following stage.
The immutable code is executed at reset. It verifies the platform configuration, such as the boot configuration and the protection mechanisms. This code is the RoT (Root Of Trust).

3. Secure Firmware Update

The Secure Firmware Updatability of the Application is a key point to ensure security while considering vulnerability risks. If the Application in the device is concerned by a security weakness, an Application update is performed in order to fix it.
The Secure Firmware Update of the Application relies on cryptography to decrypt, authenticate and check the integrity of the newly received Application image.
The Secure firmware Update can be implemented by following different strategies:
  • One slot: a new Application image overwrites the running Application within the slot. This configuration can be used when local download is allowed.
  • Two slots: the Secure firmware update verifies the new Application image within the first slot (Download slot) and install it within the second slot (Execution slot). This configuration can be used if Over The Air updates are supported.
  • Recovery: if no valid image remains within any slot, the Secure firmware update recovers a factory image.
  • Other strategies.
Regardless of the strategy used, Secure Firmware Update must handle version control. Secure Firmware Update ensures that a previous version of the Application (Application version N-1) can not be installed after running the current Application version (Application version N).
The Application is responsible for downloading the new Application image. Once the new image is received, the Application triggers a reset on the device for a Secure Boot, and Secure Firmware Update installs the new Application version.


Image programming must be resistant to asynchronous power down and reset.
Image upgrade strategy can:
- be based on overwriting, swapping, or any other mechanism.
- consider all the image updates in one time, or in sequential steps (depending on Non Volatile space).
- take into account code update and image data.


4. STM32 Secure Boot and Secure Firmware Update implementations

ST offers several implementations of Secure Boot and Secure Firmware Update, according to STM32 HW capabilities:


5. References