This message will disappear after all relevant tasks have been resolved.
Semantic MediaWiki
There are 1 incomplete or pending task to finish installation of Semantic MediaWiki. An administrator or user with sufficient rights can complete it. This should be done before adding new data to avoid inconsistencies.Coming soon |
1. What is product lifecycle
PRODUCT Lifecycle is used to control the product security configuration. It allows to control the activation of the platform’s security mechanisms.
1.1. New product lifecycle
- We are introducing a new PRODUCT Lifecycle, in order to allow more flexibilities on product manufacturing and maintenance.
- The new PRODUCT Lifecycle considers different phases using the product.
- The considered phases are:
- - development phase, offering all debug allowed to developer.
- - provisioning phase, where main assets area become protected (no more accessible) …
- - final phase, where the product is considered in the field.
- - maintenance phase: field return management.
- During all product life, the solution must guarantee that ROT and user assets are never disclosed.
- This must be true for development, provisioning, final phase, and field return phases.
- The new product Lifecycle propose the below product states:
- - Open
- - Provisioning
- - iROT-Provisioned
- - TZ-Closed (optional: only when TrustZone is supported)
- - Closed or Locked
- The goal of this document is to provide details on the different lifecycle states.
- Warning: The Debug Authentication configuration (DA-config) must be provisioned in Provisioning state.
1.2. Up to 3 third parties
- In the development and provisioning phases, the product Lifecycle allows to consider the product being developed by up to 3 third parties.
- Different third parties means that for development and provisioning, we are able to set the product in a state that's allow to protect (isolate) the different parties.
- The Lifecycle allows to consider up to 3 different third parties (iROT + TZ-Application + NS Application) for development and Provisioning.
1.2.1. ST Lifecycle consider 3 Main bricks to be installed in the product that could rely on 3 different partie
1.2.2. ST Lifecycle Development and Provisioning considering up to 3 parties
- 1 party: All Firmware owned by one entity.
- 2 parties: All Secure part owned by one part, then Non-Secure application owned by a second part.
Means 2 different
- 3 parties: iROT, Secure and Non-Secure appli owned by 3 different parties
1.2.3. ST Lifecycle Initial provisioning (from Open or Provisioning)
- We recommend to use SFI for untrusted manufacturing
- We recommend to protect all key provisioning even if the manufacturing is trusted.
1.2.4. ST Lifecycle To complete the initial provisioning
- Provisioning done based on firmware(s) already installed at initial provisioning
- - Secure Firmware Update / Secure Key Provisioning
- - In one or 2 steps
- Provisioning done based on firmware(s) already installed at initial provisioning