STM32CubeWB Zigbee MCU Package

Revision as of 16:39, 28 March 2023 by Registered User


1. Introduction

The STM32CubeWB MCU Package[1] provides software components running on STM32WB Series MCUs.
For all examples provided with the package, the following integrated development environments are supported:

  • STMicroelectronics integrated development environment for STM32 products (STM32CubeIDE)
  • IAR Systems® IAR Embedded Workbench® for Arm® (EWARM)
  • Keil® Microcontroller Development Kit (MDK-ARM)

The Firmware Package for the STM32WB series is also available on STM32CubeWB github[2].

2. STM32WB Bluetooth® LE software architecture

The STM32WB Bluetooth® low energy architecture separates the Bluetooth® Low Energy Profile and application, running on the application Cortex®-M4, from the Bluetooth® low energy real-time aspects residing in the Bluetooth® Low Energy Peripheral.

The Bluetooth® Low Energy peripheral incorporates a Cortex®-M0+ processor containing the Bluetooth® Low Energy STACK handling the link layer up to the generic attribute profile and generic access profile layers.
More information regarding the Bluetooth® LE Wireless Stack configuration

STM32WB Bluetooth® LE architecture
Connectivity STM32WB BLE Architecture.png

Regarding the Bluetooth® LE software architecture more information is available in the application note Building wireless applications with STM32WB Series microcontrollers[3].

3. STM32WB Bluetooth® LE application

The following Bluetooth® LE applications are delivered as source code.

Application Description
Bluetooth® LE SIG BLE_Beacon Application advertising different types of beacon: ibeacon, eddystone (tlm, uuid, url)
BLE_BloodPressure Application supporting the Blood Pressure Sensor as specified by the Bluetooth® SIG
BLE_HealthThermometer Application supporting the Health Thermometer Sensor as specified by the Bluetooth® SIG
BLE_HeartRate Application supporting the Heart Rate Sensor as specified by the Bluetooth® SIG
BLE_HeartRate_ThreadX Application supporting the Heart Rate Sensor with ThreadX implementation
BLE_Hid Application supporting the Human Interface Device services for mouse and keyboard as specified by the Bluetooth® SIG
BLE_Proximity Application supporting the Find Me and Proximity Services as specified by the Bluetooth® SIG
Bluetooth® LE ST proprietary BLE_AT_Server ST proprietary application to use the the STM32WB as a network processor via AT command
BLE_CableReplacement ST proprietary application to simulate the previous Bluetooth® protocol "Serial Port Profile"
BLE_DataThroughput ST proprietary application to measure data throughput between 2 STM32WB or with the dedicated ST Bluetooth® LE toolbox smartphone application (Android and IOS)
BLE_Ota ST proprietary application to upgrade the STM32WB CM4 application or the secure flash CM0+ wireless stack or FUS
BLE_p2pServer Simple ST proprietary application to use the STM32WB as a Peripheral and GATT Server
BLE_p2pClient Simple ST proprietary application to use the STM32WB as a Central and GATT Client
BLE_p2pServer_Ext Application to configure up to 8 advertising extended sets
BLE_p2pClient_Ext Application to scan the extended advertising frames with extended API’s
BLE_p2pRouter ST proprietary application to use the STM32WB as a Central & Peripheral and GATT Client & Server with multi link connection
BLE_Peripheral_Lite Simple ST proprietary application to use the STM32WB as a peripheral and GATT server with minimum activated features (no low power manager, no task sequencer, no timer server, and so on)
BLE_RfWithFlash Simple ST proprietary application to use the STM32WB P2P server with write and erase access to the flash
BLE_TransparentMode ST proprietary application to support the Direct Test Mode for RF certification. Standard host controller interface (HCI) and application (vendor) controller interface (ACI) can be sent by means of STM32CubeMonitor-RF
BLE_Sensor ST proprietary application to demonstrate capabilities of STM32WB5MM Discovery Kit with the use of board sensors
Bluetooth® LE Mesh Mesh Lighting Proxy Relay Friend Node Bluetooth® LE Mesh Lighting profile as specified by the Bluetooth® SIG supporting Proxy-Relay-Friend Node with the capacity to handle a friendship with a Low Power Node
Mesh Lighting Low Power Node Bluetooth® LE Mesh Lighting profile as specified by the Bluetooth® SIG supporting Low Power Node with the capacity to be associated to a Friend Node for friendship
Mesh Lighting Embedded Provisioner Bluetooth® LE Mesh Lighting profile supporting ST Proprietary Embedded provisioner with the capacity of creating MESH network from unprovisionned nodes, such as Proxy-Relay-Friend nodes or Low Power nodes

4. Going further based on available application

Application Description
Bluetooth® LE Feature Fast FUOTA Explanation to support fast firmware upgrade over-the-air
Additional Beaconing Explanation to implement an additional beacon
Advertising Extension Explanation to implement the extended advertising feature
Bluetooth® LE Mesh Mesh Sensor Model Client Server example Explanation and concept regarding the Mesh Sensor Model client requesting information from the sensor model server
Mesh Vendor Model example Explanation and concept regarding the ST proprietary mesh vendor model
Others Bluetooth® LE & Arduino Explanation and concept regarding the Bluetooth® LE P2P application done with Arduino framework

5. References