Click here for Cellular overview
1. How To...
1.1. Introduction
This wiki article is a guideline that describes how to perform the main activities with X-CUBE-CELLULAR.
The section "How To" is divided into three parts. The first part concerns common remarks related to Azure RTOS and Free RTOS. The second part is specific to FreeRTOS while the last part relates to Azure RTOS .
1.2. How To applicable to FreeRTOS and Azure RTOS versions
1.2.1. How to start the delivered binary firmware
The binary firmware is provided for each supported board. The example below describes how to run the STM32L496 binary for the BG96 modem, the process is he same with other hardware setups. The steps are:
- Insert an activated SIM into the BG96 modem STMod+ board.
- Plug the BG96 modem board (module up, SIM down) into the STM32L496 board, more details on Cellular hardware setup.
- Plug an USB cable (the one near the blue quad-switch) on the STM32L496 board a new volume (DIS_L496ZG) displays on your PC).
- Flash the firmware (drag and drop the .bin onto the newly appearing volume).
- Open a TeraTerm serial terminal and set the right parameters (see the section below "How to setup Teraterm parameters").
- If required (by default it is empty), enter the right SIM APN using the APN setting as defined in the related "How To" section detailed below.
1.2.2. How to find the delivered binary required
All the binaries provided are available at: \Projects\<STM32 board name>\Demonstrations\<Demonstration name>\Binaries\
Example: \Projects\B-U585I-IOT02A\Demonstrations\Cellular\Binaries\
The name of the binaries indicates its purpose, <STM32 board>_<modem>_<IP stack>.bin
- u585_bg96_stm32ip.bin is the binary for the U585 discovery board associated to the BG96 modem and the IP stack selected is the IP in the STM32.
- u585_bg96_modemip.bin is the binary for the U585 discovery board associated to the BG96 modem, and the IP stack selected is in the modem.
1.2.3. How to set up Tera Term parameters
- Terminal
- [New line]
- [Receive]: Auto
- [Transmit]: CR
- [Local echo] selected
- [New line]
- Serial
- [Baud rate]: 115200
- [Data]: 8 bi
- [Parity]: none
- [Stop]: 1 bit
- [Flow control]: none
- [Transmit delay]: 10 ms each
1.2.4. How to set up the CLI commands available list
Hit "enter" then type "help" then hit "enter" the list of commands is displayed.
List of commands example:
- help: help command
- trace: trace management
- comlib: com library commands
- cst: cellular service task management
- atcmd: send an at command
- modem: modem configuration management
Therefore, to send an AT command to the modem just enter: atcmd AT+QIRC
1.2.5. How to APN selection and configuration
See complete article about APN management and configuration
1.2.6. How to get the modem and cellular network information
1.2.6.1. using console commands
- Open a Tera Term serial terminal and set the right parameters.
- Remove the trace display by typing the commands:
- trace off
- cst poll off
Then type the Cellular Service commands:
- cst
- cst state
- cst info
- cst config
1.2.6.2. using control API
Here is a code example to retreive and display information about modem and cellular
#include "cellular_control_api.h"
cellular_sim_info_t my_sim_info;
cellular_sim_info_index_t my_sim_info_index;
cellular_operator_selection_t my_operator_selection;
cellular_info_t my_cellular_info;
cellular_signal_info_t my_signal_info;
cellular_ip_info_t my_ip_info;
cellular_get_sim_info(&my_sim_info);
/* print actual selected sim */
PRINT_FORCE("Sim Selected (slot type > status) : %d > %d", my_sim_info.sim_slot_type, my_sim_info.sim_status)
/* For each defined SIM slot, and in priority order, display : */
/* the slot interface */
/* the result of sim activation */
/* the APN information */
PRINT_FORCE("All sim information :")
for (uint8_t n = 0U; n < my_sim_info.sim_slot_nb; n++)
{
if (cellular_get_sim_info_from_index(n, &my_sim_info_index) == CELLULAR_SUCCESS)
{
PRINT_FORCE("- Sim (slot type : status) %d : %d", my_sim_info_index.sim_slot_type, my_sim_info_index.sim_status)
if(my_sim_info_index.sim_status == CA_SIM_READY)
{
/* ICCID and IMSI are known only for sim initialized and ready */
PRINT_FORCE(" ICCID : %s", my_sim_info.iccid.value)
PRINT_FORCE(" IMSI : %s", my_sim_info.imsi.value)
}
PRINT_FORCE(" APN : %s", my_sim_info_index.pdn.apn.value)
PRINT_FORCE(" APN username : %s", my_sim_info_index.pdn.username.value)
PRINT_FORCE(" APN password : %s", my_sim_info_index.pdn.password.value)
PRINT_FORCE(" CID : %d", my_sim_info_index.pdn.cid)
if (my_sim_info_index.pdn.apn_send_to_modem == CA_APN_SEND_TO_MODEM)
{
PRINT_FORCE(" APN is sent to modem")
}
else
{
PRINT_FORCE(" APN is not sent to modem")
}
}
}
/* Display NFMC information */
cellular_get_nfmc_info(&my_nfmc_info);
if (my_nfmc_info.enable != 0U)
{
/* NFMC feature active. Displays the temporization list */
/* Display all NFMC tempo */
for (i = 0U; i < my_nfmc_info.tempo_nb ; i++)
{
PRINT_FORCE("nfmc tempo %ld : %ld", i + 1U, my_nfmc_info.tempo_values[i])
}
}
else
{
PRINT_FORCE("No nfmc tempo set");
}
/* Operator registration configuration */
cellular_get_operator(&my_operator_selection);
PRINT_FORCE("Network register mode: %d", my_operator_selection.ntw_registration_mode);
if (my_operator_selection.ntw_registration_mode != CA_NTW_REGISTRATION_AUTO)
{
/* If registration is not automatic, display also : */
/* Operator name format */
PRINT_FORCE("Operator name format: %d",
my_operator_selection.operator_name_format);
/* Operator name */
PRINT_FORCE("Operator name: %s\n\r", my_operator_selection.operator_name.value);
}
/* Access techno present or not */
if (my_operator_selection.access_techno_present == CA_ACT_PRESENT)
{
PRINT_FORCE("Access techno present: Present");
/* If access techno is present, display the techno to used */
PRINT_FORCE("Network register mode: %d", my_operator_selection.access_techno);
}
else
{
PRINT_FORCE("Access techno present: Not present");
}
/* reads cellular info from cellular API */
cellular_get_cellular_info(&my_cellular_info);
/* reads signal info from cellular API */
cellular_get_signal_info(&my_signal_info);
/* reads IP address from cellular API */
cellular_get_ip_info(&my_ip_info);
PRINT_FORCE("Cellular Service Infos ")
/* Dynamic modem related information */
PRINT_FORCE("Modem state : %d", my_cellular_info.modem_state)
PRINT_FORCE("Signal Quality : %d", my_signal_info.signal_strength.raw_value)
PRINT_FORCE("Signal level(dBm) : %ld", my_signal_info.signal_strength.db_value)
/* SIM related information */
PRINT_FORCE("IMEI : %s", my_cellular_info.imei.value)
/* Modem hardware related information */
PRINT_FORCE("Manuf name : %s", my_cellular_info.identity.manufacturer_id.value)
PRINT_FORCE("Model : %s", my_cellular_info.identity.model_id.value)
PRINT_FORCE("Revision : %s", my_cellular_info.identity.revision_id.value)
PRINT_FORCE("Serial Number : %s", my_cellular_info.identity.serial_number_id.value)
/* Cellular access techno used */
PRINT_FORCE("Network bearer (AcT) : %d", my_signal_info.access_techno)
PRINT_FORCE("IP address : %d.%d.%d.%d",
(uint8_t)(my_ip_info.ip_addr.addr & (uint8_t)0xFF),
(uint8_t)((my_ip_info.ip_addr.addr >> 8) & (uint8_t)0xFF),
(uint8_t)((my_ip_info.ip_addr.addr >> 16) & (uint8_t)0xFF),
(uint8_t)((my_ip_info.ip_addr.addr >> 24) & (uint8_t)0xFF))
1.2.7. How to set modem in a particular mode
1.2.7.1. Switch modem off
This will switch off the modem. Modem power will be cut off. Switching modem off can be done in any state of the modem :
- on without sim or network management
- on restricted to sim access
- on with connection to network
1.2.7.1.1. At boot time
In the file plf_cellular_config.h
, change the value of the define PLF_CELLULAR_TARGET_STATE
to 0
:
#define PLF_CELLULAR_TARGET_STATE (0U)
1.2.7.1.2. Using console command
- Open a serial terminal and set the right parameters.
- Remove the trace display by typing the commands:
- trace off
- cst poll off
Then type the Cellular Service command :
cst modem off
1.2.7.1.3. Using control API
#include "cellular_control_api.h"
/* API call to stop the modem. */
(void)cellular_modem_stop();
1.2.7.2. Switch modem on restricted to sim access
This will switch on the modem. Only sim access will be activated, without network and data transfer management. Sim only mode equivalent to AT+CFU=4
AT command.
1.2.7.2.1. At boot time
In the file plf_cellular_config.h
, change the value of the define PLF_CELLULAR_TARGET_STATE
to 1
:
#define PLF_CELLULAR_TARGET_STATE (1U)
1.2.7.2.2. Using console command
- Open a serial terminal and set the right parameters.
- Remove the trace display by typing the commands:
- trace off
- cst poll off
Then type the Cellular Service command :
cst modem sim
1.2.7.2.3. Using control API
#include "cellular_control_api.h"
/* API call to set modem in sim only mode. */
(void)cellular_disconnect();
1.2.7.3. Switch modem on with connection to network
This will switch on the modem with network activation.
1.2.7.3.1. At boot time
In the file plf_cellular_config.h
, change the value of the define PLF_CELLULAR_TARGET_STATE
to 2
:
#define PLF_CELLULAR_TARGET_STATE (2U)
1.2.7.3.2. Using console command
- Open a serial terminal and set the right parameters.
- Remove the trace display by typing the commands:
- trace off
- cst poll off
Then type the Cellular Service command :
cst modem connected
1.2.7.3.3. Using control API
#include "cellular_control_api.h"
/* API call to start and attach the modem. */
(void)cellular_connect();
1.2.7.4. Switch modem on without sim or network management
This will switch on the modem without sim access nor network activation. The modem is on, in standalone mode. Switch the modem to this state is only possible if the modem is off. If the modem is in any other state, switch the modem on without sim nor network management will have no effect.
1.2.7.4.1. Using console command
- Open a serial terminal and set the right parameters.
- Remove the trace display by typing the commands:
- trace off
- cst poll off
Then type these Cellular Service command :
The modem should be first shut off
cst modem off
then
cst modem on
1.2.7.4.2. Using control API
#include "cellular_control_api.h"
/* API call to stop the modem. Needed before to switch modem to on only state */
(void)cellular_modem_stop();
/* API call to start the modem in power on only. */
(void)cellular_modem_start();
1.2.7.5. Restart the modem
This will switch off, and then switch on the modem. When switch back on, the modem will be in connected mode, that is with sim access ans network activated.
1.2.7.5.1. Using console command
- Open a serial terminal and set the right parameters.
- Remove the trace display by typing the commands:
- trace off
- cst poll off
Then type the Cellular Service command :
cst modem restart
1.2.7.5.2. Using control API
Using control API, you may choose the sim only mode of the modem after restart. Just use cellular_disconnect()
instead of cellular_connect()
in the code bellow.
#include "cellular_control_api.h"
/* API call to stop the modem. */
(void)cellular_modem_stop();
/* API call to start and attach the modem. */
(void)cellular_connect();
1.2.8. How to modify network poling period
1.2.8.1. Stop polling
This will stop the poling of network signal.
1.2.8.1.1. Using console command
- Open a serial terminal and set the right parameters.
- Remove the trace display by typing the command :
- trace off
Then type the Cellular Service command :
cst polling off
1.2.8.1.2. Modifying define in include file
In plf_sw_config.h
modify the CST_MODEM_POLLING_PERIOD
define.
Stop polling :
#define CST_MODEM_POLLING_PERIOD (0U)
1.2.8.2. Set/change polling period
This will enable the poling of network signal according to a certain period.
1.2.8.2.1. Using console command
- Open a serial terminal and set the right parameters.
- Remove the trace display by typing the command :
- trace off
Then type the Cellular Service command to enable the polling with the period set in the code :
cst polling on
1.2.8.2.2. Modifying define in include file
In plf_sw_config.h
modify the CST_MODEM_POLLING_PERIOD
define.
set polling according a period of 15 seconds. The define value unit is milliseconds :
#define CST_MODEM_POLLING_PERIOD (15000U)
1.2.9. How to manage bearer/techno used
- Using a BG96 modem, techno/bearer used may be modified using console command or control API as describe below.
- Using a Type 1SC modem, techno/bearer used may be modified only using specific AT commands.
- Using a GM01Q modem, techno/bearer used may be modified only by reflashing a new firmware of the modem.
1.2.9.1. Force techno to use
1.2.9.1.1. Using console command
Only to use with BG96
- Open a serial terminal and set the right parameters.
- Remove the trace display by typing the command :
- trace off
Then type the Cellular Service command to set the wanted techno/bearer to be used :
cst techno on <Techno/bearer to use>
<Techno/bearer to use>
may be one of :
- 0 for GSM
- 1 for E UTRAN = cat M = cat M1
- 2 for E_UTRAN_NBS1 = cat NB1 = NB-IoT
1.2.9.1.2. Using control API
Only to use with BG96
Code example to set techno/bearer to use :
cellular_operator_selection_t my_operator_selection;
/* Get data */
cellular_get_operator(&my_operator_selection);
/* Set access techno is present */
my_operator_selection.access_techno_present = CA_ACT_PRESENT;
/* Set now the techno to use */
/* For GSM */
my_operator_selection.access_techno = CA_ACT_GSM;
/* For E UTRAN */
/* my_operator_selection.access_techno = CA_ACT_E_UTRAN */
/* For E UTRAN NBS1 */
/* my_operator_selection.access_techno = CA_ACT_E_UTRAN_NBS1 */
/* Save data */
(void)cellular_set_operator(&my_operator_selection);
/* Need to restart the modem for new techno/bearer to be taken into account */
/* API call to stop the modem. */
(void)cellular_modem_stop();
/* API call to start and attach the modem. */
(void)cellular_connect();
1.2.9.1.3. Using AT command
Only to use with Type 1SC
To set CATM :
at at%setacfg=radiom.config.preferred_rat_list,"CATM"
To set NBIOT :
at at%setacfg=radiom.config.preferred_rat_list,"NBIOT"
1.2.9.2. automatic techno selection
In this mode, you let the modem choose techno/bearer to use toward it's own policy. Available only for BG96 modem
1.2.9.2.1. Using console command
Only to use with BG96
- Open a serial terminal and set the right parameters.
- Remove the trace display by typing the command :
- trace off
Then type the Cellular Service command to set the wanted techno/bearer to be used :
cst techno off
1.2.9.2.2. Using control API
Only to use with BG96
Code example to set techno/bearer to use :
cellular_operator_selection_t my_operator_selection;
/* Get data */
cellular_get_operator(&my_operator_selection);
/* Set access techno is not present : automatic mode use*/
my_operator_selection.access_techno_present = CA_ACT_NOT_PRESENT;
/* Save data */
(void)cellular_set_operator(&my_operator_selection);
1.2.10. How to configure the modem radio band
- Open a Tera Term serial terminal and set the right parameters
- Start the firmware and select Modem power on option in the boot menu
- Type the modem command to get help of the modem configuration.
1.2.11. How to add FreeRTOS support to Azure RTOS package
The detailed information provided in this article allows users to add FreeRTOS support over Azure RTOS.
The main idea is to download an add-on and to apply it over XCC (based on Azure RTOS).
It adds all the required files to get Cellular using FreeRTOS / LwIP up & running.
Both X-CUBE-CELLULAR, delivery are based on Azure RTOS and XCC_FreeRTOS, add-on to add FreeRTOS support are available on www.st.com.
Once X-CUBE-CELLULAR is extracted, only Azure RTOS is available. To add new needed middlewares (FreeRTOS and LwIP) and FreeRTOS examples, users must extract XCC_FreeRTOS over X-CUBE-CELLULAR.
Thus, new middlewares, BSP for B-L462I-CELL1 board and FreeRTOS based "Demonstrations" are added. All Azure RTOS parts remain available.
1.2.12. How to setup iSIM for GMS01Q
There are two STMod+ boards with Monarch Sequans modem, one with GM01Q (the default in the X-CUBE-CELLULAR delivery) and one with GMS01Q.
The GMS01Q is a GM01Q with an iSIM.
To use GMS01Q, a small modification must be done in the source code, .h file.
The file to update is Projects\<board>\Demonstrations\<Demonstration name>\STM32_Cellular\Config\plf_cellular_config.h
With <board> = B-L4S5I-IOT01A or 32L496GDISCOVERY or STWINKT1 or ... according to the STM32 board with which you are working on.
With <Demonstration name> = Cellular, CellularIoT, Nx_TCP_Echo_Client ...
Patch the file as below and rebuild the binary.
- define PLF_CELLULAR_SIM_SLOT_NB (1U)
- define PLF_CELLULAR_SIM_INDEX_0 (2U) /*!< SIM SLOT 0 interface */
- define PLF_CELLULAR_SIM_INDEX_1 (99U) /*!< SIM SLOT 1 interface */
- define PLF_CELLULAR_SIM_INDEX_2 (99U) /*!< SIM SLOT 2 interface */
- define PLF_CELLULAR_SIM_INDEX_3 (99U) /*!< SIM SLOT 3 interface */
1.2.13. How to manage EEPROM on B-L462E-CELL1
The EEPROM is filled at factory process with some data, the main information is extracted from the modem, however a PSK automatically generated is also added. Thus, in case of needs to write the EEPROM, backup the parameters to restore them, specially the PSK first.
Below is the EEPROM first bytes structure (length is 274 bytes):
// Global parameters
uint8_t Board[20]; //={"B-L462-CELL1"};
uint8_t Version [20]; // Version FG displayed on sticker {"EBL462ECELL1$KU4"};
uint8_t Revision [20]; // Revision displayed on sticker {"MB1508-L462E-C01"};
uint8_t Serial[20]; // Serial number displayed on sticker {"K192700022"};
// Modem Related
uint8_t BaseBoard[20];//={"LBAD0XX1SE"};
uint8_t Brand[16]; //={"MURATA"};
uint8_t Model[16]; //={"ALT125X"}; // returned by AT+GMM
uint8_t ModemSoftRevNumber[30]; //={"RK_02_01_02_00_57"} // returned by AT+GMR
uint8_t IMEI[16]; // returned by AT+CGSN
uint8_t PSK[20]; // Pre shared Key - randomly generated
// eSim related
uint8_t eICCID[24]; // EMBEDDED SIM CHIP, returned by AT%CCID
uint8_t eIMSI[16]; // EMBEDDED SIM CHIP, returned by AT+CIMI
uint8_t EID [32]; ///262//270
uint32_t signature; ///266//274
Note that it is easy to read and write (using HAL services HAL_I2C_Mem_Read / HAL_I2C_Mem_Write) the EEPROM after calling the I2C initialization.
1.2.14. How to activate the eSIM with B-L462E-CELL1
Pre-requisite 1: check that the country where the board must run is covered by Truphone Network footprint. You can find the list of covered countries at Truphone Web[1].
Pre-requisite 2: activate the Truphone eSIM as described in the board user manual. To enable the eSIM with Truphone connectivity, users can follow the instructions provided in the B-L462E-CELL1[2] in the chapter eSIM.
This video[3] also shows the available user experience .
Depending on the version of the modem FW configuration, the network operator could be set to "DEFAULT". In some countries, the IMSI switch may not work as expected. To solve the issue, the modem firmware must be configured to use TRUPHONE as network operator. To do this, the end-user is asked to enter the at commands manually as follows:
Step 1: download the latest version of the X-CUBE-CELLULAR
Step 2: connect the device to a PC using the STLINK USB Port and program the binary \Projects\B-L462E-CELL1\Demonstrations\CellularIoT\Binaries\xxx.bin to the board.
The procedure to program the binary is defined in this How To article.
Step 3: start a terminal application on the PC in order to enter the commands to configure the device and also to read logs and traces.
Step 4: When the board boots up, check that the SIM card is successfully identified and CCID is automatically read and displayed on the terminal
AT%CCID<CR> <CR><LF> %CCID: 8944477700000005819<CR><LF> <CR><LF> OK<CR><LF>
Step 5: press the "return" key, the user sees prompt on the terminal as shown below $>
Step 6: enter the command "at at%nwoper?", the user sees the result below:
$>at at%nwoper? ATParser:*** SEND (size=11) *** at%nwoper?<CR> <CR><LF> %NWOPER: "TRUPHONE"<CR><LF> <CR><LF> <CR><LF> OK<CR><LF> $>
Step 7: If DEFAULT is shown instead of TRUPHONE then enter the AT command at at%nwoper="TRUPHONE" to force the modem firmware to use TRUPHONE configuration. This setting is persistent as it is stored in the modem flash memory.
$>at at%nwoper="TRUPHONE" ATParser:*** SEND (size=21) *** at%nwoper="TRUPHONE"<CR> <CR><LF> OK<CR><LF>
Step 8: verify that TRUPHONE is correctly written into the modem flash memory by reading the existing nwoper by entering again at at%nwoper. Verify that TRUPHONE is displayed.
Step 9: now Truphone as NWOPERator is set, the user can reboot the board by pressing the reset button (black button) or enter the reset command at the prompt
Step 10: after the restart, let the modem starts normally. It automatically searches network and register to Truphone network. It may take up to 10 to 15 minutes to find a network and register.
Step 11: if the registration is still not successful after the latter step, record the trace from the terminal and share it with ST support team via ST community.
1.2.15. How to use another modem
The aim is to change the current modem in an existing project with a new modem.
For example to replace BG96 with GM01Q in an IAR (EWARM) L496 project.
Custom files of all the supported modem are available in the package.
- Start IDE by double cliking on .eww (project file)
- In Drivers/BSP/X_STMOD_PLUS_MODEMS, remove BG96 group
- In Drivers/BSP/X_STMOD_PLUS_MODEMS, create a new group : GM01Q
- Select files for this newly created group, from Drivers/BSP/X_STMOD_PLUS_MODEMS/MONARCH/AT_modem_monarch/Src
- Change path in project options [ Options then C/C++ Compiler]
- Replace $PROJ_DIR$\..\..\..\..\..\Drivers\BSP\X_STMOD_PLUS_MODEMS\BG96\AT_modem_bg96\Inc
- By $PROJ_DIR$\..\..\..\..\..\Drivers\BSP\X_STMOD_PLUS_MODEMS\MONARCH\AT_modem_monarch\Inc
1.2.16. How to low power / power off device properly
To switch off device for low power you need first to power off the modem properly, and then change STM32 state to shutdown or standby.
step 1 : ask the modem to power off : make a call to cellular_modem_stop()
Beware that cellular_modem_stop()
is asynchronous. The function will return immediately, but the modem won't be powered off at that time. You need to pool modem state or register a callback to be notified of modem state change. Modem state value when modem is off is : CA_MODEM_POWER_OFF
. You need to check this value to be sure modem is off before to continue to power off the device.
step 2 - pooling case : Loop reading modem state value using cellular_get_cellular_info
, wait a bit (200 ms for example) till modem_state
is CA_MODEM_POWER_OFF
/* reads cellular info from cellular API */ cellular_get_cellular_info(&my_cellular_info); /* wait a bit */ (void)rtosalDelay(200); /* waiting for 10ms */
step 2 - callback case : register a callback using cellular_info_cb_registration
, and, within callback function code, check the value of the field modem_state
.
if (cellular_info_cb_registration(app_cellular_info_status_cb, (void *) NULL) != CELLULAR_SUCCESS) { /* Manage error */ }
In callback function app_cellular_info_status_cb
, check that modem_state
is CA_MODEM_POWER_OFF
. In that case, continue treatment in your app.
step 3 : Put STM32 in low consumption mode
1.3. How To applicable only to FreeRTOS version
1.3.1. How to change default behavior of the application
The delivered firmware starts Cellular_App application. The default behavior is that a single echo service is started. This service sends data to an Echo server which replies with the same data. Once an answer from Echo server is received, the echo client resends data to Echo server after a delay. A second instance of the Echo client can be started to test multiple socket configurations. The address of the Echo server can be changed. It is also possible to send a ping command while the Echo client is running. It is also possible to start a perfomance test. To see all the possibilities, type the following in the Tera Term: cellularapp help
1.3.2. How to implement your own application
The easiest way to implement your application is to adapt the Cellular_App content to your requirements.
Another method is to add a new entry task for this new application and start it from main (do not forget to remove entry task start for Cellular_App to avoid conflicts).
Your application is in charge of initializing and starting the Cellular middleware (for this, copy and paste the required lines from Cellular_App).
1.3.3. How to to select components to include in the cellular firmware
The firmware can be customized by adding or removing components or applications.
The configuration files under Projects\<board>\Demonstrations\Cellular\STM32_Cellular\Config allows the selection of the component to include in the cellular firmware by define/undefine environment variables (if using CellularApp overwrites configuration by changing the define in plf_cellular_app_config.h).
Refer to the user manual (UM2426) on how to customize the software.
1.4. How To applicable only to Azure RTOS version
1.4.1. How to implement your own application
Coming soon.
2. References
- ↑ Truphone Web
- ↑ user manual. User manual of the B-L462E-CELL1
- ↑ User experience video