Click here for Bluetooth® Low Energy Overview
1. General software architecture
The user can rely on multiple modules and SW blocks to create its application. The whole framework is called “Application Firmware Framework”. The architecture is designed over a 3-level organization:
- Application firmware
- Bluetooth® LE Stack
- Platform resources
1.1. Application Firmware
This is the user application. It is based on:
- IPs either from ST or from Third Party.
- Features developed by ST for short-range protocols, such as Bluetooth® LE profiles and so on.
- Utilities required by the application and the protocol stacks.
- Generic Utilities that provide easy access to basic features such as Low power management, Sequencer, etc.
1.2. Bluetooth® LE Stack
The Bluetooth® LE Stack is the main interface between the application and the hardware for Bluetooth® LE purposes. It is composed of two layers:
- Bluetooth® LE Host stack
- It manages all networks and transport protocols that allow the application to communicate with other devices. Provided by ST, it can also be substituted by the user own Host stack.
- Bluetooth® LE Controller
- The Bluetooth® LE Controller manages the hardware part, the RF state and guarantees that the RF protocol is correctly followed. It includes the physical layer, the link layer and the host controller Interface.
1.3. Platform Resources
The platform resources include all the HALs, BSPs and drivers that ease the platform hardware use.
2. Project architecture
2.1. Overview
The project organization differs a bit from the application architecture. This organization is more repository based and split in 4 different parts:
EWARM Project organization | |
---|---|
2.2. Application
Application is the core part of the project. It regroups all the main information and action that define the user application. This section is divided in sub-directories:
EWARM Project View | |
---|---|
|
2.3. Drivers
The drivers are divided into four components set:
- The hardware abstraction layer (HAL)
- This layer provides the hardware abstraction drivers and the hardware interfacing methods to interact with the upper layers (application, libraries, and stacks). The HAL is composed of:
- The HAL Drivers:
- A set of portable abstraction APIs based on high level services built around standalone processes. The HAL drivers are functionalities oriented, example: for the Timer peripheral, the APIs could be split into several categories following the functions offered by the IPs (Basic timer, capture, PWM …etc.).
- Low Layer Drivers:
- A set of basic drivers with direct hardware access with no standalone process, this layer can be called either by applications or by the HAL drivers.
- The HAL Core drivers:
- A set of internal drivers to provide low level operations to the “complex” peripherals like the USB and Ethernet. They all come with a dedicated source and header files. Some drivers may have an additional file containing extended features. Those files end with "_ex".
- The BSP Drivers
- This layer contains the high-level board services for the different functionalities offered by the hardware (LED, Push buttons, etc.) and the drivers for the external components mounted on the used boards (IO expander, etc.).
- CMSIS Drivers
- Cortex Microcontroller Software Interface Standard (CMSIS) drivers that provides a single standard across all Cortex-Mx processor series vendors. It enables code re-use and code sharing across software projects.
2.4. Middleware
Libraries and protocol-based components (Bluetooth® LE stack, etc.). It is in this directory that the user will find Bluetooth® LE services management, system commands, etc.
Horizontal interactions between the components of this layer shall be done directly by calling the features APIs while the vertical interaction with the low-level drivers shall be done through specific callbacks and static macros implemented in the library interface.
2.5. Utilities
Miscellaneous software utilities that provide additional system and media resources services like sequencer tools box, timeserver, low power manager, several trace utilities and standard Library services like, memory, string, timer, and math services.
Those utilities are not specific to one platform but available to a multitude of STM32 families.