How to start with DA access on STM32H503

Revision as of 17:58, 8 March 2023 by Registered User

How to start with DA access on STM32H503Clock.png45min

Target description

This tutorial shows how to make a provisioning and then a full regression on a STM32H503 device. Provisioning process goes through 3 steps :

  • Initial Option Bytes programming
  • Code image generation and flashing
  • Password provisioning

The last step shows a full regression.

Prerequisites

  • knowledge of STM32CubeProgrammer
  • knowledge of JTAG / SWD interface

Hardware

  • Nucleo MB1814 with STM32H503

Required tools

  • STM32CubeProgrammer[1] Software programming tool for STM32 (v2.13.0 min)
    • Including STM32TrustedPackageCreator
  • STM32Cube_FW_H5_V1.0.0 [2] or upper
  • IAR Embedded Workbench v9.20.1
  • Tera Term or equivalent UART Terminal emulator


Literature

  • UM2237 STM32CubeProgrammer software description
  • UM2238 STM32 Trusted Package Creator tool software description
  • AN5054 Secure programming using STM32CubeProgrammer
  • AN2606 STM32 microcontroller system memory boot mode


Environment setup

Before starting, the first step is to prepare the environment to be able to go through the DA process.


  • Download the STM32CubeH5 package and install it

A directory NUCLEO-H503RB is included in the Projects directory

Warning white.png Warning
Place STM32CubeH5 package close to the C: root to avoid long windows path.
SECURITY Path NUCLEOH503.png
Warning white.png Warning
In case the STM32CubeProgrammer has not been installed in the default folder, the customized installation paths need to be updated in the following script :NUCLEO-H503RB\ROT_Provisioning\env.bat
:: ==============================================================================
::                               General
:: ==============================================================================
:: Configure tools installation path
set stm32programmercli="C:\Program Files\STMicroelectronics\STM32Cube\STM32CubeProgrammer\bin\STM32_Programmer_CLI.exe"
set stm32tpccli="C:\Program Files\STMicroelectronics\STM32Cube\STM32CubeProgrammer\bin\STM32TrustedPackageCreator_CLI.exe"


1. STM32H503 device specific behaviors

STM32H503 devices are based on STM32H5x3 devices architecture without any Arm® TrustZone®.
In order to allow regression thanks debug authentication, the STM32H503 should be provisioned with a password.

The flash interface doesn't provide OBKeys --> OTP is used to provision password.

Warning white.png Warning
Once provisioned during the provisioning step, password can't be changed anymore. Password needs to be kept somewhere.

2. Provisioning

The provisioning could be done thank the script NUCLEO-H503RB\ROT_Provisioning\DA\provisioning.bat
This script will :

  • Set the option bytes of the device
  • Set a password to the board
  • Set the final chosen product state according user selection
SECURITY Provisioning Script for H503 OEMiROT.png


2.1. Provisioning - Step1 : Initial Option Bytes programming

  1. Connect the board
  2. Run the provided provisioning.bat script (double click)
  3. The script will proceed with the option byte programming
  • Remove all protections
  • Erase User Flash
Security ProvisioningScript Step1-1.png

2.2. Provisioning - Step2 : Code image generation and flashing

Once Option Bytes successful programmed, script ask to flash your application

Warning white.png Warning
Don't close the provisioning script window

Don't disconnect the board and follow next instructions

Security ProvisioningScript Step2.png


For this example we will use GPIO_IOToggle application located in : Projects\NUCLEO-H503RB\Examples\GPIO\GPIO_IOToggle\EWARM

Security Path GPIO IOToggle .png


  • Open the Project.eww located in the EWARM directory :Projects\NUCLEO-H503RB\Examples\GPIO\GPIO_IOToggle\EWARM
  • Perform Project --> Rebuild all
Security IAR RebuildAll.png
  • Once project correctly builded, select : Project --> Download --> Download active application to flash the code
Security IAR Download active app.png
  • Reset the board (black button) and the green led must now blink

2.3. Provisioning - Step3 : Password provisioning and final product state setting

2.3.1. Password not yet provisioned

Warning white.png Warning
If the password has already been provisioned please jump directly to 3.2 - Password already provisioned

On STM32H503 MCUs password is provisioned on OTP. Once provisioned it can't be changed anymore

  • Go back to provisioning script window and press a key to continue procedure
  • The script asks if Password is already provisioned.

Before answering "No" you have the possibility to update the default password in user_password.bin file.

SECURITY path Pwd.png

User_passord.bin : where you define the password (16 bytes) that will be provisioned

Board_password.bin : HASH of user password which will be provisioned in the chip

Password.bin : output file in order to open the DA access for regression


Board_password.bin and Password.bin files will be automatically updated with the new password saved in user_password.bin during provisioning script.

You can also continue script without updating the default password . Answer “No” to continue

Warning white.png Warning
The password can't be updated after this step
  • Follow the script and choose the product state (PROVISIONED or CLOSED )
Warning white.png Warning
Reminder that LOCKED is a definitive product step that can’t be changed anymore.

Make a first trial setting the product in PROVISIONED state :

Security ProvisioningScript ALLsteps1.png

--> the installed code must run and the led blink

ignore next paragraph 3.2 and jump directly to step4 : Full regression

2.3.2. Password already provisioned

Warning white.png Warning
if you already provisioned password jump directly to 4- Full Regression
  • Go back to provisioning script window and press a key to continue procedure.
  • The script asks if password is already provisioned.

Answer "Yes" to continue

  • Follow the script and choose the product state (PROVISIONED or CLOSED)
Warning white.png Warning
Reminder that LOCKED is a definitive product step that can’t be changed anymore.

Make a first trial setting the product in PROVISIONED state :

Security ProvisioningScript ALLsteps1-yES.png

--> the installed code must run and the led blink

Complete the tutorial till the end.

3. Full regression

  • A full regression will erase the user stored contents.
    • Erase the user flash content
    • Set the product in open state
  • If the product is in Open state, a full regression is not needed since the device is not secured and changes can be done without any authentication.

In case the regression script is executed, it will indicate some errors

  • If the product is not in Open state, the only way to change the product state is to first do a full regression

3.1. Full regression using the provided script

The regression can be done using the provided script or using CubeProgrammer (see 4.2)

SECURITY Regression Script for H503 OEMiROT.png

To perform a full regression

  • Launch the regression.bat script located in ROT_Provisioning\DA
  • If the regression has succeeded the following message should be displayed
    Security RegressionSuccess.png

Connect STM32CubeProgrammer and check that the flash content is well erased and that the option bytes and product state are at default values.

3.2. Full regression using STM32CubeProgrammer

  • Disconnect the CubeProgrammer, remove/plug the USB cable
  • Redo the exercise starting at step1, set the “CLOSED” state
  • Select Security DA icon.png in CubeProgrammer and select “Debug Authentication”
  • Click “Discover” the information window will be filled
SECURITY H503 device Discovery cmd CubeProgrammer.png
  • Enter the password.bin file
SECURITY H503 device password for regression CubeProgrammer.png
  • Click Full regression and you get this successfull message box :
Security DA Success Message w CubeProgrammer.png
  • Check with CubeProgrammer that the flash content is well erased and that the product state and option bytes are at default values thanks ST link SWD.

4. References

No categories assignedEdit