OEMiRoT STM32H5 How to Introduction

OEMiROT states for Original Equipment Manufacturer immutable Root of Trust. OEM-iROT can be developed by users in all STM32H5xx devices.


1. OEM-iROT services

OEM-iROT can provide the same services as ST-iROT but it is the user responsibility to develop his own Root of Trust firmware (OEM-iROT).

1) The Secure Boot (Root of Trust Services):
It is an immutable code, always executed after a system reset, that activates STM32 runtime protections and verifies the authenticity and integrity of the application code before every execution.
  • Integrity: to ensure that a firmware that is going to be executed has not been corrupted or maliciously modified.
  • Authenticity: to verify that a firmware is coming from a trusted and known source in order to prevent unauthorized entities to install and execute code.
2) The Secure Firmware Update:
It is an immutable code that detects if a new firmware image is available, checks its authenticity and verifies the integrity of the code before installing it after decryption.

2. OEM-iROT use cases

There are two possible cases explained below.

  • Case 1: The user application is executed after OEM-iROT

At each Reset the OEM-iROT firmware located in User Flash is first executed in HDPL1. It is the user responsibility to develop a root of trust firmware that

  • First checks authenticity and integrity of user application
  • Secondly jumps to the user application or Bootloader depending on the authenticity and integrity checks.


File:STiROT1.png
Figure 1. Case1 User application is executed after STiROT

After a successful check of authenticity and integrity of user application, OEM-iROT can jump directly in HDPL2 or HDPL3 (user application can be installed in HDPL2 or HDPL3). User Application can be a fully secure application, a full non secure application, or a combined secure/ non secure application. If parameters configured in User Root of Trust are not respected or if Authenticity and integrity checks fail, OEM-iROT executes Bootloader to download new user application and user data. It is the user’s responsibility to activate all the required security protections during the User Application execution.


  • Case 2: Two boot stage : The updatable Root of Trust (uROT) is executed after the OEM-iROT

The uROT is in the user flash and will act as a second boot stage adapted to customer requirements. The following figure shows the entry point after reset and the OEM-iROT controlling the step to uROT. OEM-iROT is the entry point executed after any reset. After a successful verification of the uRoT, OEM-iROT executes the uRoT in temporal isolation level 2 (HDPL2) and in secure mode.

The uRoT will then execute the secure user application (S-User app) after a successful verification in temporal isolation level 3 (HDPL3) and in secure mode. In case there is a verification failure of the uROT, OEM-iROT will execute the Bootloader to download a new uRoT code and/or data.


3. OEM-iROT provisioning steps

3.1. Step 1 - OEM-iROT and Debug Authentication configuration

STM32TrustedPackageCreator tool is used to generate OEM-iROT configuration file (.obk) based on template provided in STM32CubeH5 Software package. This configuration file generates keys that will be used to - Encrypt the User application and data - Check the authenticity of the user application and data

All other parameters are configured directly by the User in his Root of Trust firmware located in HDPL1 in User Flash. This code must be able to perform authenticity and integrity checks of the User application and data images. It also configures the number of User application and images: - Number of data image secure (0 or 1) - Number of data image non-secure (0 or 1) - Number of code image secure (0 or 1) - Number of code image non-secure (0 or 1) An example of user Root of trust firmware called OEMiROT_Boot is delivered in STM32CubeH5 firmware: Projects\STM32H573I-DK\Applications\ROT\OEMiROT_Boot. During the OEMiROT execution if the number of images is wrong Bootloader is launched to load new code and/or data images. STM32TrustedPackageCreator is also used to generate the Debug Authentication configuration file (.obk) based on template provided in STM32CubeH5 Software package. This file is used to configure the conditions to reopen a protected device and the debugger. Depending on the User application additional configuration files could be generated.

3.2. Step 2 – Code and data image generation

The signed and encrypted user application code image and user data image are generated with STM32TrustedPackageCreator. The user data are optional and chosen during the OEMiROT configuration. These images are downloaded in the user flash download area. Area location and size that are defined in the OEM-iROT_Boot code. After authenticity verification, the OEM-iROT decrypts the firmware code and data and will copy it in the execution slot. Execution slot location and size are defined in the OEM-iROT code.

3.2.1. User application code image generation

The user application code binary file can be generated by any IDE. STM32TrustedPackageCreator can be launched separately to generate the encrypted and signed image file using the same encryption and authenticity keys provisioned during the OEM-iROT configuration. The image creation can also be done automatically during the user application compilation. STM32TrustedPackageCreator is using a configuration file (OEMiRoT_S_Code_Image.xml and OEMiRoT_NS_Code_Image.xml) to generate images. A file example is available in the STM32Cube_FW and can be edited using STM32TrustedPackageCreator.

In the OEMiROT_Boot application, the application code download and execution area offsets are configured. it’s mandatory to recompile the OEMiROT_Boot code to generate the correct related user application code binary. The binary file is the input to generate the signed and encrypted image using STM32TrustedPackageCreator.

3.2.2. User Data Image generation

STM32TrustedPackageCreator needs to be launched separately to generate the encrypted and signed image file using the same encryption and authenticity keys provisioned during the OEMiROT configuration. These keys are also used for the user application code image generation. In OEMiROT_Boot firmware, User determines the user data download and installation area offsets . STM32TrustedPackageCreator is using a configuration file (OEMiRoT_S_Data_Image.xml and OEMiRoT_NS_Data_Image.xml) A file example is available in the STM32Cube_FW that can be edited using STM32TrustedPackageCreator .


3.3. Step 3 – Product state setting and device provisioning

During this step:

  • The static security protection, the secure area definition and the boot address in User Flash, shall be configured
  • Product state is changed to “PROVISIONING” and configuration data are flashed into OB keys
  • Final product (“PROVISIONED”, “TZ_CLOSED”, “CLOSED” or “LOCKED”) is set. To protect the complete product including the User Application the final product state should be “CLOSED” or “LOCKED”.

For this TOE configuration, the static security protection script will include the configuration of the following option bytes:

  • TrustZone activation (TZEN): enable
  • Secure area definition (SECWM1, SECWM2): depends on the User Application configuration
  • Secure boot address (SECBOOTADD): depends on the User Application configuration
  • Lock secure boot address (SECBOOTLOCK): 0xB4
  • Memory Boot (BOOT_UBE): User Flash
  • Product state (PRODUCT_STATE): at least “Provisioned”