STM32WBA Bluetooth® LE – Data Throughput Measurement

Revision as of 15:51, 9 February 2023 by Registered User (→‎How to use)

1. Data Throughput

Data Throughput applications (BLE_DataThroughput_Client and BLE_DataThroughput_Server) are proprietary applications used to measure the throughput between devices according to different parameters, 1M or 2M PHY, different connection intervals.

The Data Throughput Server is the device exposing three characteristics to be controlled by the remote client​

  • Characteristics DATA_TRANSFER_TX (Notification) to notify data from Server TO Client​
  • Characteristics DATA_TRANSFER_RX (Write) to Send data from Client TO Server​
  • Characteristics DATA_TRANSFER_TX_RX_INFO (Notification) to notify throughput measurement of data received

The Central & GATT Client Collector can be three different applications​

  • Data Throughput Client to measure performances between 2 STM32WBA devices​
  • Smartphone ST BLE Toolbox to performs Smartphone benchmarking​
  • Web Bluetooth Interface to use laptop

This wiki page is the description of the Data throughput project provided within the STM32CubeWBA MCU Package[1]

Bluetooth® LE Data Throughput project & STM32WBA


The table below describes the structure of Data Throughput service:

Bluetooth® LE Data Throughput Service specification
Service Characteristic Mode UUID size
Data Throughput Service 0xFE80-cc7a-482a-984a-7f2ed5b3e58f
Data Transfer TX Notify 0xFE81-8e22-4541-9d4c-21edae82ed19 255
Data Transfer RX Write W/o Response 0xFE82-8e22-4541-9d4c-21edae82ed19 255
Data Transfer TX RX INFO Notify 0xFE83-8e22-4541-9d4c-21edae82ed19 255


Example 1 of flow diagram between a Data Throughput server (STM32WBA) & a Client Collector


Example 2 of flow diagram between a Data Throughput server (STM32WBA) & a Client Collector


1.1. STMicrolectronics Manufacturer Advertising Data

Data Throughput Sensor STMicroelectronics Manufacturer Advertising data
0 1 2-3 4 5 6 7 8 9 10-15
Length Manufacturer ID Company BlueSTSDK Version Device ID Firmware ID Option 1 Option 2 Option 3 Device Address
DT Sensor 0x0F 0xFF 0x0030 STMicro 0x02 0x8B Nucleo-WBA 0x88 - DT Sensor 0x00 0x00 0x00 0x08E12Axxxx


1.2. On board buttons configuration

DT Sensor Application Nucleo-WBA buttons configuration
Application Condition B1 Click B1 Long Press B2 Click B2 Long Press B3 Click B3 Long Press
DT Sensor

Idle
Connected


Starts/Stops notification

Clear Sec db

L2CAP CONN REQ


Toggle PHY (1M/2M)


2. Requirements

2.1. Software and system requirements

The software required are the following (minimum IDEs version):

  • IAR Embedded Workbench for ARM (EWARM) toolchain V9.20.1
  • RealView Microcontroller Development Kit (MDK-ARM) toolchain V??
  • STM32CubeIDE toolchain V?? [2].


Programmer:

  • STM32CubeProgrammer[3] : To flash the board with an already generated binary

2.2. Hardware requirements

NUCLEO-WBA5 [4] is necessary to install the application.

Hardware platform illustration
Nucleo-WBA5


2.3. Collector applications compatible

The STM32CubeWBA Data Throughput Sensor project is compatible with the following collector:

3. STM32WBA Data Throughput Server example description

3.1. Project directory

The "BLE_DataThroughput_Server" application is available by downloading STM32CubeWBA MCU Package[5].

Data Throughput Server project directory

3.2. Project description

3.2.1. Structure

Software project structure with the most important parts:

Data Throughput Server project structure
Connectivity WBA HeartRate Archi.png
Connectivity yellow box.png
Main applicative part files
Connectivity dark blue box.png
Services management
Connectivity green box.png
BLE libraries
Connectivity pink box.png
Link Layer System integration files

WARNING: Do not modify the files in Middlewares folder


3.2.2. Application initialization

The different steps of the application initialization are described below:

Data Throughput Server project initialization
puce1.png
  • Initialize the system (HAL, Clock, Power Mode, RTC IP, Timer Server)
  • Infinite loop for run mode
puce2.png
  • Initialize the BSP (LEDs, buttons…), Transport Layer Interface, Debugger
  • Wait for initialization done
puce3.png
  • Initialize the Bluetooth® LE App – GAP level
  • Manage GAP events (advertising,scanning)
puce4.png
  • Initialize the Bluetooth® LE App – GATT level
  • Initialize the Bluetooth® LE Stack
  • Manage GATT events
puce5.png
  • Register Event Handler
  • Initialize and manages services
  • Update characteristic
puce6.png
  • Initialize the context
  • Manage Data Throughput Service notification

3.2.3. GAP and GATT initialization and interaction

puce3.png

The Bluetooth LE Data Throughput Server application initialization is done within app_ble.c

  • Start the BLE stack - initialize the device as peripheral - configure and start advertising: ADV parameters, local name, UUID - APP_BLE_init()
  • Call the services controller initialization SVCCTL_Init() - svc_ctl.c
  • Manage the GAP event - SVCCTL_App_Notification()
    • EVT_LE_CONN_COMPLETE - provides information of the connection interval, slave latency, supervision timeout
    • EVT_LE_CONN_UPDATE_COMPLETE - provides the new information of the connection
    • EVT_DISCONN_COMPLETE - informs the application about the link disconnection and the reason
    • EVT_ENCRYPT_CHANGE - informs the application weather the link is encrypted
puce4.png

The Services management is done by the service controller - svc_ctl.c

  • Call the Initialization function of all the developed services - SVCCTL_SvcInit()
    • Data Throughput Service - DT_SERV_Init() - dt_serv.c
  • Register Services Event Handler - SVCCTL_RegisterSvcHandler(...)
  • Manage events - SVCCTL_UserEvtRx ()- from the BLE Host Stack and redirect them to the services registered - DT_SERV_EventHandler() - or gap event handler - SVCCTL_App_Notification
puce5.png

The Data Throughput Service dt_serv.c manages the specification of the service:

  • Service Init - DT_SERV_Init()
    • Register Data Throughput Event Handle to Service Controller - SVCCTL_RegisterSvcHandler(DT_SERV_EventHandler);
    • Initialize Service UUID – add Data Throughput service as Primary services

TBU

  • Update Data Throughput DT_SERV_THROUGH measurement characteristic - DT_SERV_UpdateValue()
  • Update Data Throughput DT_SERV_TX characteristic Value - DT_SERV_UpdateValue()
  • Manage the GATT event from BLE Stack - DT_SERV_EventHandler()
    • ACI_GATT_ATTRIBUTE_MODIFIED_VSEVT_CODE
      • Reception of a Write Command: DT_SERV_RX Characteristic Value
    • ACI_GATT_ATTRIBUTE_MODIFIED_VSEVT_CODE
      • Reception of an attribute modification - DT_SERV_TX Value : ENABLE or DISABLE Notification
      • Reception of an attribute modification - DT_SERV_THROUGH Value : ENABLE or DISABLE Notification
        • Notify application of the Transmitted Data - DT_SERV_Notification(DT_SERV_TX_CHAR)
        • Notify application of the Received Data - DT_SERV_Notification(DT_SERV_THROUGH_CHAR)
Data Throughput Server software module interaction


puce6.png

The application level of the Data Throughput Server is done with dt_serv_app.c:

  • Initialization of the context of the application
    • TBC
    • TBC
  • Receive notification from the Data Throughput Service - DT_SERV_Notification()
  • When Data Throughput TX characteristic is enabled by the remote, data are sent continuously DT_SERV_UpdateValue(DT_SERV_TX_CHAR)
  • When Data Throughput THROUGH characteristic is enabled by the remote, on reception of data (DT_SERV_RX_CHAR) the calculation of received data is done and sent every second DT_SERV_UpdateValue(DT_SERV_THROUGH_CHAR)

3.3. Build and install

Follow the steps described in Bluetooth® LE Build and Install Application page, applying them for STM32WBA BLE_DataThroughput_Server project.

3.4. How to use

Once the BLE Data Throughput Server application is installed on the STM32WBA platform, launch ST BLE ToolBox smartphone application. Then, scan and connect the device called DT_XX (where XX is replaced by the last byte of the BD address) to the application.
Once the Bluetooth® LE connection is established and the notifications enabled by the smartphone:

  • Pressing B1 while connected allows to start/stop sending of data through notification
  • Pressing B2 while not connected allows to clear the security database
  • Pressing B2 while connected allows to update the connection interval

With the WBA5x.Nucleo board, it is also possible to change RF PHY modulation

  • Pressing B3 while connected allows to switch between 2 Mbits and 1 Mbits PHY

3.5. UART debug trace

4. STM32WBA Data Throughput Client example description

4.1. Project directory

The "BLE_DataThroughput_Client" application is available by downloading STM32CubeWBA MCU Package[5].

Data Throughput Client project directory

4.2. Project description

4.2.1. Structure

Software project structure with the most important parts:

Data Throughput Client project structure
Connectivity WBA HeartRate Archi.png
Connectivity yellow box.png
Main applicative part files
Connectivity dark blue box.png
Services management
Connectivity green box.png
BLE libraries
Connectivity pink box.png
Link Layer System integration files

WARNING: Do not modify the files in Middlewares folder


4.2.2. Application initialization

The different steps of the application initialization are described below:

4.2.3. GAP and GATT initialization and interaction

4.3. Build and install

Follow the steps described in Bluetooth® LE Build and Install Application page, applying them for STM32WBA BLE_DataThroughput_Client project.

4.4. How to use

Install the BLE Data Throughput Client application on one STM32WBA platform.
Install the BLE Data Throughput Server application on other STM32WBA platform.

  • Pressing B1 while not connected scans and connects to Data Throughput Server device, enables all notifications.
  • Pressing B1 while connected allows to start/stop the sending of data through write w/o response

BLE Data Throughput Client application supports the pairing procedure

  • Pressing B2 while not connected allows to clear the security database
  • Pressing B2 while connected allows to request pairing

With the WBA5x.Nucleo board, it is also possible to change RF PHY modulation

  • Pressing B3 while connected allows to switch between 2 Mbits and 1 Mbits PHY

4.5. UART debug trace