![]() |
Coming soon |
1. What is AI at the edge
Smart objects are changing nearly every aspect of our daily lives, helping in our homes, workplaces, cities and factories. ST has been investing in AI for many years, recognizing that microcontrollers provide enough processing power to run AI software on smart objects and enable AI on the edge.
Local processing fixes many problems met when running AI algorithms purely in the Cloud:
- Latency and high communication costs on connected devices
- Reliability in case of limited network bandwidth or connectivity loss
- Power efficiency on battery-operated devices, as high-bandwidth connectivity requires large device batteries, leading to a rise in cost
- Data privacy since data is transformed locally and doesn't require to send all monitored data over the internet where security breach may occur during transmission or at Cloud storage
To simplify the development of AI algorithms on STM32, ST has developed a solution called STM32Cube.AI.
2. STM32Cube.AI overview
STM32Cube.AI solution brings the following:
- A CubeMX extension called X-CUBE-AI to convert an Neural Network in optimized code for STM32.
- Software examples on ST development hardware boards are available for quick prototyping:
- Audio and motion sensing with the FP-AI-SENSING1 function pack supported on the following development boards:
- Bluetooth low energy expansion board X-NUCLEOIDB05A1 + Motion MEMS and environmental sensor expansion board X-NUCLEOIKS01A2 + STM32 Nucleo-64 development board with STM32L476RG MCU NUCLEO-L476RG
- SensorTile development kit STEVALSTLKT01V1
- Multisensor kit with portable sensor box and smart sensor app STEVALMKSBOX1V1
- STM32L4 Discovery kit IoT node B-L475EIOT01A
- Vision with the FP-AI-VISION1 function pack for MCUs supported on the following development board:
- STM32H747I-DISCO Discovery board connected to the STM32F4DIS-CAM camera daughterboard
- Vision on Linux for PU with the X-LINUX-AI-CV expansion pack supported on the following development board:
- Discovery kit with STM32MP157C MPU STM32MP157C-DK2 with a USB camera
- Evaluation board with STM32MP157A MPU STM32MP157A-EV1
- Evaluation board with STM32MP157C MPU STM32MP157C-EV1 with their built-in camera module
- Avenger96 board from Linaro™ 96Boards based on the STM32MP157A microprocessor, either with a USB
- Audio and motion sensing with the FP-AI-SENSING1 function pack supported on the following development boards:
camera or the DesignCore® OV5640 camera mezzanine board from D3 Engineering
- STM32 community with dedicated neural networks topic
- AI Partner Program that brings expertise in Machine Learning and STM32 solutions
Check our list of resources for detailed information.
4. STM32 supported by STM32Cube.AI
STM32Cube.AI supports all ARM® Cortex®-M4 and Cortex®-M7 based MCUs, as well as STM32 MP1. Other MCUs are supported in our partner ecosystem or can be added on-demand.
STM32Cube.AI supports the following deep learning frameworks:
Supported versions and layers for each framework are detailed in X-CUBE-AI release note. This documentation is available in X-CUBE-AI local installation folder at this location:
STM32Cube/Repository/Packs/STMicroelectronics/X-CUBE-AI/5.0.0/Documentation/faqs.html
5. X-CUBE-AI overview
X-CUBE-AI is a tool provided to help customers to:
- Generate STM32 code from a python neural network described in supported AI frameworks. It supports quantization scheme and optimizations for STM32, reducing memory requirement by 4 and decreasing latency and power consumption by 3.
- Analyze the network and see if it fits on the target
- Validate the generated C code on the PC or on the target against the original model
It is available through STM32CubeMX Graphical User Interface, or via Command Line Interface.
Software requirements
Supported operating systems and architectures
- Windows 10 64-bit (x64)
- Linux (tested on RedHat, Fedora and Ubuntu 16.04) 64 bits
- macOS (minimum version High Sierra)
Prerequisite
- STM32CubeMX: 5.1.0 or higher is required
License
STM32CubeMX and X-CUBE-AI extension are delivered under the Mix Ultimate Liberty+OSS+3rd-party V1 software license agreement SLA0048.
6. STMicroelectronics Resources
All resources are gathered on STM32Cube.AI web page.
7. How to and Examples
- Getting started with X-CUBE-AI Expansion Package for Artificial Intelligence (AI)
- How to integrate Cube.AI generated code in OpenMV ecosystem
8. References