STM32WB-WBA GATT Data Base and bonded devices information storage

Revision as of 10:28, 6 September 2022 by Registered User (→‎Example 4 - FULL_GATTDB_NVM flag)
Under construction.png Coming soon

1. STM32WB - BLE GATT DB SRAM computation

Maximum size of SRAM allocation for the GATT database cannot be changed by the user's FW and varies for different stacks.

Calculation of the Max size allocated for GATT Data Base in SRAM is done in M0.

Max size table
Light Extended Full Full+Thread
WB55 10.5 kB 10.5 kB 10.5 kB 4 kB
WB15 2.6 kB 2.7 kB 2.7 kB Not supported


The limitation for number of services and number of attributes follows the rule:
(number of services) x 48 + (number of attributes) x 40 + CFG_BLE_ATT_VALUE_ARRAY_SIZE < Max size

To apply the limitation, it is necessary to calculate the number of services, the number of attributes and the attribute value array size.

1.1. How to calculate CFG_BLE_NUM_GATT_SERVICES ?

CFG_BLE_NUM_GATT_SERVICES defines the number of services to be stored in the GATT database.
Note that the default GAP and GATT services are automatically added at initialization.
The parameter CFG_BLE_NUM_GATT_SERVICES must be the number of user services increased by 2 (number of default GAP and GATT services).
CFG_BLE_NUM_GATT_SERVICES = 2 + number of user's services

1.2. How to calculate CFG_BLE_NUM_GATT_ATTRIBUTES ?

CFG_BLE_NUM_GATT_ATTRIBUTES defines the number of attribute records related to all the characteristics for the specific user's Bluetooth® Low Energy application.

For each characteristic:
The number of attribute records goes from 2 to 5 depending on the characteristic properties:

  • Minimum of 2 (1 for declaration and 1 for the value)
  • Add 1 more record for each additional property: Notify or Indicate, Broadcast, Extended property
    • Notify and Indicate properties correspond to CCCD (Client Characteristic Configuration Descriptor)
    • Broadcast property corresponds to SCCD (Server Characteristic Configuration Descriptor)

The parameter CFG_BLE_NUM_GATT_ATTRIBUTES must be the number of user's application attributes increased by 9 (the number of attributes of GAP and GATT default services)

CFG_BLE_NUM_GATT_ATTRIBUTES = <number of SCCD attributes for default GAP and GATT services> + 9 + number of user's attributes

Attributes of default GAP and GATT services (number = 9)


Example of DIS service

Attributes of DIS service


Example of service including characteristics with notification

Attributes of service including characteristics with notification


1.3. How to calculate CFG_BLE_ATT_VALUE_ARRAY_SIZE ?

CFG_BLE_ATT_VALUE_ARRAY_SIZE defines the size of the storage area for the attribute values.

Each characteristic contributes to the Attribute Value Array Size as follow:
Characteristic value length plus:
5 bytes if characteristic UUID is 16 bits
19 bytes if characteristic UUID is 128 bits
2 bytes if characteristic has a server configuration descriptor
2 bytes * CFG_BLE_NUM_LINK if the characteristic has a client configuration descriptor
2 bytes if the characteristic has extended properties

Each descriptor contributes to the Attribute Value Array Size value as follows:
– Descriptor length

And it is necessary to add characteristics related to the default GAP and GATT services:

  • GATT - Service change characteristic (if not removed): 9 bytes (5+2+2), 5 for UUID, 2 for indicate, 2 for characteristic value length
  • GAP - Device Name: 11 bytes (5+6), 5 for UUID, 6 for name length
  • GAP - Appearance: 7 bytes (5+2), 5 for UUID, 2 for attribute length
  • GAP - Peripheral Preferred Connection Parameters: 13 bytes (5+8), 5 for UUID, 8 for attribute length
Attribute Value Array Size of default GAP and GATT services


For this case default value array size: 9 + 31 = 40 bytes

Example of DIS service - Attribute Value Array Size

Attribute Value Array Size of DIS service


Example of service including characteristics with notification - Attribute Value Array Size

Attribute Value Array Size of service including characteristics with notification


2. STM32WB - BLE GATT DB and security record in NVM

2.1. BLE GATT DB record in NVM - FULL_GATTDB_NVM flag

The GATT DB record in NVM is composed:

  • Per service:
    • 2 bytes for handle
    • 3 bytes if 16-bit UUID or 17 bytes if 128-bit UUID
  • Per characteristic attribute:
    • 2 bytes for handle
    • 3 bytes if 16-bit UUID or 17 bytes if 128-bit UUID
    • 2 bytes for CCCD value (only if the attribute is a CCCD)

The total corresponds to size_of_gatt record. The security record in NVM is fixed and equal to 80 bytes, corresponding to size_of_sec record.

2.2. BLE GATT DB record in NVM - REDUC_GATTDB_NVM and NO_SVC_CHANGE_DESC flags

The GATT record in NVM is composed:

  • Per characteristic attribute:
    • 2 bytes for CCCD value (only if the attribute is a CCCD)

This is size_of_gatt record.

2.3. BLE GATT DB record in NVM - REDUC_GATTDB_NVM and WITH_SVC_CHANGE_DESC flags

The GATT record in NVM is composed:

  • Per characteristic attribute:
    • 2 bytes for CCCD value (only if the attribute is a CCCD)

+ 16 bytes (The DB hash characteristic stores a 128 bits value calculated from the DB structure.
Any change in the DB structure results in a different hash value.)

This is size_of_gatt record.

2.4. BLE security record

The security record in NVM is fixed and equal to 80 bytes, corresponding to size_of_sec record.

3. STM32WB - BLE number of bonded devices in NVM

Regarding the size of NVM, the computation of number n of bonded devices that can be stored in NVM is the following:

n = (total_size_of_nvm-1) / [ (size_of_sec_record+1) + (size_of_gatt record+1) ]

total_size_of_nvm = 2028 bytes (fixed in M0)
size_of_sec_record =  80 bytes (this is a constant from the BLE stack)
size_of_gatt_record is dependent of the flags chosen in the application in app_conf.h file.
See the description in previous point.

3.1. Example 1 - FULL_GATTDB_NVM flag

Default GATT configuration without adding services:

GATT record = 40 bytes

3.2. Example 2 - FULL_GATTDB_NVM flag

Default GATT configuration + 1 empty service with UUID_16

GATT record = 45 bytes
40 bytes for default + 5 bytes for the service

3.3. Example 3 - FULL_GATTDB_NVM flag

Default GATT configuration + 1 service with UUID_16 + 1 characteristic with UUID_16

GATT record = 62 bytes
40 bytes for default + 5 bytes for the service + 5 bytes for the 1st characteristic attribute + 5 bytes for the 2nd characteristic attribute + 7 bytes for the 3rd characteristic attribute (CCCD)

3.4. Example 4 - FULL_GATTDB_NVM flag

Example 4 - FULL_GATTDB_NVM flag


Formula to calculate Total Buffer Gatt Size

(number of services) x 48 + (number of attributes) x 40 + CFG_BLE_ATT_VALUE_ARRAY_SIZE
= 6 x 48 + 64 x 40 + 614
= 3462 bytes
In previous example, size_of_gatt record in SRAM is equal to 3462 bytes
And size of gatt record in NVM is equal to 435 bytes.

Formula to calculate the number of bonded devices that can be stored in NVM

n = (total_size_of_nvm-1) / [ (size_of_sec_record+1) + (size_of_gatt record+1) ]
n = ((507x4)-1) / [(80+1) + (435+1)] = 3

3.5. General information concerning NVM

We don’t store values of attributes, only the CCCD value.

it is applicable for GATT server only.

On server side it is used to: - check if services have changed - keep CCCD in memory

3.6. References