This message will disappear after all relevant tasks have been resolved.
Semantic MediaWiki
There are 1 incomplete or pending task to finish installation of Semantic MediaWiki. An administrator or user with sufficient rights can complete it. This should be done before adding new data to avoid inconsistencies.![]() |
Coming soon |
1. STM32WB - Bluetooth® Low Energy (BLE) Filter Accept List
1.1. From advertiser point of view
As soon as a device advertises with the parameter "allow scan request - allow connect request from devices in white list"
(use of aci_gap_set_undirected_connectable, advertising filter policy = 0x03)
No HCI_LE_ADVERTISING_REPORT events are sent by the device but it answers to SCAN_REQ.
1.2. For advertiser and scanner
To add a device in white list, devices need to be bonded. To get the address of the bonded device: use of aci_gap_get_bonded_devices thanks to which we get the number of bonded devices, address types and addresses of bonded devices. Then use aci_gap_configure_whitelist. The whitelist is written in RAM.
1.3. For scanner
An other possibility is to use for connection: aci_gap_start_auto_connection_establish_proc aci_gap_start_selective_connection_establish_proc
1.3.1. Add a device in White List: Phase 1
1.3.2. Add a device in White List: Phase 2