This message will disappear after all relevant tasks have been resolved.
Semantic MediaWiki
There are 1 incomplete or pending task to finish installation of Semantic MediaWiki. An administrator or user with sufficient rights can complete it. This should be done before adding new data to avoid inconsistencies.STM32 Advance USB type-C only Source
1. Target description
This tutorial will help you to: - Use the X-NUCLEO-SRC1M1 shield that includes a TCPP02-M18 protection circuit and provides a USB Type-C© connector - Create a USB legacy 3A @ 5V source application with the NUCLEO-F446RE board that does not include any USBPD peripheral and the X-NUCLEO-SRC1M1 shield using STM32CubeIDE software
2. Prerequisites
- Computer with Windows 7 (or higher)
3. Hardware
- NUCLEO-F446RE (tested on rev C-04) - X-NUCLEO-SRC1M1 shield - A USB sink device to test our USB source device
4. Software
- STM32CubeIDE (tested with V1.8.0) - X-CUBE-TCPP MCU Firmware Package (BSP)
5. Literature
- UM1724 NUCLEO-F446RE User Manual - UM2973 X-NUCLEO-SRC1M1 User Manual
Create a USB Legacy 3A @ 5V Source Device
Total 60min