![]() |
Coming soon |
This page contains information such as, application examples, document references, and tips related to STM32 LoraWan®.
1. LoRaWAN® overview
1.1. What is LoRaWAN® ?
This section provides a general overview of LoRaWAN® , particularly focusing on the LoRaWAN® end device. LoRaWAN® is a type of wireless telecommunication network designed to allow long-range communication (kilometers) at a very low bit rate (suitable for transmitting small size payloads like sensor data) and enabling long-life battery-operated sensors and actuators (they can last up to 10 years on a single coin cell battery).
Classical use case is for smart farms to measure soil moisture in rural areas, but thanks to the deep indoor penetration (e.g. easily cover multi floor buildings) it is used also for indoor application.
It can be deployed on public network as on private network (saving fees).
LoRaWAN® defines the communication and security protocol ensuring interoperability with the LoRaWAN® network.
The secure communication between the end device and the application server uses AES-128 encryption.
The authenticity and integrity of messages between the end device and the network server uses AES-CMAC (Cipher-based Message Authentication Code).
Often in LoRaWAN® literature "Message Authentication Code" is called MIC (Message Integrity Code) because MAC acronymous is used for "Media Access Control".
By a technical point of view LoRaWAN® is a MAC (Media Access Control) layer protocol built on top of LoRaTM modulation.
LoRaTM (from "long range") is a proprietary low-power wide-area network (LPWAN) modulation technology based on spread-spectrum modulation techniques that is similar to and a derivative of chirp spread spectrum (CSS) modulation. It was developed by Cycleo, later acquired by Semtech.
LoRaTM can be operated on the license free sub-gigahertz bands, like EU433 (433.05-434.79 MHz) and EU863-870 (863–870/873 MHz) in Europe, US902-928 (902–928 MHz) in North America, and so on for other countries and continents. It also can be operated on 2.4 GHz worldwide.
That explains why private network can be implemented.
LoRaWAN® is a software layer which defines how devices use the LoRaTM hardware, or better to call it protocol which defines the communication rules from the format of the messages to the network architecture and security aspects.
LoRaWAN® message types are used to transport MAC commands and application data. They can be uplink and downlink. Message types depends on the specification’s versions 1.0.x and 1.1.
The LoRaWAN® protocol is developed and maintained by the LoRa Alliance® .
As announced by the LoRa Alliance® on December 7, 2021, LoRaWAN® is officially approved as a standard for Low Power Wide Area Networking (LPWAN) by the International Telecommunication Union (ITU). The LoRa Alliance® certification program certifies end devices and provides end-users with confidence that the devices are reliable and compliant with the LoRaWAN® specification.
The LoRaWAN® device classes are defined in the table below.
Class name | Intended usage |
---|---|
A - All |
|
B - Beacon |
|
C - Continuous |
|
All LoRaWAN® devices must implement Class A, whereas Class B and Class C are extensions to the specification of Class A devices.
1.2. LoRaWAN® Network architecture
The LoRaWAN® network is structured in a star of stars topology, where the end devices are connected via a single LoRaWAN® link to one gateway.
Note: While the physical layer of LoRa® is proprietary, the rest of the protocol stack (LoRaWAN® ) is kept open and its development is carried out by the LoRa Alliance® .
The STM32WL series[1] is the ideal MCU family for developing Long Range sub-gigahertz application such sensors and transmit information to central devices.
1.3. LoRaWAN® Gateway
A Gateway is required in a LoraWan Network. It is the interface bettwen LoraWan End Device and the Cloud. A Gateway is basically converting Lora ® packet from/into an udp packet to the cloud.
- P-NUCLEO-LRWAN2: STM32 Nucleo pack LoRa™ HF band sensor and gateway
- P-NUCLEO-LRWAN3: STM32 Nucleo pack LoRa™ LF band sensor and gateway
- STM32MP1+RAK Gateway
Other Gateway:
And many more exists out there!
1.4. LoRaWAN® Network Server
- Loriot
- TTN
- Actility
2. Wiki LoraWan®: pages breakdown
STM offers different devices and hardware tools to evaluate and develop a LoraWan® End-Device. STMicrolectronics LoRaWAN Products are shown here here. The choice depends on the customer constraint and AN5408: Migrating from STM32L0, STM32L1, and STM32L4 Series associated with SX12xx transceivers to STM32WL Series microcontrollers can help customer to choose.
- STM32WL Ecosystem
- Cube Software setup
- Hardware setup
3. Getting started with STM32WL Series and LoRaWAN®
The device architecture leverage state-of-the art STM32 ultra-low-power process node and is available from 64KB up to 256KB of Flash memory and up to 256 KB of SRAM.
Various packages are available: UQFN48, BGA73.
The evaluation board is the NUCLEO-WL55JC integrating stm32wlxx, ST link, LEDs, Buttons and a Arduino connector.
The Nucleo exists in 2 frequency bands:
Nucleo Reference | Description |
---|---|
NUCLEO-WL55JC1 | High Band |
NUCLEO-WL55JC2 | LowBand |
On the software side, the STM32CubeWL MCU Package[2] provides a software solution to allow customers to quickly and easily develop their own firmware thanks to:
- several LoRaWan® certified applications
- several Radio Application
THe STM32CubeWL Software Package can also be found on Github here
4. STM32WL learning center
4.1. STM32WL LoRaWAN®
This training set introduces the STM32WL and ecosystem
4.2. STM32WL MOOC (massive online courses)
LPWAN theory
Learn main principles concerning LPWAN protocols
STM32CubeMonitor: how to perform RF functional tests on STM32WL MOOC
Learn basic principles concerning STM32WL55 RF parameters monitoring using STM32CubeMonitor
STM32WL security MOOC
Learn main principles concerning security within STM32WL family and LoRaWAN
STM32WL Lora Guide
Learn how to setup a LoRaWAN Network using a STM32WL with a LoraWan-EndNode including environmental and motion sensors
5. STM32WL software application notes and user manuals
6. STM32WL hardware guidance
7. Specific tools
- STM32CubeMonitor - Software tool to test the RF performance of STM32-based hardware devices
- STM32CubeMX - STM32Cube initialization code generator
- STM32CubeProgrammer - Software Programmer for all STM32
- STM32PowerShield - Power and Analyze current consumption
8. References
9. LoraWan Alliance
https://lora-alliance.org/ lorawan-certification
10. Frequently Asked Questions
- Numbered list item
11. The ST Blog
12. Terms and definitions
Term | Definition |
---|---|
LoRaWAN | Long Range Wireless Area Network |
Example | Example |
Example | Example |
Example | Example |