Datalogging guidelines for a successful NanoEdge AI project

Revision as of 18:13, 16 March 2022 by Registered User (Shifumi draft 2)

This documents presents several use case studies where NanoEdge AI Studio has been used successfully to create smart devices with machine learning features using a NanoEdge AI library.

It aims at explaining the methodology and thought process behind the choice of crucial parameters during the initial datalogging phase (that is, even before starting to use NanoEdge AI Studio) that can make or break a project.

For each use case, it will focus on the following aspects:

  • what is a meaningful representation of the physical phenomenon being observed
  • how to select the optimal sampling frequency for the datalogger
  • how to select the optimal buffer size for the data sampled
  • how to format the data logged properly for the Studio

Details about hardware and code implementation are irrelevant here and will not be discussed.

Warning white.png Warning

For simplicity, everything that follows uses a "buffer" approach for datalogging. It is valid for anomaly detection, classification and extrapolation projects (that is, for all project types in NanoEdge AI Studio) except in anomaly detection projects where the "Multi-sensor" sensor is explicitly selected. See Exception: Multi-sensor for more information.

Please refer to the NanoEdge AI documentation for more information.


1. Summary of important concepts

1.1. Definitions

Here are some clarifications regarding important terms that will be used in this document:

  • "axis/axes": total number of variables outputted by a given sensor. Example: a 3-axis accelerometer outputs a 3-variable sample (x,y,z) corresponding to the instantaneous acceleration measured in 3 perpendicular directions.
  • "sample": this refers to the instantaneous output of a sensor, and contains as many numerical values as the sensor has axes. For example, a 3-axis accelerometer outputs 3 numerical values per sample, while a current sensor (1-axis) outputs only 1 numerical value per sample.
  • "signal", "signal example", or "learning example": used interchangeably, these refer to a collection of numerical values that are used as input in the NanoEdge AI functions, either for learning of for inference. The term "line" is also used to refer to a signal example, because in the input files for the Studio, each line represents an independent signal example.
  • "buffer size", or "buffer length"; this is the number of samples per signal. It must be a power of 2. For example, a 3-axis signal with buffer length 256 is represented by 768 (256*3) numerical values.
Warning DB.png Important

Sampling the data which constitute "signal examples" is a continuous process, but in NanoEdge AI, the learning and inference processes (which use these signal examples as input) are not continuous.

In NanoEdge AI, the "signal examples" that are passed to the NanoEdge AI functions for learning or for inference are completely independent from one another. When the signal sampled is temporal (example: 3-axis accelerometer), it is made of a collection of several samples, and has an associated temporal length (which depends on the sampling frequency used).

For the whole duration of this "signal example", the samples have to be taken at regular time intervals. However, whatever happens outside of the scope of this signal example does not matter for NanoEdge AI. Each signal example may be separated from the others by a variable amount of time (because signals are independent), which means that neither learning nor inference functions have to be called at regular time intervals.


1.2. Sampling frequency

The sampling frequency, sometimes referred to as (output) data rate, corresponds to the number of samples measured per second.

The speed at which the samples are taken must allow the signal to be accurately described, or "reconstructed"; the sampling frequency must be high enough to account for the rapid variations of the signal. The question of choosing the sampling frequency therefore naturally arises:

  • If the sampling frequency is too low, the readings are too far apart; if the signal contains relevant features between two samples, they are lost.
  • If the sampling frequency is too high, it may negatively impact the costs, in terms of processing power, transmission capacity, or storage space for example.
Warning DB.png Important

To choose the sampling frequency, prior knowledge of the signal is useful in order to know its maximum frequency component. Indeed, to accurately reconstruct an output signal from an input signal, the sampling frequency must be at least twice as high as the maximum frequency that you wish to detect within the input signal. For more information, see Nyquist Frequency.

The issues related to the choice of sampling frequency and the number of samples are illustrated below:

  • Case 1: the sampling frequency and the number of samples make it possible to reproduce the variations of the signal.
NanoEdgeAI sampling freq 1.png
  • Case 2: the sampling frequency is not sufficient to reproduce the variations of the signal.
NanoEdgeAI sampling freq 2.png
  • Case 3: the sampling frequency is sufficient but the number of samples is not sufficient to reproduce the entire signal (meaning that only part of the input signal is reproduced).
NanoEdgeAI sampling freq 3.png


1.3. Buffer size

The buffer size corresponds to the total number of samples recorded per signal, per axis. In the case of a temporal signal, the sampling frequency and the buffer size put a constraint on the effective signal temporal length.

The buffer size must be a power of 2.

The buffer length must be chosen carefully, depending on the characteristics of the physical phenomenon sampled. For instance, the buffer may be chosen to be as short as a few periods in the case of a periodic signal (such as current, or stationary vibrations). In other cases, for instance when the signal is not purely periodic, the buffer size can be chosen to be as long as a complete operational cycle of the target machine to monitor (example: a robotic arm that moves from point A to point B, or a motor that ramps up from speed 1 to speed 2, and so on).

In some cases, where the signal considered is not temporal (example: time-of-flight sensor), the buffer size is simply constrained by the size and resolution of the sensor's output (for instance, a buffer size of 64 for a 8x8 time-of-flight array).


1.4. Data format

In the Studio, each signal is represented by an independent line, which format is completely constrained by the chosen buffer length and sampling frequency.

Warning DB.png Important

In summary, there are three important parameters to consider, for temporal signals:

  • n: buffer size
  • f: sampling frequency
  • L: signal length

They are linked together via: n = f * L. In other words, by choosing two (according to your use case), the third one is constrained.

Example:

Here is the input file format for a 3-axis sensor (in this example, an accelerometer), where the buffer size chosen is 256. Let's consider that the sampling frequency chosen is 1024 Hz. It means that each line (here, "m" lines in total) represents a temporal signal of 256/1024 = 250 milliseconds.

In summary, this input file contains "m" signal examples representing 250-millisecond slices of the vibration pattern the accelerometer is monitoring.

NanoEdgeAI input example.png


2. Use case studies

2.1. Vibration patterns on a ukulele

2.1.1. Context and objective

In this project, the goal is to capture the vibrations produced when the ukulele is strummed, in order to be able to classify them, based on which individual musical note, or which chord (superposition of up to 4 notes), is played.

This is achieved using vibration (3-axis accelerometer) instead of sound (microphone). The 3-axis accelerometer is placed directly onto the ukulele, or in the sounding box, wherever the vibrations are expected to be most intense.

In this application, the signals used are temporal.

NanoEdgeAI uku instrument.jpg
NanoEdgeAI uku position.jpg


2.1.2. Initial thoughts

Even before starting data collection, it is necessary to analyze the use case, and think about the characteristics of the signal we are about to sample. Indeed, we want to make sure that we capture the essence of the physical phenomenon that takes place, in a way that will be mathematically meaningful for the Studio (that is, making sure the signal captured contains as much useful information as possible).

When strumming the ukulele, some important characteristics of the vibration produced can be noted:

  1. The action of strumming is sudden, therefore the signal created is a burst of vibration, and dies off after a couple of seconds. The vibration may be continuous on a short time scale, but it does not last long, and is not periodic on a medium or long time scale. This will be helpful to determine when to start signal acquisition.
  2. The previous observation will also be useful to choose a proper buffer size (how long the signals should be, or how long the signal capture should take).
  3. The frequencies involved in the vibration produced are clearly defined, and can be identified through the pitch of the sound produced. This will be helpful to determine the target sampling frequency (output data rate) of the accelerometer.
  4. The intensity of the vibrations are somewhat low, so we'll have to be careful about where to place the accelerometer on the ukulele's body, and how to choose the accelerometer's sensitivity.


2.1.3. Sampling frequency

When strumming the ukulele, all the strings vibrate at the same time, which makes the ukulele itself vibrate. This produces the sound that we hear, so we can assume that the sound frequencies, and the ukulele vibration frequencies, are closely related.

Each chord contains a superposition of 4 musical notes, or pitches. This means we have 4 fundamental frequencies (or base notes) plus all the harmonics (which give the instrument its particular sound). These notes are quite high-pitched, compared to a piano for example. For reference, we humans can usually hear frequencies between 20 and 20000 Hz, and that the note A (or la) usually has a fundamental frequency of 440 Hz. So we can estimate that the chords played on the ukulele contain notes between 1000 and 10000 Hertz maximum.

To be more precise, and learn more about our signal, we can use a simple real-time frequency analyzer. In this example, we are using Spectroid, a free Android app.

Here is the spectrogram obtained when playing the C major chord (or do) several times.

NanoEdgeAI uku c major.jpg

Here's the spectrogram on a F major chord (fa).

NanoEdgeAI uku f major.jpg


In both cases, the fundamental frequency (0) and the 3 first harmonics (1, 2, 3) are between around 380 and 1000 Hz. There are many more harmonics up to 10 kHz, but they rapidly decrease in intensity, so we can assume for the moment that 1000 Hz is the maximum frequency to sample.

To do so, we need to set the sampling frequency to at least double that frequency; 2000 Hz minimum.

In this example, the accelerometer used only supports a discrete range of sampling frequencies, among which: 1666 Hz, 3333 Hz and 6666 Hz.

We will start testing with a sampling frequency of 3333 Hz. We will adapt later, depending on the results we get from the Studio, for instance by doubling the frequency to 6666 Hz for more precision.


2.1.4. Buffer size

The buffer size is the number of samples composing our vibration signal.

When strumming the ukulele, the sound produced lasts for one second or so. The vibration on the ukulele body quickly dies off, so we can assume that capturing a signal of maximum 0.5 seconds will be enough. We will adapt later, depending on the results we get from the Studio.

With a target length of approximately 0.5 seconds, and a sampling frequency of 3333 Hz, we get a target buffer size of 3333*0.5 = 1666.

The chosen buffer size should be **a power of two**, so we'll go with 1024 instead of 1665. We could have picked 2048, but 1024 samples is enough for a first test. We can always increase it later if required.

As a result, the sampling frequency of 3333 Hz with the buffer size of 1024 (samples per signal per axis) make a recorded signal length of 1024/3333 = 0.3 seconds approximately.

So each signal example that is used for data logging, or passed to a NanoEdge AI function for learning or inference, will represent a 300-millisecond slice of vibration pattern. During these 300 ms, all 1024 samples are recorded continuously. But since all signal examples are independent from one another, whatever happens between two consecutive signals does not matter (signal examples don't have to be recorded at precise time intervals, or continuously).


2.1.5. Sensitivity

The accelerometer used supports accelerations ranging from 2g up to 16g. For gentle ukulele strumming, 2g or 4g should be enough (we can always adjust it later).

We choose a sensitivity of 4g.


2.1.6. Signal capture

In order to create our signals, we can imagine continually recording accelerometer data. However, we chose an actual signal length of 0.3 seconds. So if we started strumming the ukulele randomly, using continuous signal acquisition, we would end up with 0.3-second signal slices that do not necessarily contain the useful part of the strumming, and have no guarantee that the relevant signals are captured. Also, a lot of "silence" would be recorded, between strums.

Instead, we implement a trigger mechanism; so that only the vibration signature that directly follows a strum is recorded.

Here are a few ideas on how to implement such a trigger mechanism that detects a strum:

  • We want to the capture of a single signal buffer (1024 samples) whenever the intensity of the ukulele's vibrations cross a threshold.
  • We need to monitor the vibrations continuously, and check whether or not the intensity has suddenly risen.
  • To measure the average vibration intensity at any time, we collect very small data buffers from the accelerometer (example: 4 consecutive samples), and compute the average vibration intensity across all sensor axes for each such "small buffer".
  • We continuously compare the average vibration intensities obtained from one "small buffer" (let's call it I1) to the next (call it I2).
  • We choose a threshold (example: 50%) to decide when to trigger (here, for instance, whenever I2 is at least 50% higher than I1).
  • We trigger the recording of a full 1024 sample signal buffer whenever I2 >= 1.5*I1 (here using 50%).

The resulting 1024-sample buffer is used as input signal in the Studio, and later on in the final device, as argument to the NanoEdge AI learning and inference functions.

Of course, different approaches (equivalent, or more elaborate) could be used in order to get a clean signal.

Here is what the signal obtained after strumming one chord on the ukulele looks like (plot of intensity (g) vs. time (sample number), representing the accelerometer's x-axis only):

NanoEdgeAI uku signal long.png


Observations:

  1. There is no saturation / clipping on the signal (y-axis of the plot above), so the sensitivity chosen for the accelerometer seems right.
  2. The length seems appropriate because it is much longer than a few periods of all the frequency components contained in our vibration, and therefore contains enough information.
  3. The length also seems appropriate also because it represents well the vibration burst associated to the strumming, including the quick rise and the slower decay.
  4. If the signal needs to be shortened (for instance, if we need to limit the amount of RAM consumed in the final application), we could consider cutting it in half (truncating it after the first 512 samples), and the resulting signal would probably still be very usable.
  5. The number of numerical values in the signal shown here is 1024 because we're only showing the x-axis of the accelerometer. In reality, the inpu signal is composed of 1024*3 = 3072 numerical values per signal.


2.1.7. From signals to input files

Now that we managed to get a seemingly robust method to gather clean signals, we need to start logging some data, to constitute the datasets that will be used as inputs in the Studio.

The goal is to be able to distinguish all main diatonic notes and chords of the C major scale (C, D, E, F, G, A, B, Cmaj, Dm, Em, Fmaj, G7, Am, Bdim) for a total of 14 individual classes.

For each class, we record 100 signal examples (100 individual strums). This represents a total a 1400 signal examples across all classes.

100 is an arbitrary number, but fits well within the guidelines: a bare minimum of 20 signal examples per sensor axis (here 20*3 = 60 minimum) and a maximum of 10000 (there is usually no point in using more than a few hundreds to a thousand learning examples).

When recording data for each class (example, strumming a Fmaj chord 100 times), we make sure to introduce some amount of variety: slightly different finger pressures, positions, strumming strength, strumming speed, strumming position on the neck, overall orientation of the ukulele, an so on. This increases the chances that the NanoEdge AI library obtained generalizes / performs well in different operating conditions.


NanoEdgeAI uku f major chord.jpg


Depending on the results obtained with the Studio, we will adjust the number of signals used for input, if needed.

In summary:

  • there are 14 input files in total, one for each class
  • the input files contain 100 lines each
  • each line in each file represents a single, independent "signal example"
  • there is no relation whatsoever between one line and the next (they could be shuffled), other than the fact that they pertain to the same class
  • each line is composed of 3072 numerical values (3*1024) (3 axes, buffer size of 1024)
  • each signal example represent a 300-millisecond temporal slice of the vibration pattern on the ukulele

2.1.8. Results

Here are the benchmark results obtained in the Studio, with 14 classes, representing all main diatonic notes and chords of the C major scale.

NanoEdgeAI uku bench.png


Here are the performances of the best classification library, summarized by its confusion matrix.

NanoEdgeAI uku matrix.png


Here are some other candidate libraries that were found during benchmark, with their associated performances, memory footprint, and ML model info.

NanoEdgeAI uku candidates.png


Observations:

  1. We get excellent results with very few misclassifications.
  2. There is no need to adjust the datalogging settings.
  3. We could consider adjusting the size of the signal (taking 512 samples instead of 1024) to reduce the memory footprint (RAM) of the libraries.
  4. Before deploying the library, we could do additional testing, by collecting more signal examples, and running them through the NanoEdge AI Emulator, to check that our library indeed performs as expected.
  5. If collecting more signal examples is impossible, we could restart a new benchmark using only 60% of the data, and keep the remaining 40% exclusively for testing using the Emulator.


2.2. Static pattern recognition using Time-of-Flight

2.2.1. Context and objective

In this project, the goal is to use a Time-of-Flight sensor to capture static hand patterns, and classify them depending on which category their belong to.

The 3 patterns that will be recognized here are: "Rock, Paper, Scissors", which correspond to 3 distinct hand positions, typically used during a "Rock paper scissors" game.

This will be achieved using a time-of-flight sensor, by measuring the distances between the sensor and the hand, using a square array of size 8x8.


2.2.2. Initial thoughts

In this application, the signals used are not temporal.

Only the shape/distance of the hand is measured, not its movement.

Here is an illustration of 4 examples of outputs from the time-of flight sensor. The coordinates of each measuring pixel is translated by its position on the 2D array, and the color of each pixel translates how close to the sensor the object is (the brighter the pixel, the closer the hand).

NanoEdgeAI rps arrays.png

2.2.3. Sampling frequency

Because each signal is time-independent, the choice of a sampling frequency is irrelevant to the structure of our signals. Indeed, what we here consider as a full "signal" is nothing more than a single sample; a 8x8 array of data, in the form of 64 numerical values.

However, we choose a sampling frequency of 15 Hz, meaning that a full signal will be outputted every 1/15th of a second.


2.2.4. Buffer size

The size of the signal is already constrained by the size of the sensor's array.

NanoEdgeAI rps arrays.png

As mentioned above, each "signal example" used as input in the studio is a single 8x8 array, as shown above. In practice, each array it will be represented as a line composed of 64 numerical values representing distances in millimeters. For example:

96.0 93.0 96.0 90.0 105.0 98.0 101.0 0.0 93.0 96.0 98.0 94.0 105.0 98.0 96.0 0.0 97.0 98.0 98.0 96.0 104.0 98.0 96.0 0.0 97.0 99.0 97.0 94.0 104.0 100.0 96.0 0.0 100. 0 98.0 96.0 96.0 103.0 98.0 98.0 0.0 99.0 97.0 98.0 97.0 102.0 98.0 101.0 0.0 102.0 99.0 100.0 100.0 102.0 98.0 102.0 0.0 102.0 95.0 99.0 96.0 96.0 96.0 102.0 102.0


2.2.5. Signal capture

In order to create our signals, we can imagine continually recording time-of-flight arrays. However, it would be preferable to do so only when needed (that is, only when some movement is detected under the sensor). This will also be useful after the datalogging phase is over, when we implement the NanoEdge AI Library; inferences (classifications) will only happen after some movement has been detected.

So instead of continuous monitoring, we use a trigger mechanism that only starts recording signals (arrays, buffers) when movement is detected. Here, it is built-in to the time-of-flight sensor, but it could easily be programmed manually. For instance:

  1. Choose threshold values for the minimum maximum detection distances
  2. Continuously monitor the distances contained in the 8x8 time-of-flight buffer
  3. Only keep a given buffer if at least 1 (or a predefined percentage) or the pixels returns a distance value comprised between the two predefined thresholds

During the datalogging, this approach prevents the collection of "useless" empty buffers (no hand). After the datalogging procedure (after the library is implemented), this approach is also useful to limit the number of inferences, effectively decreasing the computational load on the microcontroller, and its power consumption.


2.2.6. From signals to input files

The input signal is well defined, and needs to be captured in a relevant manner for what needs to be achieved.

The goal is to distinguish among 3 possible patterns, or classes. Therefore, we create 3 input files, each corresponding to one of the classes: : rock, paper, scissors.

Each input file will contain a significant number of signal examples (~100 minimum), covering the whole range of "behaviors" or "variety" that pertain to a given class. For instance, for "stone", we need to provide examples of many different versions of "stone" hand positions, that describe the range of everything that could happen and rightfully be called "stone". In practice, this means capturing slightly different hand positions (offset along any of the 2 directions of the time-of-flight array, but also, at slightly different distances from the sensor), orientations (hand tilt), and shapes (variations in the way the gesture is performed).

This data collection process is greatly helped by the fact that we sample sensor arrays at 15 Hz, which means that we get 900 usable signals per minute.

For each class, we collect data in this way for approximately 3 minutes. During these 3 minutes, slight variations are made:

  1. to the hand's position in all 3 directions (up/down left/right, top/bottom)
  2. to the hand's orientation (tilt in 3 directions)
  3. to the gesture itself (example, for the "scissors" gesture, wiggle the two fingers slightly)

We get a total of 3250 signal examples for each class.


2.2.7. Results

Here are the classification benchmark results obtained in the Studio with these 3 classes.

NanoEdgeAI rps benchmark.png

Here are the performances of the best classification library, summarized by its confusion matrix.

NanoEdgeAI rps confusion.png

Here are some other candidate libraries that were found during benchmark, with their associated performances, memory footprint, and ML model info.

NanoEdgeAI rps libs.png

Observations:

  1. We get excellent results with very few misclassifications.
  2. Before deploying the library, it is good practice to test it by collecting more signal examples, and running them through the NanoEdge AI Emulator, to check that our library indeed performs as expected.
  3. Considering two libraries with similar performances (accuracy, confidence), experience shows that libraries requiring more Flash memory often generalize better to unseen data (more reliable / adaptable when testing in slightly different conditions).

{{Important| Mitigating false classifications:

Here, the time of flight sensor outputs 15 fresh signals per seconds, which means that we could run approximately 15 inferences per second (a bit less, considering inference time, which is in the order of a few tens of milliseconds). This is much quicker than a typical game of "rock, paper, scissors", and too fast from a human's perspective.

We can use this high number of inferences per second to confirm/verify the classifications, and only output a consolidated result, instead of displaying the classification output of each single inference. Typically, we just wait until we get N (10 for example) identical inference outputs in a row, to display a reliable result, and otherwise, we don't output anything.

Here, we would output a consolidated "rock" result:

  rock rock [...x7] rock

While here, no shape is clearly identified, and we can't get a consolidated result, so we would wait:

<syntaxhighlight lang="sh"

rock rock [...x5] paper rock rock [...x6] paper </syntaxhighlight >



2.3. Vibration patterns on an electric motor

2.3.1. Context and objective

2.3.2. Initial thoughts

2.3.3. Sampling frequency

2.3.4. Buffer size

2.3.5. AAAA

2.3.6. BBBB

2.3.7. From signals to input files

2.3.8. Results

2.4. Current sensing on a 3-phase motor

2.4.1. Context and objective

2.4.2. Initial thoughts

2.4.3. Sampling frequency

2.4.4. Buffer size

2.4.5. AAAA

2.4.6. BBBB

2.4.7. From signals to input files

2.4.8. Results

3. Resources