STM32WB Bluetooth® LE – Heart Rate Sensor Project

Revision as of 12:35, 4 February 2022 by Registered User (→‎optimize Low power)

1. Heart Rate Profile Presentation

Heart Rate Profile (HRP) [1] is a Generic Attribute Profile (GATT) based low energy profile defined by the Bluetooth® Special Interest Group[2]
The HRP, widely used in fitness applications, defines the communication between a GATT-server of a Heart Rate Sensor device, such as a wrist band, and a GATT-client Collector device, such as a smartphone or tablet.
Heart Rate Sensor is the device that measures heart rate data and other information, it can be defined as a GAP peripheral and GATT server implemented with the Heart Rate Service [3]

This wiki page is the description of the Heart Rate Sensor project provided within the STM32CubeWB MCU Package[4]

Bluetooth® LE Heart Rate profile overview
Connectivity Heart-Rate-Profile-Overview.png


The table below describes the structure of Heart Rate Sensor services :

Bluetooth® LE Heart Rate Service specification
Service Characteristic Mode UUID
Heart Rate Service 0x180D
Heart Rate Measurement Notify 0x2A37
Body Sensor Location Read 0x2A38
Heart Rate Control Point Write 0x2A39
Device Information Service 0x180A
Manufacturer Name String Read 0x2A29

2. Heart Rate Profile Interaction

Heart Rate Profile is a combination of a Heart Rate Collector and a Heart Rate Sensor to connect and exchange data in differents applications.

  • The Heart Rate Sensor:
    • Measures the heart rate and exposes it via the Heart Rate Service.
    • Contains the Device Information Service, which contains information for example about the manufacturer of the device.
    • Is the GATT server.
  • The Heart Rate Collector:
    • Accesses the information exposed by the Heart Rate Sensor and can for example display it to the end user or store it on non-volatile memory for later analysis.
    • Is the GATT client.

The GAP - Generic Access Profile defines and manages advertising and connection.

Collector Central device and Sensor Peripheral device
Connectivity HR GAP Interaction.png


The GATT - Generic Attribute Profile defines and manages in/out data exchanges.

Collector GATT Client device and Sensor GATT Service device
Connectivity HR GATT Interaction.png



Once Bluetooth® LE connection established & notification enabled :

  • Heart Rate measurement provided to remote every 1s.
  • Connection interval may be changed by application.

3. Requirements

3.1. Software and System requirements

Software required are the following (minimum IDEs version) :

  • IAR Embedded Workbench for ARM (EWARM) toolchain V8.20.2
  • RealView Microcontroller Development Kit (MDK-ARM) toolchain V5.31
  • STM32CubeIDE toolchain V1.7.0 [5].


Programmer:

  • STM32CubeProgrammer[6] : To flash the board with an already generated binary

3.2. Hardware requirements

P-NUCLEO-WB55 [7] or STM32WB5MM-DK Discovery Kit [8] is necessary to install the application.

Hardware platforms illustration
Connectivity hardware-presentation.png


3.3. Smartphone Application

BLE_HeartRate application works with ST BLE Sensor and ST BLE ToolBox applications. More information about these smartphone applications on this page.

4. STM32WB Heart Rate Sensor Example Description

4.1. Project Directory

The "BLE_HeartRate" application is available by downloading STM32CubeWB MCU Package[9].

Heart Rate project directory
Connectivity heartRate.png

4.2. Project Description

4.2.1. Structure

Software project structure with the most important parts :

Heart Rate project structure
Connectivity HR project structure.png
Connectivity yellow box.png
Main applicative part files
Connectivity blue box.png
Bluetooth® LE Stack API Interface
Connectivity dark blue box.png
Services management
Connectivity green box.png
System commands
Connectivity pink box.png
Transport Layer Interface

WARNING: Do not modify the files in Middlewares folder


4.2.2. Application Initialization

The different steps of application initialization are described bellow :

Heart Rate project initialization
Connectivity HR Application Initialization.png
puce1.png
  • Initialize the system (HAL, Clock, Power Mode, RTC IP, Timer Server)
  • Infinite loop for run mode
puce2.png
  • Initialize the BSP (LEDs, buttons…), Transport Layer Interface, Debugger
  • Wait for initialization done
puce3.png
  • Initialize the Bluetooth® LE App – GAP level
  • Manage GAP events (advertising,scanning)
puce4.png
  • Initialize the Bluetooth® LE App – GATT level
  • Initialize the Bluetooth® LE Stack
  • Manage GATT events
puce5.png
  • Register Event Handler
  • Initialize and manages services
  • Update characteristic
puce6.png
  • Initialize the context
  • Manage Heart Rate Service notification

4.2.3. GAP & GATT Initialization & Interaction

puce3.png

The Bluetooth LE Heart Rate Sensor Application initialization is done within app_ble.c

  • starts the BLE Stack - initialize the device as Peripheral - configure & start Advertising : ADV Parameters, Local Name, UUID - APP_BLE_init()
  • call the services controller initialization SVCCTL_Init() - svc_ctl.c
  • manages the GAP event - SVCCTL_App_Notification()
    • EVT_LE_CONN_COMPLETE - Provides information of the connection interval, slave latency, Supervision timeout
    • EVT_LE_CONN_UPDATE_COMPLETE - Provides the new information of the connection
    • EVT_DISCONN_COMPLETE - Informs the application about the link disconnection and the reason
    • EVT_ENCRYPT_CHANGE - Informs the application weather the link is encrypted
puce4.png

The Services management is done by the service controller - svc_ctl.c

  • Calls the Initialization function of all the developed services - SVCCTL_SvcInit()
    • Heart Rate service - HRS_Init() - hrs.c
    • Device Information service - DIS_Init() - dis.c
  • Registers Services Event Handler - SVCCTL_RegisterSvcHandler(...)
  • manages events - SVCCTL_UserEvtRx ()- from the BLE Host Stack and redirect them to the services registered - HearRate_Event_Handler() - or gap event handler - SVCCTL_App_Notification
puce5.png

The Heart Rate Service hrs.c manages the specification of the service:

  • Service Init - HRS_Init()
    • Register Heart Rate Event Handle to Service Controller - SVCCTL_RegisterSvcHandler(HearRate_Event_Handler);
    • Initialize Service UUID – add Heart Rate service as Primary services
      • Initialize Heart rate Measurement Characteristic
      • Initialize Body Sensor Location Characteristic
  • Update Heart Rate Measurement Characteristic - HRS_UpdateChar()
  • Update Body Sensor Location Characteristic Value - HRS_UpdateChar()
  • manage the GATT event from BLE Stack - HeartRate_Event_Handler()
    • ACI_GATT_WRITE_PERMIT_REQ_VSEVT_CODE
      • reception of a Write Command : HR Control Point Characterictic Value
        • Send an aci_gatt_write_response() with an OK or KO status.
        • Notify application to Reset Energy Expended - HRS_Notification(HRS_RESET_ENERGY_EXPENDED_EVT)
    • ACI_GATT_ATTRIBUTE_MODIFIED_VSEVT_CODE
      • reception of an attribute modification - HR Measurement Characteristics Description Value : ENABLE or DISABLE Notification
        • Notify application of the Measurement Notification - HRS_Notification(HRS_NOTIFICATION_ENABLED/DISABLED)
Heart Rate sensor software module interaction
Connectivity HeartRate-Project.png


puce6.png

The application level of the Heart Rate Sensor is done with hrs_app.c:

  • initialization the context of the application
    • measurement value flags support
    • body sensor location - HRS_BODY_SENSOR_LOCATION_HAND
  • receive notification from the heart rate service - HRS_Notification()
  • when Heart rate measurement characteristics enabled by the remote, simulate every 1s the Heart Rate Measure (HRSAPP_Measurement) and increase the energy expended to transfer to the remote device (collector) - HRS_UpdateChar()

4.3. Build and Install

Follow steps described in Bluetooth® LE Build and Install Application page, applying it for BLE_HeartRate project.

4.4. How to use

Once the BLE Heart Rate application installed on the STM32WB platform, launch ST BLE Sensor or ST BLE ToolBox smartphone application. Then, scan and connect the device called HRSTM to the application.
Once Bluetooth® LE connection is established & notification is enabled by the smartphone:

  • Heart Rate measurement is provided to remote every 1s.
    • thanks to the timer server and the task manager

BLE Heart Rate application support the pairing procedure

  • SW1 allows to clear the security database
  • SW2 allows to request pairing

With the WB55.Nucleo board, it is possible to change RF PHY modulation

  • SW3 allows to switch to 2Mbits or 1Mbits PHY

4.5. optimize Low power

/**

* SMPS supply
* SMPS not used when Set to 0
* SMPS used when Set to 1
*/
  1. define CFG_USE_SMPS 1

par defaut c'est low power mais sans SMPS - description pour une meilleure optimisation SMPS = 1 dans app_conf.h

4.6. UART Debug Trace

/**

* When set to 1, the traces are enabled in the BLE services
*/
  1. define CFG_DEBUG_BLE_TRACE 1

/**

* Enable or Disable traces in application
*/
  1. define CFG_DEBUG_APP_TRACE 1

5. Heart Rate Collector - Smartphone Application

5.1. ST BLE Sensor Application

Once the BLE Heart Rate application installed on the STM32WB platform, launch the ST BLE Sensor smartphone application. Click on Connect one Device interface. Then your device should be visible and connectable by clicking on it. Now bpm measurement is displayed in real time.

BLE Heart Rate application on ST BLE Sensor
Connectivity Heart-Rate-screen-cap-1.jpg
Connectivity Heart-Rate-application-2.jpg
Connectivity Heart-Rate-App-3.jpg


5.2. ST BLE ToolBox Application

Once the BLE Heart Rate application installed on the STM32WB platform, launch the ST BLE ToolBox smartphone application. Application starts scanning and allows to see advertisement data or to connect to device. Once device is connected bpm and kcal measurement are displayed in real time.

BLE Heart Rate application on ST BLE ToolBox
Connectivity ST BLE ToolBox HR Scan.jpg
Connectivity ST BLE ToolBox HR adv.jpg
Connectivity ST BLE ToolBox HR.jpg


With Discovery Kit Platform, the Heart Rate is also visible from the board LCD screen, and Heart pulse is illustrated:

Heart Rate on DK illustration
Connectivity heart-rate-DK.png

6. References