Introduction to Zigbee

Revision as of 12:28, 1 February 2022 by Registered User

1. Introduction

Zigbee® is an IEEE 802.15.4-based communication protocol used to create wireless personal area (WPAN) networks. The aim is to provide a simple networking layer and standard application profiles that can be used to create interoperable solutions, with low-power and low-bandwidth constraints.

Zigbee is used in many application areas:

  • Home automation
  • Industrial control systems
  • Building automation
  • Medical data collection & monitoring
  • HVAC control
  • Wireless sensor networks

The data throughput is 250 kbps in 2.4 GHz band and the typical range is 10-20 meters. 250 kbps is raw data rate at PHY level. At application level, data rate is lower due to protocol stack overhead.

2. Zigbee network

2.1. Topology

Zigbee supports 3 types of network topologies as shown on the figure.

Zigbee network topologies

2.2. Type of devices

In Zigbee, there are 3 logical device types:

  • Coordinator (ZC): This is the first node to be started. The coordinator is responsible for forming the network by allowing other nodes to join the network through it. The coordinator is responsible for starting the network and for choosing certain key network parameters. Once the network is established, the coordinator has a routing role. In a centralized network, every Zigbee mesh network must have one and only one coordinator.
  • Router (ZR): This is a node with a routing capability which is also able to send and receive data. It also allows other nodes to join the network through it. A Zigbee® mesh network can have multiple routers.
  • End Device (ZED): This is a node which is only capable of sending and receiving data. It has no routing capability. A Zigbee mesh network can have multiple end devices. End device can also be sleepy end device (SED) allowing very low power consumption.

The figure below gives an overview of a Zigbee Mesh network with the different device types.

Zigbee mesh network example with device roles

2.3. Type of network

To satisfy a wide range of applications and to ensure the optimal balance of security, Zigbee offers two types of networks: distributed and centralized.

  • In a distributed network, there are no coordinator. In this configuration, any router can issue network security keys. As more routers and end devices join the network, a router that is already on the network securely sends the network key. All devices on the network use the same network key to encrypt messages.
  • In a centralized network, there is an entity named Trust Center (TC), which is typically the coordinator. The TC forms a centralized network and allows routers and end devices to join the network if they have proper credentials. In a centralized network, only the TC can issue encryption keys. The TC also establishes a unique TC Link Key for each device on the network as they join and link keys for each pair of devices as requested.

For obvious reasons, the centralized network is much more secure than the distributed one. Most of the Zigbee examples provided inside the STM32WB firmware package are using a centralized network.

3. Architecture

As described before, Zigbee is built on top of the IEEE 802.15.4 standard. Zigbee provides routing and multi-hop functions to the packet-based radio protocol. It is built on top of two layers specified by 802.15.4: the physical (PHY) and MAC layers. The figure describes the main components of a Zigbee stack and its articulation with IEEE 802.15.4 and general application layer.

Zigbee stack overview

3.1. MAC Layer

In MAC frame there is 2-byte field for control. Bits 0-2 indicate frame type, which could be one of the four following types:

  • Beacon frame (000), used to scan networks
  • Data frame (001), used to transmit data from higher layers
  • Acknowledgment frame (010)
  • MAC command (011), like Association request, Data request, etc.

At the end of each MAC frame, there are two bytes CRC used to verify the integrity of the packet.

3.2. Network Layer

The network layer takes care of topology construction, maintenance, naming, routing, and security.
Zigbee specification defines 2 device types:

  • FFD, Full Feature Device, can accept any role in the network (router, coordinator, or end device).
  • RFD, Reduced Feature Device, can support only end device role.

3.3. Application Layer

The APL layer is composed of several sublayers. The components of the APL layer are shown in following Figure.

Application layer sublayers

3.3.1. Application Support Sublayer (APS)

APS provides an interface between the network layer (NWK) and the application layer through a general set of services that are used by both the ZDO and the manufacturer-defined application objects. The APS is responsible for:

  • Binding management
  • Message forwarding
  • Group address definition and management
  • Address mapping from 64-bit extended addresses to 16-bit NWR addresses
  • fragmentation and reassembly of packets
  • Reliable data transport

3.3.2. Zigbee Device Object (ZDO)

The ZDO component handles the device management and communication functions. It includes:

  • Initializing the APS sublayer and the NWK layer
  • Device discovery
  • service discovery
  • Network management, including defining the operating mode of the device (ZC, ZR or ZED).
  • Security management
  • Initiating and/or responding to binding requests

4. Zigbee Profiles

4.1. Zigbee Application Profiles

The Application profile is a collection of device descriptions, which together form a cooperative application. The Profile defines the data exchange form for the application functions of a ZigBee physical device. A Profile consists of one or more Endpoints, each with one or more clusters associated.

Clusters are a group of commands and attributes that define what a device can do. Clusters are managed by the ZCL (ZigBee Cluster Library).

Endpoint number that can be used for a ZigBee application are comprise between 1 and 240.

  • Zigbee device object (ZDO) is attached to endpoint 0
  • endpoint 255 is used to broadcast to all endpoints
  • endpoints 241-254 are reserved for special functions
Zigbee Application Profile organization

Several clusters are supported on the STM32WB:

Number Cluster ID Cluster Name
1 0x0000 Basic
2 0x0001 Power Configuration
3 0x0003 Identify
4 0x0004 Groups
5 0x0005 Scenes
6 0x0006 On/Off
7 0x0008 Level Control
8 0x000a Time
9 0x0019 OTA Upgrade
10 0x0020 Poll Control
11 0x0021 Green Power Proxy
12 0x0102 Window Covering
13 0x0202 Fan Control
14 0x0204 Thermostat User Interface Configuration
15 0x0300 Color control
16 0x0301 Ballast Configuration
17 0x0400 Illuminance Measurement
18 0x0402 Temperature Measurement
19 0x0406 Occupancy Sensing
20 0x0502 IAS Warning Device (WD)
21 0x0b05 Diagnostics
22 0x1000 Touchlink
23 0x0002 Device Temperature Configuration
24 0x0007 On/Off Switch Configuration
25 0x0009 Alarms
26 0x000b RSSI Location
27 0x0015 Commissioning
28 0x001a Power Profile Cluster
29 0x0024 Nearest Gateway Cluster
30 0x0101 Door Lock
31 0x0200 Pump Configuration and Control
32 0x0201 Thermostat
33 0x0203 Dehumidification Control
34 0x0401 Illuminance Level Sensing
35 0x0403 Pressure Measurement
36 0x0405 Relative Humidity Measurement
37 0x0500 IAS Zone
38 0x0501 IAS Ancillary Control Equipment (ACE)
39 0x0700 Price
40 0x0701 Demand Response and Load Control
41 0x0702 Metering
42 0x0703 Messaging
43 0x0704 Smart Energy Tunneling (Complex Metering)
44 0x0800 Key Establishment
45 0x0904 Voice Over ZigBee
46 0x0b01 Meter Identification
47 0x0b04 Electrical Measurement

4.2. Zigbee Device Profiles

The Zigbee Device Profile is a collection of device descriptions and clusters run directly by the ZDO. It applies to all Zigbee devices. The Zigbee Device Profile is a template that show of how to write an application profile. It is defined in the Zigbee Application Level Specification.

5. Acronyms and definitions

Term Definition
APS Application support sub-layer
MAC Media Access Control
PAN Personal Area Network
SED Sleepy end device
ZDO Zigbee Device Object