1. Heart Rate Profile Presentation
Heart Rate Profile (HRP) [1] is a Generic Attribute Profile (GATT) based low energy profile defined by the Bluetooth® Special Interest Group[2]
The HRP, widely used in fitness applications, defines the communication between a GATT-server of a Heart Rate Sensor device, such as a wrist band, and a GATT-client Collector device, such as a smartphone or tablet.
Heart Rate Sensor is the device that measures heart rate data and other information, it can be defined as a GAP peripheral and GATT server implemented with the Heart Rate Service [3]
This wiki page is the description of the Heart Rate Sensor project provided within the STM32CubeWB MCU Package[4]
Bluetooth® LE Heart Rate profile overview |
---|
The table below describes the structure of Heart Rate Sensor services :
Heart Rate Sensor services |
---|
2. Heart Rate Profile Interaction
Heart Rate Profile is a combination of a Heart Rate Collector and a Heart Rate Sensor to connect and exchange data in differents applications.
- The Heart Rate Sensor:
- Measures the heart rate and exposes it via the Heart Rate Service.
- Contains the Device Information Service, which contains information for example about the manufacturer of the device.
- Is the GATT server.
- The Heart Rate Collector:
- Accesses the information exposed by the Heart Rate Sensor and can for example display it to the end user or store it on non-volatile memory for later analysis.
- Is the GATT client.
The GAP - Generic Access Profile defines and manages advertising and connection.
Collector Central device and Sensor Peripheral device |
---|
The GATT - Generic Attribute Profile defines and manages in/out data exchanges.
Collector GATT Client device and Sensor GATT Service device |
---|
Once Bluetooth® LE connection established & notification enabled :
- Heart Rate measurement provided to remote every 1s.
- Connection interval may be change by application.
3. Requirements
3.1. Software and System requirements
Software required are the following (minimum IDEs version) :
- IAR Embedded Workbench for ARM (EWARM) toolchain V8.20.2
- RealView Microcontroller Development Kit (MDK-ARM) toolchain V5.31
- STM32CubeIDE toolchain V1.7.0 [5].
Programmer:
- STM32CubeProgrammer[6] : To flash the board with an already generated binary
3.2. Hardware requirements
P-NUCLEO-WB55 [7] or STM32WB5MM-DK Discovery Kit [8] is necessary to install the application.
Hardware platforms illustration |
---|
|
3.3. Smartphone Application
ST BLE Sensor application (for Android[9], or iOS[10]) or ST BLE ToolBox application (for Android[11], or IOS[12]).
4. STM32WB Heart Rate Sensor Example Description
4.1. Project Directory
The "BLE_HeartRate" application is available by downloading STM32CubeWB MCU Package[13].
Heart Rate project directory |
---|
4.2. Project Description
4.2.1. Structure
Software project structure with the most important parts :
WARNING: Do not modify the files in Middlewares folder
4.2.2. Application Initialization
The different steps of application initialization are described bellow :
4.2.3. GAP & GATT Initialization & Interaction
The GAP level of Heart Rate Sensor is managed by the file app_ble.c - APP_BLE_init()
- initialization of the device as Peripheral - Configure & Start Advertising : ADV Parameters, Local Name, UUID
- call the the services controller initialization SVCCTL_Init() - svc_ctl.c
- management of the GAP event:
- EVT_LE_CONN_COMPLETE
- Provides information of the connection interval, slave latency, Supervision timeout
- EVT_LE_CONN_UPDATE_COMPLETE
- Provides the new information of the connection
- EVT_DISCONN_COMPLETE
- Informs the application about the link disconnection and the reason
- EVT_ENCRYPT_CHANGE
- Informs the application weather the link is encrypted
- EVT_LE_CONN_COMPLETE
The Services management is done by the service controllers - svc_ctl.c
- Calls the Initialization function of all the developed services
- Heart Rate service - HRS_Init() hrs.c
- Device Information service - DIS_Init() dis.c
- Registers Service Event Handler
- SVCCTL_RegisterSvcHandler();
- function receiving the GATT events from the svc_ctl.c and redirect them to the application (hrs_app.c)
- SVCCTL_RegisterSvcHandler();
The Heart Rate Service hrs.c manages the specification of the service:
- Service Init - HRS_Init()
- Register Heart Rate Event Handle to Service Controller
- Initialize Service UUID
- aci_gatt_add_serv – add Heart Rate service as Primary services
- Initialize Heart rate Measurement Characteristic
- aci_gatt_add_char – add Heart Rate Characteristic
- Initialize Body Sensor Location Characteristic
- aci_gatt_add_char – add Body Sensor Location Characteristic
- Update Heart Rate Measurement Characteristic
- aci_gatt_update_char_value – update the wished characteristics with a value aligned with the specification
- Update Body Sensor Location Characteristic Value
- aci_gatt_update_char_value - update the wished characteristics with a value aligned with the specification
- HeartRate_Event_Handler(void *Event) – manage HCI Vendor Type Event:
- EVT_BLUE_GATT_WRITE_PERMIT_REQ
- Server receives a Write Command
- HR Control Point Char. Value
- Reset Energy Expended command then:
- Send an aci_gatt_write_response() with an OK status.
- Notify HRS application to Reset Energy Expended
- Or Send an aci_gatt_write_response() with an Error.
- EVT_BLUE_GATT_WRITE_PERMIT_REQ
- EVT_BLUE_GATT_ATTRIBUTE_MODIFIED
- HR Measurement Char. Description Value
- ENABLE Or DISABLE Notification
- Notify HRS application of the Measurement Notification
- HR Measurement Char. Description Value
- EVT_BLUE_GATT_ATTRIBUTE_MODIFIED
Heart Rate sensor software module interaction |
---|
4.3. Build and Install
Follow steps described in Bluetooth® LE Build and Install Application page, applying it for BLE_HeartRate project.
5. Heart Rate Collector - Smartphone Application
Once the BLE Heart Rate application installed on the STM32WB platform, launch the ST BLE Sensor smartphone application.
Click on Connect one Device interface:
Heart Rate application interface 1 |
---|
Your device should be visible from this interface, connect to it:
Heart Rate application interface 2 |
---|
Now bpm measurement is displayed in real time.
Heart Rate application interface 3 |
---|
With Discovery Kit Platform, the Heart Rate is also visible from the board LCD screen, and Heart pulse is illustrated:
Heart Rate on DK illustration |
---|
6. References
- ↑ Heart Rate profile specification
- ↑ Bluetooth® SIG
- ↑ Heart Rate service specification
- ↑ STM32CubeWB MCU Package
- ↑ STM32CubeIDE
- ↑ STM32CubeProgrammer Software
- ↑ P-NUCLEO-WB55 package
- ↑ STM32WB5MM-DK board
- ↑ ST BLE Sensor Android application
- ↑ ST BLE Sensor iOS application
- ↑ ST BLE Toolbox Android Application
- ↑ ST BLE Toolbox iOS Application
- ↑ STM32CubeWB MCU Package