STM32WB Bluetooth® LE – Heart Rate Sensor Project

Revision as of 12:36, 27 January 2022 by Registered User (→‎Structure)

1. Heart Rate Profile Presentation

Heart Rate Profile (HRP) [1] is a Generic Attribute Profile (GATT) based low energy profile defined by the Bluetooth® Special Interest Group[2]
The HRP, widely used in fitness applications, defines the communication between a GATT-server of a Heart Rate Sensor device, such as a wrist band, and a GATT-client Collector device, such as a smartphone or tablet.
Heart Rate Sensor is the device that measures heart rate data and other information, it can be defined as a GAP peripheral and GATT server implemented with the Heart Rate Service [3]

This wiki page is the description of the Heart Rate Sensor project provided within the STM32CubeWB MCU Package[4]

Bluetooth® LE Heart Rate profile overview
Connectivity Heart-Rate-Profile-Overview.png


2. Heart Rate Sensor Example

2.1. Requirements

2.1.1. Software and System requirements

Software required are the following:
minimum IDEs version:

  • IAR Embedded Workbench for ARM (EWARM) toolchain V8.20.2
  • RealView Microcontroller Development Kit (MDK-ARM) toolchain V5.31
  • STM32CubeIDE toolchain V1.7.0 [5].


Programmer:

  • STM32CubeProgrammer[6] : To flash the board with an already generated binary

2.1.2. Hardware requirements

A Nucleo board[7], a STM32WB USB dongle[7], or a STM32WB Discovery Kit[8] is necessary to install the application.

Hardware platforms illustration
Connectivity hardware-presentation.png


Plus a smartphone with ST BLE Sensor application (for Android[9], or iOS[10]).

2.1.3. Project Directory

The "BLE_HeartRate" application is available by downloading STM32CubeWB MCU Package[11].

Heart Rate project directory
Connectivity heartRate.png

2.2. Project Description

2.2.1. Structure

Software project structure with the most important parts :

Connectivity HR project structure.png


Connectivity yellow box.png
Main applicative part files
Connectivity blue box.png
Bluetooth® LE Stack API Interface
Connectivity dark blue box.png
Services management
Connectivity green box.png
System commands
Connectivity pink box.png
Transport Layer Interface


2.2.2. Application Initialization

The different steps of application initialization are described bellow :

Connectivity HR Application Initialization.png
puce1.png
  • Initialize the system (HAL, Clock, Power Mode, RTC IP, Timer Server)
  • Infinite loop for run mode
puce2.png
  • Initialize the BSP (LEDs, buttons…), Transport Layer Interface, Debugger
  • Wait for initialization done
puce3.png
  • Initialize the Bluetooth® LE App – GAP level
  • Manage GAP events (advertising,scanning)
puce4.png
  • Initialize the Bluetooth® LE App – GATT level
  • Initialize the Bluetooth® LE Stack
  • Manage GATT events
puce5.png
  • Initialize services
  • Manage services

2.2.3. GAP & GATT Initialization & Interaction

Interaction between Middleware and User Application is described in the following illustration. lionel to explain...

Heart Rate project architecture
Connectivity HeartRate-Project.png


2.3. Build and Install

Follow steps described in Bluetooth® LE Build and Install Application page, applying it for BLE_HeartRate project.

2.4. Handle

Once the BLE Heart Rate application installed on the STM32WB platform, launch the ST BLE Sensor smartphone application.

Click on Connect one Device interface:

Heart Rate application interface 1
Connectivity Heart-Rate-screen-cap-1.jpg


Your device should be visible from this interface, connect to it:

Heart Rate application interface 2
Connectivity Heart-Rate-application-2.jpg


Now bpm measurement is displayed in real time.

Heart Rate application interface 3
Connectivity Heart-Rate-App-3.jpg


With Discovery Kit Platform, the Heart Rate is also visible from the board LCD screen, and Heart pulse is illustrated:

Heart Rate on DK illustration
Connectivity heart-rate-DK.png

3. References