STM32WB BLE STM32CubeMX

Revision as of 17:40, 19 November 2021 by Registered User (→‎Code Generation)

Click here for Bluetooth® Low Energy overview.

1. Introduction

This wiki page defines how to generate a Bluetooth® Low Energy (BLE) server custom application for STM32WB55RG MCU using STM32CubeMX software.

2. Build a Bluetooth® Low Energy application on STM32WB with CubeMX

The STM32WB55RG device flashed with the generated application can send data to a smartphone (using ST BLE Toolbox application), and receive commands from it through Bluetooth® Low Energy.

System presentation


This GATT Server application shall be able to expose 2 services:

  • 1st service exposes 2 characteristics
  • 2nd service exposes 3 characteristics

The first service (My_P2P_Server) looks like P2P Server (STM proprietary) with 2 characteristics:

  • Characteristic 1 has Write property
  • Characteristic 2 has Notify property

Writing to characteristic 1 toggles blue LED.
Pressing SW1 on Nucleo board send data to the phone

Custom Service


The second service (My_Heart_Rate) is build as a SIG Heart Rate, but the behavior won't be managed.

The following steps are recommended to build this application example:

  1. CubeMX initialization for STM32WB55RGVx
  2. STM32WB application configuration
    1. Clock configuration
    2. IP configuration
    3. System configuration (WPAN)
  3. Bluetooth® LE GAP/GATT Custom Application Configuration

Services and Characterics configuration are given in the following table:

P2P Server and Heart Rate services configuration

3. Tools

3.1. Software tools

To make and use this project, the needed software tools to complete the application:

  • STM32CubeMX software
  • STM32CubeWB MCU Package[1]
  • IDE: STM32CubeIDE[2] or IAR[3]
  • Serial Terminal (TeraTerm[4])
  • ST BLE Toolbox app (iOS[5] or Android[6])

3.2. Hardware Tools

A STM32WB Nucleo board and a micro-B to Type-A USB cable are also needed.

Hardware presentation


The PC is connected to the ST-LINK connector of the NUCLEO board (right connector from the top view

ST-LINK connection


4. CubeMX initialization for P-NUCLEO-WB55

4.1. STM32CubeMX initial setup

Open STM32CubeMX and start a new project from the "Access to MCU selector" button

New Project Menu


Chose the MCU and then start the new project:

puce1.png
Check STM32WB in MCU/MPU Selector tab
puce2.png
Select the STM32WB55RG part number
puce3.png
Start the project
Project Interface


4.2. Pinout and IP configuration

To configure the system, enable all the required system resource and peripherals clicking on A->Z to display all IPs.

Pinout & Configuration Interface


BLE mode is reachable once the following system resources and peripherals are turned to enable.

  • HSEM :activated
  • IPCC : activated, ITs enabled
  • RCC : HSE and LSE on Crystal/Ceramic resonator
  • RTC : activate clock source and enable internal wakeup
  • RF : activate RF1
  • STM32WPAN : BLE
IP list

4.2.1. HSEM

The Hardware SEMaphore (HSEM) is needed to manage shared resources between the two CPU cores in the STM32WB.

HSEM activation

4.2.2. IPCC

Configuration of Inter-Processor Controller Communication (IPCC) is done as follow:

puce1.png
Select IPCC
puce2.png
Activate it
puce3.png
Go to NVIC Settings tab
puce4.png
Enable IPCC RX occupied interrupt
puce5.png
Enable IPCC TX free interrupt
IPCC activation & setup

4.2.3. RCC

On Reset and Clock Controller (RCC), High Speed clock (HSE) and Low Speed Clock (LSE) are mandatory for Bluetooth® LE radio.

RCC setup

4.2.4. RTC

Configuration of Real Time Counter (RTC) is done as follow:

puce1.png
Select RTC
puce2.png
Activate clock source
puce3.png
Set WakeUp as internal WakeUp
puce4.png
Go to NVIC Settings tab
puce5.png
Enable RTC wake up interrupt through EXTI line 19
RTC activation & setup

4.2.5. RF

Activate RF1:

RF activation

4.2.6. BLE

Finally, under STM32_WPAN check BLE box:

Bluetooth® LE activation

4.3. Clock configuration

On clock configuration tab, run the automatic clock issue solver:


Then:

puce1.png
Set RTC/LCD Source MUX on LSE
puce2.png
Set System Clock MUX on HSE_SYS
puce3.png
Set RFWKP Clock MUX to LSE
puce4.png
Set SMPS Clock MUX to HSE
puce5.png
Set SMPS Div on /4
Clock configuration

4.4. Project manager

All the project configuration is done on the Project Manager pane within 3 sections, and done as follow :

4.4.1. Project

puce1.png
Configure the project
puce2.png
Define the project name
puce3.png
Chose the project location
puce4.png
Select the Toolchain IDE and version
puce5.png
Define linker settings
puce6.png
Use default FW location
Project configuration


4.4.2. Code Generator

Manages files, packages and embedded software packs

Project generation


4.4.3. Advanced Settings

Definition of drivers to use (HAL/LL) and generated function calls

Advanced settings interface

5. BLE GAP/GATT Custom application configuration

  • Bluetooth® LE Peripheral Custom Template GATT Server Application can be defined:
    • On STM32WB
    • With STM32CubeMX
  • GAP peripheral : advertising configuration
  • GATT server configuration:
    • 5 services maximum
    • 5 characteristics maximum per service
  • ACI commands:
    • AN5270 : STM32WBx5 Bluetooth® Low Energy (BLE) wireless interface[7].

5.1. BLE Applications and Services

To start the definition of the Bluetooth® LE application :

puce1.png
Open Pinout & Configuration interface
puce2.png
Select STM32_WPAN
puce3.png
Go to BLE Application and Services tab
puce4.png
Enable Custom Template and disable Custom P2P Server


STM32_WPAN Interface: Application & Services Settings

5.2. Advertising Configuration

Advertising parameters are defined under BLE Advertising tab:

  • advertising configuration data are located in app_conf.h and ble_conf.h files
  • advertising elements data are located in app_ble.c file
STM32_WPAN Interface: Bluetooth® LE Advertising tab


Open Advertising Configuration and set the CFG_GAP_DEVICE_NAME to something of your liking, for example MY_APPLI.

STM32_WPAN Interface: Bluetooth® LE Advertising configuration


In the generated code these parameters are defined in :
1. app_conf.h file:

  • #define ADV_TYPE
  • #define BLE_ADDR_TYPE
  • #define FILTER
  • #define CFG_GAP_DEVICE_NAME

2. ble_conf.h file:

  • #define BLE_CFG_PERIPHERAL
  • #define BLE_CFG_CENTRAL
STM32_WPAN Interface: Bluetooth® LE Advertising configuration (2)


In Advertising elements:

  • Turn to “yes” the elements to add in the advertising packet payload as described in the image below puce1.png:
    - Tx power: AD_TYPE_TX_POWER_LEVEL
    - Complete local name: AD_TYPE_COMPLETE_LOCAL_NAME
    - 16 bits service UUID: AD_TYPE_16_BIT_SERV_UUID_CMPLT_LIST
    - Manufacturer specific data: AD_TYPE_MANUFACTURER_SPECIFIC_DATA
  • Set the value for the other elements as mentioned in the image below puce2.png:
    - Complete Local name: AD_TYPE_COMPLETE_LOCAL_NAME = MyCST
    - Service 1 UUID: UUID 1 = 0D18
STM32_WPAN Interface: Advertising elements


The advertising information is represented by advertising data elements, which are standardized on the Bluetooth SIG.
These elements are included in the advertising packet payload and are located in app_ble.c file (here the advertising packet structure’s length = 19 bytes).

Advertising elements: corresponding code


Warning white.png Warning
Pay attention to not oversize the ad_data[ ] length array.

This array size is automatically calculated by STM32CubeMX and does not exceed 25 bytes


5.3. Services and Characteristics Definition

All created services and characteristics are managed in custom_stm.c file. Each service and characteristic is added in SVCCTL_InitCustomSvc() function using:

  • aci_gatt_add_service(…) for services,
  • aci_gatt_add_char(…) for characteristics.

5.3.1. Services Definition

Each created service is defined in a dedicated CubeMX tab:

  • Up to 5 Characteristics per Service
  • UUID type can be defined as 16 or 128 bits
  • UUID definition
  • Type value is Primary or Secondary Service


A custom application can define up to 5 services.
In the following example, we define 2 Services, My_P2P_Server and My_Heart_Rate.

You can set the number of service to define in the BLE GATT tab (present in STM32_WPAN interface):

puce1.png
Go to BLE GATT Tab,
puce2.png
Enter the number of services to define,
puce3.png
Enter the long and short names,
puce4.png
For each Service, a tab with the given Service long name is created.
Bluetooth® LE GATT services definition


For each defined service puce1.png, set the number of Characteristics and the service UUID value as defined in the following images puce2.png.
2 Characteristics for My_P2P_Server service.

Bluetooth® LE GATT services definition


3 Characteristics for My_Heart_Rate service.

Bluetooth® LE GATT services definition


Info white.png Information
If UUID type is 128bits reduced, the UUID value (on 16 bits) is encapsulated in a 128 bits data thanks to COPY_xxx_UUID macro (where xxx is Service or Characteristic long name) to bring it in 128 bits.

For example an UUID of 0xFE41 is encapsulated as : 0x00,0x00,0xfe,0x41,0x8e,0x22,0x45,0x41,0x9d,0x4c,0x21,0xed,0xae,0x82,0xed,0x19.

If UUID type is 16bits, the UUID value is used as this to create the service or characteristic.

5.3.2. Characteristics Definition

For each Characteristic the following parameters must be defined

  • General
  • Properties
  • Permissions
  • GATT events


My_P2P_Server Characteristics:
My_P2P_Server service have 2 characteristics, with respective short name LED_C and SWITCH_C.
Defined as follow:

MY_P2P_Server characteristics definition



My_Heart_Rate Characteristics:
My_Heart_Rate service have 3 characteristics, with respective short name HRS_M, HRS_SL and HRS_CTRL.
Defined as follow:

My_Heart_Rate characteristics definition


5.3.3. Pairing Definition

Pairing is done to support secure connection method.
All pairing parameters defined in the BLE_Pairing tab are located in app_conf.h file.
When PAIRING_PARAMETERS is set to ON, pairing parameters are available on the interface and can be defined as follow:

Pairing definition



Once configuration is done in STM32CubeMX, the code can be generated by following the steps described in Code Generation chapter.
If you want to enable traces before generating the project, go to next chapter.
If you want to setup User button and LED, you can refer to P2P Server: Notifications and Writes Setup chapter.

6. Enable Traces

6.1. USART Configuration

Go to USART1 setup interface and select Asynchronous Mode:

USART Setup Interface


Then, go to DMA Settings tab puce1.png, click on Add button puce2.png and select USART1_TX puce3.png.

USART Setup : DMA Settings


Ensure DMA1 Channel1 is selected, and click on USART1_TX line to show DMA Request Settings.

USART Setup : DMA Settings 2


Go to NVIC Settings tab puce1.png and enable USART1 global interrupt puce2.png.

USART Setup : NVIC Settings


6.2. NVIC Configuration

Go to NVIC Settings interface puce1.png and set DMA1 Channel 1 global interrupt Preemption Priority to 15 (lowest priority) puce2.png.
Check that USART1 global interrupt is enabled puce3.png.

6.3. USART1 Pinout Definition

Go to Pinout view puce1.png.
Set UASRT1_TX on PB6 and USART1_RX on PB7:

  • Click on PB6
  • Select USART1_TX in the list
  • Click on PB7
  • Select USART1_RX in the list

You can use the search located in the bottom right of the pinout view window puce2.png to find a pin or signal name easily (here PB6 and PB7)

Pinout View


6.4. STM32_WPAN Configuration

Go to STM32_WPAN setup interface and select the Configuration tab puce1.png.
Enable the application traces puce2.png, set CFG_DEBUG_TRACES_UART on hw_uart1 puce3.png.
Configure the debug traces to manage the different types of logs puce4.png.

STM32WPAN Setup


6.5. Project Manager Settings

Go to Project Manager interface puce1.png and select the Advanced Settings tab puce2.png.
Configure MX_UASRT1_UART_Init function puce3.png as:

  • Check Do Not Generate Function Call checkbox.
  • Uncheck Visibility (Static) checkbox.
MX_UASRT1_UART_Init function Settings



Once the traces configuration is done in STM32CubeMX, the code can be generated by following the steps described in Code Generation chapter.

6.6. Add USER CODE section in app_entry.c

In order to make the application able to manage debug messages, app_entry.c file must be updated.
In MX_APPE_Init() function, add a call to APPD_Init() function into the USER CODE APPE_Init_1 section as follow:

void MX_APPE_Init( void )
{
  System_Init( );       /**< System initialization */

  SystemPower_Config(); /**< Configure the system Power Mode */

  HW_TS_Init(hw_ts_InitMode_Full, &hrtc); /**< Initialize the TimerServer */

/* USER CODE BEGIN APPE_Init_1 */
  APPD_Init();
/* USER CODE END APPE_Init_1 */
  appe_Tl_Init();	/* Initialize all transport layers */


Open a debug terminal as TeraTerm connected on USART1 to display application messages. Refer to TeraTerm Setup chapter.

7. P2P Server Notifications and Writes management

In order to use P2P Server Notification and Write characteristics, several points have to be configured:

  • User Button and the related Interrupt, to Notify the P2P Client
  • Blue LED, to receive a P2P Client write operation
  • Custom application code to manage SW1 and write operation on P2P Server service
STM32WB Nucleo board


7.1. User Button and LED pinout

In the Nucleo board, LED pinout is:

  • Blue LED : PB5
  • Green LED: PB0
  • Red LED: PB1

Switch (user button) pinout is:

  • SW1: PC4
  • SW2: PD0
  • SW3: PD1

When used:

  • Switch pins are declared as GPIO_EXTIx (x = pin number)
  • LED pins are declared as GPIO_OUTPUT





7.2. Blue LED Setup

Go to Pinout & Configuration -> Pinout View Interface puce1.png, click on PB5 puce2.png and select GPIO_OUTPUT puce3.png.

Blue LED Pinout


In Pinout & Configuration interface, go to the GPIO tab puce1.png.
Select the GPIO line corresponding to PB5 puce2.png and configure the PB5 configuration pane puce3.png as follow:

  • GPIO Mode: Output Push/Pull
  • GPIO Pull-up/Pull-down: No Pull-up and no pull-down
  • Maximum outpus speed: High
  • User Label: Blue_Led
Blue LED : GPIO Configuration


7.3. SW1 Button Setup

Go to Pinout & Configuration -> Pinout View Interface puce1.png, click on PC4 puce2.png and select GPIO_EXTI4 puce3.png.

SW1 Button Pinout


In Pinout & Configuration interface, go to the GPIO tab puce1.png.
Select the GPIO line corresponding to PC4 puce2.png and configure the PC4 configuration pane puce3.png as follow:
* GPIO Mode: External Interrupt Mode with Rising edge trigger detection

  • GPIO Pull-up/Pull-down: Pull-up
  • User Label: SW1_User
SW1 Button : GPIO Configuration



Go to NVIC interface puce1.png and click on the NVIC tab puce2.png.
Enable the EXTI line4 interrupt puce3.png, this interrupt corresponds to SW1.

SW1 Button : GPIO Configuration


7.4. Code Modification : User Sections

Once your SW1 Button and Blue LED GPIOs are correctly setup, generate your project by following the steps described in Code Generation chapter.

The generated source code contains several sections called User Sections where users can add custom application code parts.
These sections are not erased/modified at project regeneration from CubeMX.

In order to manage SW1 and write operation on P2P Server service, some code parts have to be added in User Sections of the following files and theire respective header files:

Files to update


  • In app_conf.h:

Define the task for the characteristic My_Switch_Char of My_P2P_Server by adding code in CFG_Task_Id_With_HCI_Cmd_t User Code Section:

/**< Add in that list all tasks that may send a ACI/HCI command */
typedef enum
{
    CFG_TASK_ADV_CANCEL_ID,
#if (L2CAP_REQUEST_NEW_CONN_PARAM != 0 )
    CFG_TASK_CONN_UPDATE_REG_ID,
#endif
    CFG_TASK_HCI_ASYNCH_EVT_ID,
/* USER CODE BEGIN CFG_Task_Id_With_HCI_Cmd_t */
    CFG_TASK_SW1_BUTTON_PUSHED_ID,                                              /* Code Line to add */
/* USER CODE END CFG_Task_Id_With_HCI_Cmd_t */
    CFG_LAST_TASK_ID_WITH_HCICMD,                                               /**< Shall be LAST in the list */
} CFG_Task_Id_With_HCI_Cmd_t;


  • In app_entry.c:

Define the callback for handling the interrupts from SW1 presses by adding code in FD_WRAP_FUNCTIONS User Code Section:

/* USER CODE BEGIN FD_WRAP_FUNCTIONS */
void HAL_GPIO_EXTI_Callback( uint16_t GPIO_Pin )
{                                                                                                 
  switch (GPIO_Pin)                                                                  
  {                                                                                             
    case SW1_User_Pin:                                                          
     APP_BLE_Key_Button1_Action();                                      
      break;                                                                                 
    default:                                                                                 
      break;                                                                                
  }                                                                                             
  return;                                                                                   
}                                                                                              
/* USER CODE END FD_WRAP_FUNCTIONS */


  • In app_ble.c:

Define function for SW1 action by adding code in FD_SPECIFIC_FUNCTIONS User Code Section:

/* USER CODE BEGIN FD_SPECIFIC_FUNCTIONS */
void APP_BLE_Key_Button1_Action(void)
{
  P2PS_APP_SW1_Button_Action();
}
/* USER CODE END FD_SPECIFIC_FUNCTIONS */


  • In app_ble.h:

Declare the APP_BLE_Button1_Action() function, in EF User Code Section:

/* Exported functions ---------------------------------------------*/
  void APP_BLE_Init( void );

/* USER CODE BEGIN EF */
void APP_BLE_Key_Button1_Action(void);        /* Code Line to add */
/* USER CODE END EF */


  • In custom_app.h:

Declare P2PS_APP_SW1_Button_Action function, in EF User Code Section:

/* Exported functions ---------------------------------------------*/
  void Custom_APP_Init( void );
  void Custom_APP_Notification( Custom_App_ConnHandle_Not_evt_t *pNotification );
/* USER CODE BEGIN EF */
  void P2PS_APP_SW1_Button_Action( void );        /* Code Line to add */
/* USER CODE END EF */


  • In custom_app.c:

Add SW1_Status variable in CUSTOM_APP_Context_t User Code Section:

/* Private typedef -----------------------------------------------------------*/
typedef struct
{
  /* My_P2P_Server */
  uint8_t               Switch_c_Notification_Status;
  /* My_Heart_Rate */
  uint8_t               Hrs_m_Notification_Status;
  /* USER CODE BEGIN CUSTOM_APP_Context_t */
  uint8_t               SW1_Status;                      /* Code Line to add */
  /* USER CODE END CUSTOM_APP_Context_t */

  uint16_t              ConnectionHandle;
} Custom_App_Context_t;

/* USER CODE BEGIN PTD */

/* USER CODE END PTD */


In the same file, update snippets shown. The following traces code is to indicate the Smartphone requests to enable or disable notifications and write requests on My_P2P_Server service.
In CUSTOM_STM_LED_C_WRITE_NO_RESP_EVT User Section:

/* Functions Definition ------------------------------------------------------*/
void Custom_STM_App_Notification(Custom_STM_App_Notification_evt_t *pNotification)
{
  /* USER CODE BEGIN CUSTOM_STM_App_Notification_1 */

  /* USER CODE END CUSTOM_STM_App_Notification_1 */
  switch(pNotification->Custom_Evt_Opcode)
  {
    /* USER CODE BEGIN CUSTOM_STM_App_Notification_Custom_Evt_Opcode */

    /* USER CODE END CUSTOM_STM_App_Notification_Custom_Evt_Opcode */

  /* My_P2P_Server */
    case CUSTOM_STM_LED_C_READ_EVT:
      /* USER CODE BEGIN CUSTOM_STM_LED_C_READ_EVT */

      /* USER CODE END CUSTOM_STM_LED_C_READ_EVT */
      break;

    case CUSTOM_STM_LED_C_WRITE_NO_RESP_EVT:
      /* USER CODE BEGIN CUSTOM_STM_LED_C_WRITE_NO_RESP_EVT */
      APP_DBG_MSG("\r\n\r** CUSTOM_STM_LED_C_WRITE_NO_RESP_EVT \n");
      APP_DBG_MSG("\r\n\r** Write Data: 0x%02X %02X \n", pNotification->DataTransfered.pPayload[0], pNotification->DataTransfered.pPayload[1]);
      if(pNotification->DataTransfered.pPayload[1] == 0x01)
      {
        HAL_GPIO_WritePin(Blue_Led_GPIO_Port, Blue_Led_Pin, GPIO_PIN_SET); 
      }
      if(pNotification->DataTransfered.pPayload[1] == 0x00)
      {
        HAL_GPIO_WritePin(Blue_Led_GPIO_Port, Blue_Led_Pin, GPIO_PIN_RESET); 
      } 
     /* USER CODE END CUSTOM_STM_LED_C_WRITE_NO_RESP_EVT */
      break;


In CUSTOM_STM_SWITCH_C_NOTIFY_ENABLED_EVT and CUSTOM_STM_SWITCH_C_NOTIFY_DISABLED_EVT User Sections:

case CUSTOM_STM_SWITCH_C_NOTIFY_ENABLED_EVT:
      /* USER CODE BEGIN CUSTOM_STM_SWITCH_C_NOTIFY_ENABLED_EVT */
      APP_DBG_MSG("\r\n\r** CUSTOM_STM_BUTTON_C_NOTIFY_ENABLED_EVT \n");

      Custom_App_Context.Switch_c_Notification_Status = 1;        /* My_Switch_Char notification status has been enabled */
      /* USER CODE END CUSTOM_STM_SWITCH_C_NOTIFY_ENABLED_EVT */
      break;

    case CUSTOM_STM_SWITCH_C_NOTIFY_DISABLED_EVT:
      /* USER CODE BEGIN CUSTOM_STM_SWITCH_C_NOTIFY_DISABLED_EVT */
      APP_DBG_MSG("\r\n\r** CUSTOM_STM_BUTTON_C_NOTIFY_DISABLED_EVT \n");

      Custom_App_Context.Switch_c_Notification_Status = 0;        /* My_Switch_Char notification status has been disabled */
      /* USER CODE END CUSTOM_STM_SWITCH_C_NOTIFY_DISABLED_EVT */
      break;


Add code snippets in Custom_App_Init() function to register the send notification task that is started when SW1 button is pressed, in CUSTOM_APP_Init User Section:

void Custom_APP_Init(void)
{
  /* USER CODE BEGIN CUSTOM_APP_Init */
  UTIL_SEQ_RegTask( 1<< CFG_TASK_SW1_BUTTON_PUSHED_ID, UTIL_SEQ_RFU, Custom_Switch_c_Send_Notification );

  Custom_App_Context.Switch_c_Notification_Status = 0;   
  Custom_App_Context.SW1_Status = 0;                 

  /* USER CODE END CUSTOM_APP_Init */
  return;
}


And code snippet to allow the task to run once SW1 is pressed, in FD_LOCAL_FUNCTIONS User Section:

/* USER CODE BEGIN FD_LOCAL_FUNCTIONS*/
  void P2PS_APP_SW1_Button_Action(void)
  {
    UTIL_SEQ_SetTask( 1<<CFG_TASK_SW1_BUTTON_PUSHED_ID, CFG_SCH_PRIO_0);

    return;
  }
/* USER CODE END FD_LOCAL_FUNCTIONS*/


Add code snippet for sending notification request to the smart phone, in Switch_c_NS User Section:

void Custom_Switch_c_Send_Notification(void) /* Property Notification */
 {
  if(Custom_App_Context.Switch_c_Notification_Status)
  {
    Custom_STM_App_Update_Char(CUSTOM_STM_SWITCH_C, (uint8_t *)NotifyCharData);
    /* USER CODE BEGIN Switch_c_NS*/
    if (Custom_App_Context.SW1_Status == 0)
    {
      Custom_App_Context.SW1_Status = 1;
      NotifyCharData[0] = 0x00;
      NotifyCharData[1] = 0x01;
    }
    else
    {
      Custom_App_Context.SW1_Status = 0;
      NotifyCharData[0] = 0x00;
      NotifyCharData[1] = 0x00;
    }

    if(Custom_App_Context.Switch_c_Notification_Status)
    {
      APP_DBG_MSG("-- CUSTOM APPLICATION SERVER  : INFORM CLIENT BUTTON 1 PUSHED \n ");
      APP_DBG_MSG(" \n\r");
      Custom_STM_App_Update_Char(CUSTOM_STM_SWITCH_C, (uint8_t *)NotifyCharData);
    } 
    else
    {
      APP_DBG_MSG("-- CUSTOM APPLICATION SERVER : CAN'T INFORM CLIENT -  NOTIFICATION DISABLED\n ");
    }

    return;
    /* USER CODE END Switch_c_NS*/
  }
  else
  {
    APP_DBG_MSG("-- CUSTOM APPLICATION : CAN'T INFORM CLIENT -  NOTIFICATION DISABLED\n ");
  }
  return;
}


  • In custom_stm.c:

Update Custom_STM_Event_Handler() function to manage My_LED_Char write, in CUSTOM_STM_Service_1_Char_1_ACI_GATT_ATTRIBUTE_MODIFIED_VSEVT_CODE User Section:

static SVCCTL_EvtAckStatus_t Custom_STM_Event_Handler(void *Event)
{
  []
 event_pckt = (hci_event_pckt *)(((hci_uart_pckt*)Event)->data);

  switch(event_pckt->evt)
  {
    case HCI_VENDOR_SPECIFIC_DEBUG_EVT_CODE:
      blecore_evt = (evt_blecore_aci*)event_pckt->data;
      switch(blecore_evt->ecode)
      {
        case ACI_GATT_ATTRIBUTE_MODIFIED_VSEVT_CODE:
        []
          else if(attribute_modified->Attr_Handle == (CustomContext.CustomLed_CHdle + CHARACTERISTIC_VALUE_ATTRIBUTE_OFFSET))
          {
            return_value = SVCCTL_EvtAckFlowEnable;
            /* USER CODE BEGIN CUSTOM_STM_Service_1_Char_1_ACI_GATT_ATTRIBUTE_MODIFIED_VSEVT_CODE */
            Notification.Custom_Evt_Opcode = CUSTOM_STM_LED_C_WRITE_NO_RESP_EVT;
            Notification.DataTransfered.Length=attribute_modified->Attr_Data_Length;
            Notification.DataTransfered.pPayload=attribute_modified->Attr_Data;
            Custom_STM_App_Notification(&Notification);
            /* USER CODE END CUSTOM_STM_Service_1_Char_1_ACI_GATT_ATTRIBUTE_MODIFIED_VSEVT_CODE */
          } /* if(attribute_modified->Attr_Handle == (CustomContext.CustomLed_CHdle + CHARACTERISTIC_VALUE_ATTRIBUTE_OFFSET))*/
          /* USER CODE BEGIN EVT_BLUE_GATT_ATTRIBUTE_MODIFIED_END */

          /* USER CODE END EVT_BLUE_GATT_ATTRIBUTE_MODIFIED_END */
          break;


7.5. ST BLE Toolbox: P2P Server Notification And Write

If you are not familiar with ST BLE Toolbox Android[6]/iOS[5] application, a first introduction is available on ST BLE Toolbox Application chapter.


1. Scan and Connect
Open a serial terminal (see: TeraTerm Configuration chapter) and connect your smartphone to your board using ST BLE Toolbox application.
Once connected, the following message is displayed on TeraTerm.

P2P Server Connection logs


2. P2P Server Notification
Search and open P2P Server service.
Enable P2P Notify, on characteristic FE42 to receive notification from the STM32WB Nucleo board, using SW1 button as configured in previous example.

ST BLE Toolbox: Enable P2P Notify


  • When notifications have been enabled, the application displays the following message on the terminal:
Notification enabled logs


  • In the same way, when notifications are disabled, the following debug message is displayed on the terminal:
Notification disabled logs


Once notifications enabled, press SW1 button on Nucleo board to notify the P2P Server Characteristic.
The P2P Notify characteristic value toggles each time the SW1 button is pressed.

ST BLE Toolbox: Notify characteristic value


3. P2P Write
Using FE41 (LED_C) characteristic which is defined as a Write Without Response property, the P2P service writes data to the STM32WB Nucleo Board.
Press WRITE button and select Hexadecimal format puce1.png, then define the data to write puce2.png and press SEND button puce3.png to write it in the LED_C characteristic.

ST BLE Toolbox: P2P Write


  • Writing 0x0000 in 0xFE41 characteristic switch the LED 1 OFF.
  • Writing 0x0001 in 0xFE41 characteristic switch the LED 1 ON.

On the debug terminal, the message with the written data is displayed.

P2P Write logs

8. Code Generation

Once configuration is done in STM32CubeMX, the code can be generated puce1.png:

Code Generation


Project can then be open puce2.png:

Generated project pop-up


Open Project with IAR IDE, (\EWARM\ Project.eww) and ensure project options are correctly defined:

IAR Project Setup



Project build from IAR IDE:

  • Check there is no error when building the project from IAR.
Warning white.png Warning
Some build warnings could be listed due to declared functions but never referenced, or variables not used when pairing is off.
  • Connect the Nucleo board to the PC with USB cable.
  • Flash the binary file into the P-NUCLEO-WB55[8] board.
  • Run the application to make it advertise.
  • Connect MyCST application thanks to ST BLE ToolBox Android[6] or iOS[5] application. Refer to ST BLE Client Toolbox chapter.

9. TeraTerm Configuration

This chapter describe how to setup TeraTerm in order to display traces from the STM32WB projects.
The ST-Link of the Nucleo board is displayed as a Virtual COM Port (as shown in the Device Manager window below).
USART1 pins are routed through this port, which is connected to serial terminal (TeraTerm) to display traces.

Device Configuration manager


In TeraTerm interface, select the corresponding serial port:

TeraTerm Serial port selection


Set the Serial Port configuration as follow:

TeraTerm Serial port configuration


Once the TeraTerm is configured and connected to the Nucleo board you can run your code and the enabled logs must be displayed.

10. ST BLE Toolbox Application

The following chapter describes ST BLE ToolBox Android[6] or iOS[5] application utilization.

10.1. Scan and Connect

When you launch ST BLE ToolBox smartphone application, it scans to search WB devices. On the scan interface, the name (MyCST) of the application previously generated and build using STM32CubeMX and IAR must be displayed once discovered.

Select the application by clicking on his name, then click on Connect button:

ST BLE Toolbox: scan interface

10.2. Discover Services and Characteristics

When connected to MyCST, scroll on services to find the defined ones.

  • P2P Server Service:

Tap P2P Server to display the associated characteristics:

ST BLE Toolbox Services interface


As defined in STM32CubeMX we see P2P Server’s characteristics and associated properties:

puce1.png
Service P2P Server : UUID = 0xFE40
puce2.png
Characteristic 1 : UUID = 0xFE41 is Readable and Writable
puce3.png
Characteristic 2 : UUID = 0xFE42 is Notify
ST BLE Toolbox : P2P Server Characteristics interface


  • Heart Rate Service:

Tap Heart Rate to display the associated characteristics.

ST BLE Toolbox Services interface


As defined in STM32CubeMX we see Heart Rate’s characteristics and associated properties (tap details puce1.png):

  • Service Heart Rate : UUID = 0x180D
  • Characteristic 1 : UUID = 0x2A37 is Notify
  • Characteristic 3 : UUID = 0x2A38 is Readable
  • Characteristic 2 : UUID = 0x2A39 is Writable
ST BLE Toolbox : Heart Rate Characteristics interface


11. References