![]() |
Coming soon |
Click here for BLE overview
1. Titre 1
1.1. Titre 2
Ajouter une image de 800px de large et centrée :
Créer un lien:
Test Lien
retour ligne
retour ligne
liste:
- element 1
- element 2
- element 3
Test
2. Introduction
This document defines how to create a BLE server custom application on a STM32WB55RG MCU using STM32CubeMX (from v6.3.0).
3. Build a BLE an application on STM32WB with CubeMX
The created device can report values to mobile phone and receive commands from it.
System illustration |
---|
This GATT Server application shall be able to expose 2 services:
- 1st service exposes 2 characteristics
- 2nd service exposes 3 characteristics
The first service (My_P2P_Server) looks like P2P Server (STM proprietary) with 2 characteristics:
- Characteristic 1 has Write property
- Characteristic 2 has Notify property
Writing to characteristic 1 toggles blue LED.
Pressing SW1 on Nucleo board send data to the phone
Custom Service illustration |
---|
The second service (My_Heart_Rate) will be build as a SIG Heart Rate, but the behavior won't be managed.
The following steps are recommended to build this application example:
- CubeMX initialization for STM32WB55RGVx
- STM32WB application configuration
- Clock configuration
- IP configuration
- System configuration (WPAN)
- BLE GAP/GATT Custom Application Configuration
Services and Characterics configuration are given in the following table:
P2P Server and Heart Rate services configuration |
---|
4. Tools
4.1. Software tools
To make and use this project, the needed software tools to complete the application:
- STM32CubeMX v6.3.0
- STM32CubeWB v1.12.0 (or the last one)
- IAR IDE v8.20.2 (at least)
- Serial Terminal (TeraTerm)
- ST BLE Toolbox app (iOS or Android)
4.2. Hardware Tools
A STM32WB Nucleo board and a micro-B to Type-A USB cable are also needed.
Hardware presentation |
---|
The PC is connected to the ST-LINK connector of the NUCLEO board (right connector from the top view
ST-LINK connection |
---|
5. CubeMX initialization for P-NUCLEO-WB55
5.1. STM32CubeMX initial setup
Open STM32CubeMX and start a new project from the "Access to MCU selector" button
New Project Menu |
---|
Chose the MCU and then start the new project:
Project Interface |
---|
5.2. Pinout and IP configuration
To configure the system, enable all the required system resource and peripherals clicking on A->Z to display all IPs.
Pinout & Configuration Interface |
---|
BLE mode is reachable once the following system resources and peripherals are turned to enable.
- HSEM :activated
- IPCC : activated, ITs enabled
- RCC : HSE and LSE on Crystal/Ceramic resonator
- RTC : activate clock source and enable internal wakeup
- RF : activate RF1
- STM32WPAN : BLE
IP list |
---|
5.2.1. HSEM
The Hardware SEMaphore (HSEM) is needed to manage shared resources between the two CPU cores in the STM32WB.
HSEM activation |
---|
5.2.2. IPCC
Configuration of Inter-Processor Controller Communication (IPCC) is done as follow:
IPCC activation & setup |
---|
5.2.3. RCC
On Reset and Clock Controller (RCC), High Speed clock (HSE) and Low Speed Clock (LSE) are mandatory for BLE radio.
RCC setup |
---|
5.2.4. RTC
Configuration of Real Time Counter (RTC) is done as follow:
RTC activation & setup |
---|
5.2.5. RF
Activate RF1:
RF activation |
---|
5.2.6. BLE
Finally, under STM32_WPAN check BLE box:
BLE activation |
---|
5.3. Clock configuration
On clock configuration tab, run the automatic clock issue solver:
Then:
Clock configuration |
---|
5.4. Project manager
All the project configuration is done on the Project Manager pane within 3 sections, and done as follow :
5.4.1. Project
Project configuration |
---|
5.4.2. Code Generator
Manages files, packages and embedded software packs
Project generation |
---|
5.4.3. Advanced Settings
Definition of drivers to use (HAL/LL) and generated function calls
Advanced settings interface |
---|
6. BLE GAP/GATT Custom application configuration
- BLE Peripheral Custom Template GATT Server Application can be defined:
- On STM32WB
- With STM32CubeMX
- GAP peripheral : advertising configuration
- GATT server configuration:
- 5 services maximum
- 5 characteristics maximum per service
- ACI commands:
- AN5270 : STM32WBx5 Bluetooth® Low Energy (BLE) wireless interface[1].
- AN5270 : STM32WBx5 Bluetooth® Low Energy (BLE) wireless interface[1].
6.1. BLE Applications and Services
To start the definition of the BLE application :
STM32_WPAN Interface: Application & Services Settings |
---|
6.2. Advertising Configuration
Advertising parameters are defined under BLE Advertising tab:
- advertising configuration data are located in app_conf.h and ble_conf.h files
- advertising elements data are located in app_ble.c file
STM32_WPAN Interface: BLE Advertising tab |
---|
Open Advertising Configuration and set the CFG_GAP_DEVICE_NAME to something of your liking, for example MY_APPLI.
STM32_WPAN Interface: BLE Advertising configuration |
---|
In the generated code these parameters are defined in :
1. app_conf.h file:
- #define ADV_TYPE
- #define BLE_ADDR_TYPE
- #define FILTER
- #define CFG_GAP_DEVICE_NAME
2. ble_conf.h file:
- #define BLE_CFG_PERIPHERAL
- #define BLE_CFG_CENTRAL
STM32_WPAN Interface: BLE Advertising configuration 2 |
---|
In Advertising elements:
- Turn to “yes” the elements to add in the advertising packet payload as described in the image below
.
Here we set 4 advertising elements:
- Tx power
- Complete local name
- 16 bits service UUID
- Manufacturer specific data - Set the value for the other elements as mentioned in the image below
.
STM32_WPAN Interface: Advertising elements |
---|
The advertising information is represented by advertising data elements, which are standardized on the Bluetooth SIG.
These elements are included in the advertising packet payload and are located in app_ble.c file (here the advertising packet structure’s length = 19 bytes).
Advertising elements: corresponding code |
---|
6.3. Services and Characteristics Definition
All created services and characteristics are managed in custom_stm.c file. Each service and characteristic is added in SVCCTL_InitCustomSvc() function using:
- aci_gatt_add_service(…) for services,
- aci_gatt_add_char(…) for characteristics.
6.3.1. Services Definition
Each created service is defined in a dedicated CubeMX tab:
- Up to 5 Characteristics per Service
- UUID type can be defined as 16 or 128 bits
- UUID definition
- Type value is Primary or Secondary Service
A custom application can define up to 5 services.
In the following example, we define 2 Services, My_P2P_Server and My_Heart_Rate.
You can set the number of service to define in the BLE GATT tab:
BLE GATT services definition |
---|
For each defined service, set the number of Characteristics.
2 Characteristics for My_P2P_Server service.
BLE GATT services definition |
---|
3 Characteristics for My_Heart_Rate service.
BLE GATT services definition |
---|
6.3.2. Characteristics Definition
For each Characteristic the following parameters must be defined
- General
- Properties
- Permissions
- GATT events
My_P2P_Server Characteristics:
My_P2P_Server service have 2 characteristics, LED_C and SWITCH_C.
Defined as follow:
MY_P2P_Server characteristics definition |
---|
My_Heart_Rate Characteristics:
My_Heart_Rate service have 3 characteristics, My_HRS_Meas, My_Sensor_loc and My_HRS_CTRL_Point.
Defined as follow:
My_Heart_Rate characteristics definition |
---|
6.3.3. Pairing Definition
Pairing is done to support secure connection method.
All pairing parameters defined in the BLE_Pairing tab are located in app_conf.h file.
When PAIRING_PARAMETERS is set to ON, pairing parameters are available on the interface and can be defined as follow:
Pairing definition |
---|
Once configuration is done in STM32CubeMX, the code can be generated by following the steps described in Code Generation chapter.
7. Enable Traces
7.1. USART Configuration
Go to USART1 setup interface and select Asynchronous Mode:
USART Setup Interface |
---|
Then, go to DMA Settings tab , click on Add button
and select USART1_TX
.
USART Setup : DMA Settings |
---|
Ensure DMA1 Channel1 is selected, and click on USART1_TX line to show DMA Request Settings.
USART Setup : DMA Settings 2 |
---|
Go to NVIC Settings tab and enable USART1 global interrupt
.
USART Setup : NVIC Settings |
---|
7.2. NVIC Configuration
Go to NVIC Settings interface and set DMA1 Channel 1 global interrupt Preemption Priority to 15 (lowest priority)
.
Check that USART1 global interrupt is enabled .
7.3. USART1 Pinout Definition
Go to Pinout view .
Set UASRT1_TX on PB6 and USART1_RX on PB7:
- Click on PB6
- Select USART1_RX in the list
- Click on PB7
- Select USART1_TX in the list
You can use the search located in the bottom right of the pinout view window to find a pin or signal name easily (here PB6 and PB7)
Pinout View |
---|
7.4. STM32_WPAN Configuration
Go to STM32_WPAN setup interface and select the Configuration tab .
Enable the application traces , set CFG_DEBUG_TRACES_UART on hw_uart1
.
Configure the debug traces to manage the different types of logs .
STM32WPAN Setup |
---|
7.5. Project Manager Settings
Go to Project Manager interface and select the Advanced Settings tab
.
Configure MX_UASRT1_UART_Init function as:
- Check Do Not Generate Function Call checkbox.
- Uncheck Visibility (Static) checkbox.
MX_UASRT1_UART_Init function Settings |
---|
Once the traces configuration is done in STM32CubeMX, the code can be generated by following the steps described in Code Generation chapter.
7.6. Add USER CODE section in app_entry.c
In order to make the application able to manage debug messages, app_entry.c file must be updated.
In MX_APPE_Init() function, add a call to APPD_Init() function into the USER CODE APPE_Init_1 section as follow:
void MX_APPE_Init( void )
{
System_Init( ); /**< System initialization */
SystemPower_Config(); /**< Configure the system Power Mode */
HW_TS_Init(hw_ts_InitMode_Full, &hrtc); /**< Initialize the TimerServer */
/* USER CODE BEGIN APPE_Init_1 */
APPD_Init();
/* USER CODE END APPE_Init_1 */
appe_Tl_Init(); /* Initialize all transport layers */
Open a debug terminal as TeraTerm connected on USART1 to display application messages. Refer to TeraTerm Setup chapter.
8. User Button and LED configuration and use
8.1. Switch and LED pinout
In the Nucleo board, LED pinout is:
- Blue LED : PB5
- Green LED: PB0
- Red LED: PB1
Switch pinout is:
- SW1: PC4
- SW2: PD0
- SW3: PD1
When used:
- Switch pins are declared as GPIO_EXTIx (x = pin number)
- LED pins are declared as GPIO_OUTPUT
8.2. Blue LED Setup
Go to Pinout & Configuration -> Pinout View Interface , click on PB5
and select GPIO_OUTPUT
.
Blue LED Pinout |
---|
In Pinout & Configuration interface, go to the GPIO tab .
Select the GPIO line corresponding to PB5 and configure the PB5 configuration pane
as follow:
- GPIO Mode: Output Push/Pull
- GPIO Pull-up/Pull-down: No Pull-up and no pull-down
- User Label: Blue_Led
Blue LED : GPIO Configuration |
---|
8.3. SW1 Button Setup
Go to Pinout & Configuration -> Pinout View Interface , click on PC4
and select GPIO_EXTI4
.
SW1 Button Pinout |
---|
In Pinout & Configuration interface, go to the GPIO tab .
Select the GPIO line corresponding to PC4 and configure the PC4 configuration pane
as follow:
* GPIO Mode: External Interrupt Mode with Rising edge trigger detection
- GPIO Pull-up/Pull-down: Pull-up
- User Label: SW1_User
SW1 Button : GPIO Configuration |
---|
Go to NVIC interface and click on the NVIC tab
.
Enable the EXTI line4 interrupt , this interrupt corresponds to SW1.
SW1 Button : GPIO Configuration |
---|
8.4. Code Modification : USER Sections
Once your SW1 Button and Blue LED GPIOs are correctly setup, generate your code, you can refer to the ... chapter.
9. Code Generation
Once configuration is done in STM32CubeMX, the code can be generated :
Code Generation |
---|
Generated project pop-up |
---|
In IAR IDE, ensure project option are correctly defined:
IAR Project Setup |
---|
Project build from IAR IDE:
- Check there is no error when building the project from IAR.
- Connect the Nucleo board to the PC with USB cable.
- Flah the binary file into the P-NUCLEO-WB55[2] board.
- Run the application to make it advertise.
- Connect MyCST application thanks to ST BLE ToolBox Android[3] or iOS[4] application. Refer to ST BLE Client Toolbox chapter.
10. TeraTerm Configuration
This chapter describe how to setup TeraTerm in order to display traces from the STM32WB projects.
The ST-Link of the Nucleo board is displayed as a Virtual COM Port (as shown in the Device Manager window below).
USART1 pins are routed through this port, which is connected to serial terminal (TeraTerm) to display traces.
Device Configuration manager |
---|
In TeraTerm interface, select the corresponding serial port:
TeraTerm Serial port selection |
---|
Set the Serial Port configuration as follow:
TeraTerm Serial port configuration |
---|
Once the TeraTerm is configured and connected to the Nucleo board you can run your code and the enabled logs must be displayed.
11. Client ST BLE Toolbox
The following chapter describes ST BLE ToolBox Android[3] or iOS[4] application utilization.
11.1. Scan and Connect
When you launch ST BLE ToolBox smartphone application, it scans to search WB devices. On the scan interface, the name (MyCST) of the application previously generated and build using STM32CubeMX and IAR must be displayed once discovered.
Select the application by clicking on his name, then click on Connect button:
ST BLE Toolbox: scan interface |
---|
11.2. Discover Services and Characteristics
When connected to MyCST, scroll on services to find the defined ones.
- P2P Server Service:
Tap P2P Server to display the associated characteristics:
ST BLE Toolbox Services interface |
---|
As defined in STM32CubeMX we see P2P Server’s characteristics and associated properties:
ST BLE Toolbox : P2P Server Characteristics interface |
---|
- Heart Rate Service:
Tap Heart Rate to display the associated characteristics.
ST BLE Toolbox Services interface |
---|
As defined in STM32CubeMX we see Heart Rate’s characteristics and associated properties (tap details ):
- Service Heart Rate : UUID = 0x180D
- Characteristic 1 : UUID = 0x2A37 is Notify
- Characteristic 3 : UUID = 0x2A38 is Readable
- Characteristic 2 : UUID = 0x2A39 is Writable
ST BLE Toolbox : Heart Rate Characteristics interface |
---|