STM32WB-WBA GATT Data Base and bonded devices information storage

Under construction.png Coming soon

1. STM32WB - BLE GATT DB SRAM computation

How to calculate CFG_BLE_NUM_GATT_ATTRIBUTES ? Defines the maximum number of attribute records related to all the required characteristics that can be stored in the GATT database, for the specific BLE user application

For each characteristic, the number of attribute records goes from two to five depending on the characteristic properties:

minimum of two (one for declaration and one for the value)
add one more record for each additional property: notify or indicate, broadcast, extended property.

The total calculated value must be increased by 9, due to the records related to the standard attribute profile and GAP service characteristics, and automatically added when initializing GATT and GAP layers

Min value: <number of user attributes> + 9
Max value: depending on the GATT database defined by user application

GATT default - Number of GATT attributes

Example of DIS service - Number of GATT attributes

Example of service including characteristic with notification - Number of GATT attributes

Example of service including characteristic with notification and user description descriptor - Number of GATT attributes

How to calculate CFG_BLE_NUM_GATT_SERVICES ? Defines the maximum number of services that can be stored in the GATT database. Note that the GAP and GATT services are automatically added at initialization so this parameter must be the number of user services increased by two.

Min value: <number of user service> + 2
Max value: depending GATT database defined by user application

How to calculate CFG_BLE_ATT_VALUE_ARRAY_SIZE ? Defines the size of the storage area for the attribute values

Each characteristic contributes to the Attribute Value Array Size as follow:
Characteristic value length plus:
– 5 bytes if characteristic UUID is 16 bits
– 19 bytes if characteristic UUID is 128 bits
– 2 bytes if characteristic has a server configuration descriptor
– 2 bytes * CFG_BLE_NUM_LINK if the characteristic has a client configuration descriptor
– 2 bytes if the characteristic has extended properties
Each descriptor contributes to the Attribute Value Array Size as follow:
Descriptor length

Example of DIS service - Attribute Value Array Size

Example of service including characteristic with notification - Attribute Value Array Size

Example of service including characteristic with notification and user description descriptor - Attribute Value Array Size

Moreover, it is necessary to add characteristics related to the default GATT services.

For example: 
Service change characteristic (if not removed): 9 (5+2+2), 2 for indicate, 2 for number of link
Device Name: 13 (5+2+6), 2 for broadcast, 6 for name length
Appearance: 7 (5+2), 2 for attribute length
Peripheral Preferred Connection Parameters: 13 (5+8), 8 for attribute length

For this case

default value array size: 9 + 31 =  42 bytes

2. STM32WB - BLE GATT DB and security record in NVM

The GATT record in NVM is composed

per service
2 bytes for handle
3 or 17 bytes for UUID
per characteristic attribute
2 bytes for handle
3 or 17 bytes for UUID
2 bytes for CCCD value (only if the attribute is a CCCD)
This is size_of_gatt record

Example of DIS service - GATT DB stored in NVM

Example of service including characteristic with notification - GATT DB stored in NVM

Example of service including characteristic with notification and user description descriptor - GATT DB stored in NVM

The security record in NVM is fixed and equal to

80 bytes
This is size_of_sec_record

3. STM32WB - BLE number of bonded devices in NVM

Regarding the size of NVM, the computation of number of bonded devices that can be "theoretically" stored in NVM is the following:

n = (total_size_of_nvm-1) / [ (size_of_sec_record+1) + (size_of_gatt record+1) ]

Here:

total_size_of_nvm = 507 words (fixed in M0)

size_of_sec_record = 20 words (this is a constant from the BLE stack)

The GATT record is composed the following way:

per service
  • 2 bytes for handle
  • 3 or 17 bytes for UUID
per characteristic attribute
  • 2 bytes for handle
  • 3 or 17 bytes for UUID
  • 2 bytes for CCCD value (only if the attribute is a CCCD)

3.1. Example 1

Default GATT configuration without adding services:

GATT record = 12 words
47 bytes for default

3.2. Example 2

Default GATT configuration + 1 empty service with UUID_16

GATT record = 13 words
47 bytes for default
+ 5 bytes for the service

3.3. Example 3

Default GATT configuration + 1 service with UUID_16 + 1 characteristic with UUID_16

GATT record = 18 words
47 bytes for default
+ 5 bytes for the service 
+ 5 bytes for the 1st characteristic attribute
+ 5 bytes for the  2nd characteristic attribute
+ 7 bytes for the 3rd characteristic attribute (CCCD)

If we consider the example used in section 1 and 2

Example - GATT DB stored in SRAM and in NVM

Formula to calculate Total Buffer Gatt Size

(number of services) x 48 + (number of attributes) x 40 + CFG_BLE_ATT_VALUE_ARRAY_SIZE
In previous example, 
size_of_gatt record is equal to 614 bytes

Formula to calculate the number of bonded devices that can be stored in NVM

n = (total_size_of_nvm-1) / [ (size_of_sec_record+1) + (size_of_gatt record+1) ]

3.4. General information concerning NVM

We don’t store values of attributes, only the CCCD value.

it is applicable for GATT server.

On client side it is not at all used. On server side it is used to: - check if services have changed - keep CCCD in memory

3.5. References