Revision as of 15:50, 9 November 2021 by Registered User (→‎Introduction)
Under construction.png Coming soon

Click here for BLE overview

1. Introduction

The STM32CubeWB MCU Package[1] provides software components running on the STM32WB Series MCU.
For all examples provided with the package, the following integrated development environments are supported:

  • STMicroelectronics integrated development environment for STM32 products (STM32CubeIDE)
  • IAR Systems® IAR Embedded Workbench® for Arm® (EWARM)
  • Keil® Microcontroller Development Kit (MDK-ARM)

The Firmware Package for the STM32WB series is also available on STM32CubeWB github[2].

It contains the following Bluetooth® LE applications delivered as source code.

  • BLE SIG Application
    • Beacon
    • Blood Pressure Monitor
    • Health Thermometeher Sensor.
    • Herat Rate sensor.
    • Human Interface Device for Mouse & Keyboard.
    • Find Me & Promixity device -- > device with Immediate Alert, Link Loss Servcies.
  • proprietary
    • Command AT Server.
    • Cable Replacement.
    • Data Throughput Measurement.
    • Peer to Peer Application.
  • BLE Mesh Application

2. STM32WB Bluetooth® LE Software Architecture

The STM32WB Bluetooth Low Energy architecture separates the Bluetooth Low Energy Profile and Application, running on the application Cortex-M4, from the Bluetooth Low Energy real-time aspects residing in the Bluetooth Low Energy peripheral.

The Bluetooth Low Energy peripheral incorporates a Cortex-M0+ processor containing the Bluetooth Low Energy STACK handling the link layer up to the Generic Attribute Profile and Generic Access Profile layers.

STM32WB BLE Architecture

More information is available on the Application Note Building wireless applications with STM32WB Series microcontrollers[3]

3. Bluetooth® LE SIG Profile application

  • Heart Rate Sensor
  • ...

4. Proprietary Application

5. BLE Mesh

6. STM32CubeWB versions

7. Concepts