1. What is NanoEdge AI Library for classification?
NanoEdge™ AI Library is an Artificial Intelligence (AI) static library originally developed by Cartesiam, for embedded C software running on Arm® Cortex® microcontrollers.
When embedded on microcontrollers, it gives them the ability to easily "classify" sensor patterns, by themselves, without the need for the user to have additional skills in Mathematics, Machine Learning, or data science.
The NanoEdge AI static library for classification is the code that contains an AI model (for example, as a bundle of signal treatment, Machine Learning model, or optimally tuned hyperparameters) designed to identify a sensor pattern in a class. All classes are defined by the user in NanoEdge AI Studio (NanoEdgeAIStudio), also called the Studio) and are used during the training process of the AI model.
2. Install / Getting started
The main functions available via the library are:
knowledge_init()
|
run first before the classification process to load the knowledge |
classifier()
|
run a classification iteration (inference) |
2.1. Static library
The static NanoEdge AI Library is only available via NanoEdge AI Studio in its full version.
- In NanoEdge AI Studio, after obtaining a library, click Compile (on the "Deploy" screen, which follows the "Optimize and Benchmark" and "Emulator" screens)
- Open the .zip file obtained
- Select and copy the static library
libneai.a
- Link this static library to your project code
2.2. NanoEdge AI Library functions
2.2.1. Initialization
uint8_t NanoEdgeAI_knowledge_init(const float knowledge_buffer[]);
Initialization must be called at the beginning to load the knowledge.
- Input:
const float knowledge_buffer[]
, this buffer is defined in the header file knowledge.h provided in the .zip file containing the static NanoEdge AI Library.
- Output:
0
means success (the knowledge has been loaded), other values mean that loading has failed.123
: the library is being used on a board that is not authorized (only for libraries that are limited to partner/authorized development boards).
2.2.2. Classification
uint16_t NanoEdgeAI_classifier(float input_buffer[], float output_buffer[], uint8_t class_threshold);
This function returns the class identifier.
- Input:
float input_buffer[]
, the length of the buffer isDATA_INPUT_USER * AXIS_NUMBER
.float output_buffer[]
, the length of the buffer isCLASS_NUMBER
.uint8_t class_thresold
,0
or1
.
- Output:
- The class identifier (the input signal has been classified).
2.2.3. Getting status
uint8_t NanoEdgeAI_get_status_classifier(void)
This function returns the current status of the library.
- Input: None
- Output: The status of the library.
0
: the library is successfully deployed and ready to be used.123
: the library is being used on a board that is not authorized (only for libraries that are limited to partner/authorized development boards).
2.3. Example "Hello World!"
Header files:
NanoEdgeAI.h and knowledge.h (provided in the .zip file that you download by clicking Compile in NanoEdge AI Studio (on the "Deploy" screen after obtaining a library)
Example of NanoEdge AI Library header file:
/*
/**
* Copyright (c) 2021 STMicroelectronics.
* All rights reserved.
*
* This software component is licensed by ST under Ultimate Liberty license
* SLA0044, the "License"; You may not use this file except in compliance with
* the License. You may obtain a copy of the License at:
* www.st.com/SLA0044
*
******************************************************************************
*/
/* Includes */
#include <stdint.h>
/* Define */
#define NEAI_ID "5d5fd41ec8e0327c934"
#define AXIS_NUMBER 3
#define DATA_INPUT_USER 256
#define CLASS_NUMBER
/* Input and output buffers */
float input_user_buffer[DATA_INPUT_USER * AXIS_NUMBER];
float output_class_buffer[CLASS_NUMBER];
/* Array for mapping class id to class name */
const char *id2class[CLASS_NUMBER + 1] = {
"unknown",
"stop",
"low",
"medium",
"high"
};
/* Function prototypes */
#ifdef __cplusplus
extern "C" {
#endif
uint8_t NanoEdgeAI_knowledge_init(const float knowledge_buffer[]);
uint16_t NanoEdgeAI_classifier(float input_buffer[], float output_buffer[], uint8_t class_threshold);
#ifdef __cplusplus
}
#endif
Main program: main.c
This program must be completed by the user (depending on the applications or the desired features).
/**
* Copyright (c) 2021 STMicroelectronics.
* All rights reserved.
*
* This software component is licensed by ST under Ultimate Liberty license
* SLA0044, the "License"; You may not use this file except in compliance with
* the License. You may obtain a copy of the License at:
* www.st.com/SLA0044
*
******************************************************************************
*/
/* Includes -------------------------------------------------------------------*/
#include "NanoEdgeAI.h"
#include "knowledge.h"
/* Private define -------------------------------------------------------------*/
/* Private variables defined by user ------------------------------------------*/
/* Private function prototype defined by user ---------------------------------*/
/*
* @brief Collect data process
*
* This function is defined by user, depends on applications and sensors
*
* @param sample_buffer: [in, out] buffer of sample values
*
* @retval None
*/
void get_buffer(float sample_buffer[])
{
/* USER BEGIN */
/* USER END */
}
/* ----------------------------------------------------------------------------*/
int main()
{
/* Initialization ----------------------------------------------------------*/
uint8_t error_code = NanoEdgeAI_knowledge_init(knowledge);
if (error_code != 0) {
/* This happens if the knowledge is not loaded. */
}
/* Classification ----------------------------------------------------------*/
uint16_t id_class;
while (true) {
get_buffer(input_user_buffer);
id_class = NanoEdgeAI_classifier(input_user_buffer, output_class_buffer, 0);
/* USER BEGIN */
/*
* e.g.: Trigger functions depending on id_class
* (print output class probabilities using output_class_buffer[],
* print the name of the identified class using id2class[id_class],
* blink LED, ring alarm, etc.).
*/
/* USER END */
}
}
3. Resources
Documentation
All NanoEdge AI Studio documentation is available here.
Tutorials
Step-by-step tutorials, to use NanoEdge AI Studio to build a smart device from A to Z.