Revision as of 18:09, 25 October 2021 by Registered User (→‎Heart Rate Example)

1. Heart Rate Profile Presentation

Heart Rate Profile is a Generic Attribute Profile (GATT) based profile defined by the Bluetooth Special Interest Group (SIG).

The Heart Rate profile defines 2 roles, Sensor and Collector. Heart Rate Sensor is the device that measures heart rate and other information, it can be defined as a GAP peripheral and GATT server. The Collector is a GAP Central and GATT Client which receives heart rate measurement and other data.

The HRP is widely used in fitness applications to collect heart rate measurements.

2. Heart Rate Example

2.1. Requirements

2.1.1. Software and System requirements

Software required are the following:
IDE:

  • IAR Systems® v8.20.2
  • STM32CubeIDE[1].
  • Keil® µVision® v5.23

Programmer:

  • STM32CubeProgrammer[2] : To flash the board with an already generated binary

2.1.2. Hardware requirements

A Nucleo board[3], a STM32WB USB dongle[3], or a STM32WB Discovery Kit[4] is necessary to install the application.



Plus a smartphone with ST BLE Sensor application (for Android[5], or iOS[6]).

2.2. Setup

The "BLE_HeartRate" application is available by downloading STM32CubeWB release.

2.3. Project Description

Interaction between Middleware and User Application is described in the following illustration:


2.4. Build and Install

Follow steps described in BLE Build and Install Application page, applying it for BLE_HeartRate project.

2.5. Handle

Once the BLE Heart Rate application installed on the STM32WB platform, launch the ST BLE Sensor smartphone application.

Click on Connect one Device interface:

Your device should be visible from this interface, connect to it:

Now bpm measurement is displayed in real time.

Note: With Discovery Kit Platform, the Heart Rate is also visible from the board LCD screen, and Heart pulse is illustrated:

3. References