This message will disappear after all relevant tasks have been resolved.
Semantic MediaWiki
There are 1 incomplete or pending task to finish installation of Semantic MediaWiki. An administrator or user with sufficient rights can complete it. This should be done before adding new data to avoid inconsistencies.1. Heart Rate Profile Presentation
2. Heart Rate Example
2.1. Requirements
2.1.1. Software and System requirements
Software required are the following:
IDE:
- IAR Systems® v8.20.2
- STM32CubeIDE[1].
- Keil® µVision® v5.23
Programmer:
- STM32CubeProgrammer[2] : To flash the board with an already generated binary
2.1.2. Hardware requirements
A Nucleo board[3], a STM32WB USB dongle[3], or a STM32WB Discovery Kit[4] is necessary to install the application.
Plus a smartphone with ST BLE Sensor application (for Android[5], or iOS[6]).
2.2. Setup
The "BLE_HeartRate" application is available by downloading STM32CubeWB release.
2.3. Build and Install
Follow steps described in BLE Build and Install Application page, applying it for BLE_HeartRate project.
2.4. Handle
Once the BLE Heart Rate application installed on the STM32WB platform, launch the ST BLE Sensor smartphone application.
Click on Connect one Device interface:
Your device should be visible from this interface, connect to it:
Now bpm measurement is displayed in real time.