This message will disappear after all relevant tasks have been resolved.
Semantic MediaWiki
There are 1 incomplete or pending task to finish installation of Semantic MediaWiki. An administrator or user with sufficient rights can complete it. This should be done before adding new data to avoid inconsistencies.1. Heart Rate Profile Presentation
2. Heart Rate Example
2.1. Requirements
2.2. Software and System requirements
Software required are the following:
IDE:
- IAR Systems® v8.20.2
- STM32CubeIDE[1].
- Keil® µVision® v5.23
Programmer:
- STM32CubeProgrammer[2] : To flash the board with an already generated binary
2.3. Hardware requirements
A Nucleo board[3], a STM32WB USB dongle[3], or a STM32WB Discovery Kit[4] is necessary to install the application.
Plus a smartphone with ST BLE Sensor application (for Android[5], or iOS[6]).