STM32Cube.AI model performances

Revision as of 12:53, 10 August 2021 by Registered User

This article is providing benchmark of a set of well-known or reference pre-trained neural network models. Some STM32 results will be officially submitted to the MLPerf™ Tiny benchmark from MLCommons™.

Info white.png Information
  • STM32Cube.AI is a software aiming at the generation of optimized C code for STM32 and neural network inference. It is delivered under the Mix Ultimate Liberty+OSS+3rd-party V1 software license agreement (SLA0048).
  • Inference time, current and energy measures process is described, not done in a certified laboratory but can be reproduce by any user. The results are average values and will vary depending on the input data (random data are currently used), temperature and the STM32 device itself.
  • Published data on this article are not contractual.

1. Benchmark results

STM32 Board STM32
characterist.
Model
Source/Link
Flash
Wgt.
RAM
Buf.
Proc
Time
Current
(mA)
Energy
(mJ)
@ 3.3V
Version Comments
STM32H723
NUCLEO-H723ZG
Flash 1MB
RAM 564KB
(432KB)
Freq 550MHz
mobilenet v1
0.25 128 quant
source
500 KB 200 KB 10 ms NA NA Cube AI v7.0.0
Cube IDE v1.7.0
STM32H723
NUCLEO-H723ZG
Flash 1MB
RAM 564KB
(432KB)
Freq 550MHz
Anomaly Detection v0.5
MLPerf™Tiny
KB KB ms NA NA Cube AI v7.0.0
Cube IDE v1.7.0
STM32H723
NUCLEO-H723ZG
Flash 1MB
RAM 564KB
(432KB)
Freq 550MHz
Key Word Spotting v0.5
MLPerf™Tiny
KB KB ms NA NA Cube AI v7.0.0
Cube IDE v1.7.0
STM32H723
NUCLEO-H723ZG
Flash 1MB
RAM 564KB
(432KB)
Freq 550MHz
Image Classif. v0.5
MLPerf™ Tiny
KB KB ms NA NA Cube AI v7.0.0
Cube IDE v1.7.0
STM32H723
NUCLEO-H723ZG
Flash 1MB
RAM 564KB
(432KB)
Freq 550MHz
Visual Wake Word v0.5
MLPerf™Tiny
KB KB ms NA NA Cube AI v7.0.0
Cube IDE v1.7.0
STM32H743
NUCLEO-H743ZI
Flash 2MB
RAM 1MB
(512 KB)
Freq 480MHz
mobilenet v1
0.25 128 quant
source
KB KB ms NA NA Cube AI v7.0.0
Cube IDE v1.7.0
STM32H747 SMPS
STM32H747I-DISCO
Cortex® M7
Flash 2MB
(512 KB)
RAM 1MB
Freq 400MHz
mobilenet v1
0.25 128 quant
source
KB KB ms NA NA Cube AI v7.0.0
Cube IDE v1.7.0
On Cortex® M7 core in SMPS mode 400MHz instead of 480 max in LDO
STM32H7A3
NUCLEO-H7A3ZI-Q
Flash 2MB
RAM 1.4MB
(1.18 MB)
Freq 280MHz
mobilenet v1
0.25 128 quant
source
KB KB ms NA NA Cube AI v7.0.0
Cube IDE v1.7.0
STM32U585
B-U585I-IOT02A
Flash 2MB
RAM 786KB
Freq 160MHz
mobilenet v1
0.25 128 quant
source
KB KB ms NA NA Cube AI v7.0.0
Cube IDE v1.7.0
STM32L4R5
NUCLEO-L4R5ZI
Flash 2MB
RAM 640KB
Freq 120MHz
mobilenet v1
0.25 128 quant
source
KB KB ms NA NA Cube AI v7.0.0
Cube IDE v1.7.0

2. Measure process

On this benchmark only the machine learning model inference processing is reported. In a complete application, the sensor acquisition, the data conditioning and pre-processing shall also be considered.

The STM32 characteristics column provides the available internal Flash size, the full internal RAM size and the frequency. The RAM size includes the different kind of memories and banks, TCM, SRAM etc. For the time being, the buffers used by X-CUBE-AI shall be placed in a continuous memory area, the maximal RAM size available in continuous area is provided between "()" if not equal to the full size. The frequency indicated is the operating frequency used for the benchmark, so generally the maximal frequency. The only different case is with the STM32H747 Discovery Kit which is operating by default in SMPS power mode and therefore is limited to 400 MHz instead of 480 MHz.

The memory footprints are the one reported by X-CUBE-AI using the "Analyze" function (the version of X-CUBE-AI used is mentioned in the table).

The column Flash Wgt. reports the model weights occupancy in Flash.

The column RAM Buf. reports the RAM buffers occupancy used to store the model activations as well as input and output buffers. Note that to gain RAM space the "Use activation buffer for input buffer" and "Use activation buffer for the output buffer" options are selected (through X-CUBE-AI Advanced Settings panel).

The column Proc Time reports the model inference processing time. When the current / energy is indicated the measure is done thanks to X-CUBE-AI "System Performance" application following the process described on this WiKi article on power measurement. Otherwise the "Validation on target" application is used. In all case, when generating the application, the selected clock source is always the HSI, X-CUBE-AI is generating first the optimal clock settings and eventually afterwards the clock is set to HSI. STM32CubeMX then autonomously reconfigures the clock settings.

Current and Energy are computed following the process describe in the WiKi article on power measurement and specifically in the section 4.3.1 "Measure process when current is below 50 mA" (using 10 s windows for averaging) using HSI as clock source.

Accuracy is not reported. X-CUBE-AI is not modifying the DL/ML model topology. The impact on accuracy should be limited. X-CUBE-AI is providing through the "Validation" application a way to measure the accuracy either on x86 or on the target. It can be used to check the eventual impact on accuracy. When running the "Validation on target" application several metrics are computed, one of them is the X-Cross providing error metrics between the original model executed in Python and the C model executed on the target. Random data can be used to compute the RMSE/MAE/L2R errors. For all models reported here, the L2R (scalar value of the relative 2-norm or Euclidean distance between the generated values of the original model and the C-model) is below 0.01, so a low probability of significant impact on the accuracy. For more details on the metrics, please refer to the X-CUBE-AI Embedded Documentation. Note that accuracy check is important to compare a float model to a quantize model or when using the Weight compression feature of X-CUBE-AI for float modles.

No categories assignedEdit