STM32WB-WBA Zigbee memory requirements

Revision as of 17:51, 3 July 2024 by Registered User (→‎Memory consideration)


1. Introduction

The Zigbee stack is a software component designed to enable Zigbee communication on the STM32WB/WBA microcontroller. Like any software, the stack requires memory to operate. There are two main types of memory that are relevant to the stack: RAM and Flash memory.

RAM (Random Access Memory) is a type of volatile memory that is used for temporary storage of data and program code. The stack uses RAM to store data structures, variables, and other runtime objects. The amount of RAM required by the stack will depend on the application and the used features.
Flash memory, on the other hand, is a type of non-volatile memory that is used for long-term storage of program code and data. The stack uses Flash memory to store the code and data that make up the stack itself. The amount of Flash memory required by the stack will depend on.

Memory Types in Microcontrollers
Connectivity Types of memory in Microontroller.png

Another important concept to understand is memory allocation. The stack uses a heap to allocate memory dynamically at runtime. This means that the stack can allocate memory as needed, rather than requiring a fixed amount of memory to be allocated at compile time. However, this also means that the stack requires some amount of overhead to manage the heap.
Developers should carefully consider their application's requirements and consult the stack's documentation to determine the appropriate memory requirements.

2. Memory Layout of C Code

Microcontrollers Flash memory contains different segments of application code such as, interrupt vector table, code segment, initialized data segment, uninitialized data segment, constant data segment etc. The linker script file defines where each of these segments will store in flash memory.
These are the typical sections of a given C binary:

  1. Text Section: This section contains the machine code of the compiled C program. It is read-only and contains the instructions that the processor executes.
  2. Data Section: This section contains the initialized global and static variables of the program. It is writable and read-only.
  3. BSS Section: This section contains the uninitialized global and static variables of the program. It is writable and read-only.
  4. Heap Section: This section is dynamically allocated by the program during runtime. It is used for dynamic memory allocation. The heap area begins at the end of the BSS segment and grows upwards to higher memory addresses.
  5. Stack Section: This section is used for storing local variables and function parameters. It grows and shrinks as functions are called and returned. On the standard x86 architecture it grows downwards to lower addresses.
Simple Memory Layout of C Program
Connectivity memory organization.png

Heap is not automatically managed and should be explicitly allocated using malloc() for example, and deallocated using free(). So it is managed by the programmer.
Later, we will focus on heap memory and we will give formula to compute it on STM32WB for a given Zigbee application.

3. Startup File and Linker Script

The startup file and the linker script allow to initialize the microcontroller's hardware and link the various sections of the code together. The startup file includes functions that set up the stack, initialize the memory, and configure the clock and other peripherals so that the user application can run. The linker script determines how the code and data are organized in memory, it defines the ROM_start, ROM_end, RAM_start and RAM_end for example.

The following figure shows the memory map representation of the On/Off STM32WB55.Nucleo application example of the STM32Cube MCU Package. We have two separate linker files, the first for M4 and the second for M0, which is common and necessary to ensure that the code and data are placed in the correct memory regions for each core.

Connectivity Zigbee Memory map file example.png

4. STM32WB series

4.1. STM32WB Zigbee software architecture

As a reminder, the STM32WB MCUs are built with two separate cores, Arm® Cortex®-M4 and Arm® Cortex®-M0+ cores. The architecture is depicted in the figure below. Mainly, the M0 core contains the Zigbee stack, and the M4 core contains clusters and the developer’s application.

STM32WB Zigbee architecture
Connectivity Zigbee MCU STM32WB.png

STM32WB contains up to 1 Mbyte of flash memory single bank architecture, can be accessed starting from address 0x0000 0000 or 0x0800 0000, internal SRAM1 (up to 192 KB) and internal SRAM2a (32 KB) + SRAM2b (32 KB).
From system point of view, there are 2 heaps:

  • one on M4 side
  • one on M0 side to be used by Zigbee stack

4.2. STM32WB stack memory requirements

4.2.1. STM32WB stack heap size

The stack allocates run-time objects, such as packets, timers, and endpoints, using a heap. The application can configure the size of the heap using the ZbInit struct ZbInitTblSizesT parameters, specifically heapPtr and heapSz. The heap memory is allocated from the M4 core, allowing any memory, such as packets, passed between the M0 and M4 to be accessed and modified by either core.
M0 heap is included in M4 heap and allocated using ZbMalloc when ZbInit is called.

If ZbInit is called providing a NULL heapPtr, M0 heap will be allocated with default size depending on SW type:

  • FFD SW: 32 KB
  • RFD SW: 16 KB

4.2.2. STM32WB stack tables size

The following table describes the impact on memory usage for each additional entry:

Entry Type Memory Usage Per Entry (bytes)
Network Neighbor Table entry (nwkNeighborTblSz) 144
Network Routing Table entry (nwkRouteTblSz) 28
Network Address Mapping Table (nwkAddrMapTblSz) 24
APS Link Key Table (apsPeerLinkKeyTblSz) 48

Default network topology in FFD SW is:

  • ZB_NWK_NEIGHBOR_TABLE_DEFAULT_SIZE=16U
  • ZB_NWK_NLME_ADDRMAP_TABLE_DEFAULT_SIZE=16U
  • ZB_NWK_NLME_ROUTE_TABLE_DEFAULT_SIZE=16U
  • ZB_NWK_NLDE_BTT_TABLE_DEFAULT_SIZE=16U
  • ZB_NWK_NLME_RREQ_TABLE_DEFAULT_SIZE=4U
  • ZB_APS_DEVICE_KEY_PAIR_DEFAULT_COUNT=16U

With such configuration, overall M4 heap consumption is close to 52 KB with 32 KB allocated for M0 heap + fixed M0 allocation + variable memory size depending on topology.

To compute M4 heap requirement for a given topology, you can use below formula:

M4 heap size= (32+16)*1024 + neighb_table_size*144 + routing_table_size*28 + address_mapping_table_size*24 + aps_link_key_table_size*48
Info white.png Information
Formula is accurate +/-10%

4.2.3. Device Configuration And Memory Usage

Description nwkNeighborTblSz nwkRouteTblSz nwkAddrMapTblSz apsPeerLinkKeyTblSz Heap kB Total Memory kB
Coordinator, 30 Devices, 30 Neighbors / Children 30 30 30 30 32 54
Coordinator, 100 Devices, 40 Neighbors / Children 40 30 100 100 32 60
Coordinator, 200 Devices, 40 Neighbors / Children 40 30 200 200 32 67
Router, 30 Neighbors / Children 30 30 4 4 32 52
Router, 100 Neighbors / Children 100 30 4 4 32 61
End-Device, 8 Neighbors 8 0 2 2 8 14.5

Note: Total Memory includes some items with constant overhead, which are not listed in this table.

5. STM32WBA series

5.1. STM32WBA Zigbee software architecture

As a reminder, the STM32WBA MCUs are built with Arm® Cortex®-M33 core. The architecture is depicted in the figure below.

STM32WBA Zigbee architecture
Connectivity Zigbee MCU STM32WBA.png

STM32WBA5x devices contain a 1 Mbyte flash memory from address offset 0x00 0000 to 0x0F FFFF, and 128 KB of SRAM defined below:

  • SRAM1 region start = 0x20000000
  • SRAM1 region end = 0x2000FFFF
  • SRAM2 region start = 0x20010000
  • SRAM2 region end = 0x2001FFFF

STM32WBA6x devices contain a 2 Mbyte flash memory, and 512 KB of as defined below:

  • SRAM1 region start = 0x20000000
  • SRAM1 region end = 0x2003FFFF
  • SRAM2 region start = 0x20040000
  • SRAM2 region end = 0x2007FFFF

5.2. STM32WBA stack memory requirements

5.2.1. Memory consideration

The stack allocates run-time objects, such as packets, timers, and endpoints, using the heap. The stack needs also to configure different tables which depend on device capabilities and network topology. These values depend on the use case which is targeted. This is the reason why dynamic memory allocation is being used inside the stack. The FFD library requires more memory than the RFD library so it can handle routing packets and the overhead that entails.
Inside the Zigbee stack, two functions are used to allocate memory : ZIGBEE_PLAT_HeapMalloc() and ZIGBEE_PLAT_ZbMalloc()

  • ZIGBEE_PLAT_HeapMalloc() is used to allocate memory from the system during stack initialization (via ZbInit(..)), and it is not freed until calling ZbDestroy(..).
  • ZIGBEE_PLAT_ZbHeapMalloc() is used to allocate memory during the run-time operation of the stack. These are mostly short-lived memories, such as packets, timers, etc. Once the memory is no longer needed, it is freed by calling ZbHeapFree().

By default, these memory allocation APIs are linked to the ST memory manager. The relevant functions, including ZIGBEE_PLAT_ZbHeapInit(), ZIGBEE_PLAT_ZbHeapMalloc(), ZIGBEE_PLAT_ZbHeapFree(), ZIGBEE_PLAT_ZbInit(), ZIGBEE_PLAT_ZbMalloc(), and ZIGBEE_PLAT_ZbFree(), are defined within the Zigbee_plat.c file.By default, in the examples provided inside our Cube firmware, the ZIGBEE_PLAT_xx APIs are mapped to our Advanced Memory Manager. The size of the memory pool which is used by the advanced memory manager is available in the app_conf.h file and is specific to each example.For a more detailed information about the ST memory manager, please consult the resource provided in the STM32CubeWBA Memory Management wiki

These APIs are customizable and can be redefined to meet specific application requirements if necessary.

5.2.2. Typical memory footprint of a Zigbee Application

In our standard application examples, as included in our regular releases, we have used default parameters of the heap size and various Zigbee table sizes for all applications including SED ones. For more efficient use of memory, we implemented an optimized example of On/OFF Coordinator communicating with an On/Off SED. Below is a table that illustrates the optimized memory consumption values for both applications:

Application Flash (KB) RAM (KB)
R23 Zigbee_OnOff_Server_Coord (FFD) 438 82
Zigbee_OnOff_Client_SED (RFD) 370 39
R22 Zigbee_OnOff_Server_Coord (FFD) 381 82
Zigbee_OnOff_Client_SED (RFD) 329 39

Note that for next releases, we will include at least 2 applications examples using this optimized configuration for memory usage.


The details associated to a typical Zigbee Application acting as a router based on R23 is summarized below:

Component Type Flash consumption RAM consumption Comment
Zigbee R23 FFD ZigBeeProR23_FFD.a 324 KB 1KB + 67 KB of Heap reserved for dynamic allocation by the Application (typical value. Refer to chapter STM32WBA stack heap chapter for more details) Full R23 FFD Zigbee stack library including Green Power Proxy feature and traces
MAC wba_mac.lib.a 15 KB 3.1 KB
LinkLayer LinkLayer15_4.a 56 KB 5.3 KB
Clusters ZigbeeClusters.a

Can be delivered in source code on demand

At minimum : 1KB 0 KB It used the same heap pool as the one used by the Zigbee stack This is fully dependent on the Clusters selection done by the Application. To give some rough data, we can consider :

•       OnOff clusters less than 1KB bytes

•       All  Cluster Server  : 57 KB

•        All Zigbee Cluster Client: 22 KB

Appli src code At minimum : 4KB At minimum 2K Overall Cstack allocated : 4K This is fully dependent on the application Zigbee_OnOff_Router : 3KB
Infra src code At minimum : 38 KB At minimum 2K This includes the standard framewok and drivers used in the Applications provided inside the Firmware Cube delivery
TOTAL Binary ready to be flashed At minimum :438 KB At minimum 82 The Zigbee_OnOff_Server_Coord application provided in the firmware package consume 438 KB of flash and 82KB of RAM. This doesn’t include Flash used for persistent data

The Zigbee_FindBind_Coord application example consumes 450 KB of Flash and 82KB of RAM.

ST is providing several flavors of the stack as shown in the table below. The selection of the stack depends on the use case which is targeted. For an application in which the device will act as a sleepy end device for example, the RFD flavor of the stack should be used

Component Flash consumption RAM consumption Comment
Zigbee R23 FFD 324 KB 1KB + 67 KB of Heap reserved for dynamic allocation by the Application (typical value. Refer to chapter STM32WBA stack heap chapter for more details) Full R23 FFD Zigbee stack library including Green Power Proxy feature and traces
ZigBeeProR23_RFD 264/284 ? 1KB + 25 KB of Heap reserved for dynamic allocation by the Application  typical value. Refer to chapter STM32WBA stack heap chapter for more details)
ZigBeeProR22_FFD 266
ZigBeeProR22_RFD To be filled

5.2.3. STM32WBA stack heap size for an FFD device

The heap size has to be carefully tuned according to the use case targeted. A Router which wants to support a huge mesh network will have to allocate bigger routing tables than a simple router linked to one or two end devices. With the default setup available on the V1.4 Cube release, the Zigbee Router is able to address 32 end devices in parallel and will require at minimum 80Kb of RAM.
For both the Coordinator and Router device types, the number of neighbors or children the device can support is dependent on the size of the Network Neighbor Table (NNT). The NNT must be large enough to maintain the other Routers it is in direct contact with in order to route packets through the network, and also large enough to maintain any potential End-Device children which want to join to it. For more details refer to AN 059(a verifier).
All the Zigbee tables are allocated at startup dynamically when calling ZbInit()

ZbInit(uint64_t extAddr, struct ZbInitTblSizesT *tblSizes, struct ZbInitSetLoggingT *setLogging)

If the parameter tblSizes is set to 0, default table sizes are used by the stack to manage typical use cases (For ex : FFD : Router addressing 32 neighbors , RFD : End device addressing 16 neighbors on the V1.5 release)

On the V1.4 release (Default table sizes)

Default config FFD RFD Comment
ZB_NWK_NEIGHBOR_TABLE_DEFAULT_SIZE 32 32 This table stores information about devices that are within the radio range of a particular device. It typically includes the device's network address, extended address, relationship (parent, child, sibling), device type (coordinator, router, end device), and other link quality indicators.
ZB_NWK_NLME_ADDRMAP_TABLE_DEFAULT_SIZE 32 32 The Address Map table is used to map between the network address and the corresponding extended (IEEE 64-bit) address. This is useful for routing and for various network layer operations.
ZB_NWK_NLME_ROUTE_TABLE_DEFAULT_SIZE 32 32 This table contains the routing information that a device uses to send packets to other devices in the network. It includes entries for destination addresses and the next hop addresses to which frames should be forwarded to reach the destination.
ZB_NWK_NLDE_BTT_TABLE_DEFAULT_SIZE 32 NA The Broadcast Transaction Table is used to track broadcast messages and ensure they are only relayed once through the network. It helps prevent broadcast storms by keeping a record of the recent broadcasts and their transaction sequence numbers.
ZB_NWK_NLME_RREQ_TABLE_DEFAULT_SIZE 16 NA requests and manage the route discovery process.
ZB_APS_DEVICE_KEY_PAIR_DEFAULT_COUNT 32 32 This table is part of the Application Support Sublayer (APS) and is used for storing security key material related to other devices in the network. It includes the network address of the partner device and the associated link keys for secure communication.

On the V1.5 release

Default config FFD RFD
ZB_NWK_NEIGHBOR_TABLE_DEFAULT_SIZE 64 16
ZB_NWK_NLME_ADDRMAP_TABLE_DEFAULT_SIZE 32 2
ZB_NWK_NLME_ROUTE_TABLE_DEFAULT_SIZE 32 NA
ZB_NWK_NLDE_BTT_TABLE_DEFAULT_SIZE 32 9
ZB_NWK_NLME_RREQ_TABLE_DEFAULT_SIZE 16 NA
ZB_APS_DEVICE_KEY_PAIR_DEFAULT_COUNT 32 2

5.2.4. STM32WBA stack tables size

The following table describes the impact on memory usage for each additional entry:

Entry Type Memory Usage Per Entry (bytes)
Network Neighbor Table entry (nwkNeighborTblSz) 136
Network Routing Table entry (nwkRouteTblSz) 32
Network Address Mapping Table (nwkAddrMapTblSz) 24
APS Link Key Table (apsPeerLinkKeyTblSz) 88

Default network topology in FFD SW is:

  • ZB_NWK_NEIGHBOR_TABLE_DEFAULT_SIZE=32U
  • ZB_NWK_NLME_ADDRMAP_TABLE_DEFAULT_SIZE=64U
  • ZB_NWK_NLME_ROUTE_TABLE_DEFAULT_SIZE=16U
  • ZB_NWK_NLDE_BTT_TABLE_DEFAULT_SIZE=16U
  • ZB_NWK_NLME_RREQ_TABLE_DEFAULT_SIZE=4U
  • ZB_APS_DEVICE_KEY_PAIR_DEFAULT_COUNT=64U

6. Acronyms and definitions

Term Definition
APS Application Support Sublayer
RAM Random Access Memory
FFD Full Function Device
RFD Reduced Function Device
SED Sleepy End Device

7. References


[[Category:Getting_Started_with_STM32WB-WBA_and_Zigbee|10]]

No categories assignedEdit