How to start with DA access on STM32H7RS

Revision as of 14:13, 2 May 2024 by Registered User

How to start with DA access on STM32H7S


Literature


Target description

The purpose of this article is to explain step by step how to use the Debug Authentication STM32CubeFW example provided by ST.
The user application flashed during the provisioning is the GPIO_IOToggle example from STM32CubeFW, installed in external memory.

Info white.png Information
This step by step shows an example of Debug Authentication with NUCLEO-H7S3L8 board.

All the files used in this step by step are located in STM32Cube_FW_H7RS\Projects\NUCLEO-H7S3L8 folder.


Introduction

In this "getting started" a simple way to flash a user application in external memory and to provision the chip are shown based on the example provided in STM32CubeFW.

Through this practical example you will learn:

  • How to use the STM32CubeFW example which is provided.
  • How to configure the debug authentication for this example.
  • What the device provisioning is and how to perform the setup of the device.
  • How the user application is installed.
  • How to perform a regression to retrieve an empty board.

Prerequisites

  • Hardware
    • Nucleo-144 board NUCLEO-H7S3L8 board
SECURITY NUCLEO-H7S3L8 picture.png

STM32H7S devices have all the available security features, including the HW crypto accelerator.
The HW cryptographic acceleration is not support for STM32H7R devices. It is possible to follow this step by step with a STM32H7R, the encryption must be disable during the Debug Authentication configuration.

  • Required tools
    • STM32Cube_FW_H7RS_V1.0.0 or later
    • STM32CubeProgrammer_rev2.16.0 or more recent (with trusted package creator (TPC) selected at installation).
    • IAR Embedded Workbench® rev 9.20.1 or later.
    • Tera Term / Putty or equivalent terminal emulator.
Info white.png Information
The TPC installed together with CubeProgrammer in the bin folder located in default STM32CubeProgrammer path : C:\Program Files\STMicroelectronics\STM32Cube\STM32CubeProgrammer\bin You can pin this tool to the taskbar to simplify the "STiRoT Getting started" process :
Security PinToTask.png


  • STM32Cube Firmware
    • Download the STM32Cube_FW_H7RS Cube firmware (advise is to place it close form the C: in order to avoid long windows paths)
    • A directory NUCLEO-H7S3L8 is included in "STM32Cube_FW_H7RS\Projects"
SECURITY DA access env bat NUCLEO H7S.png
  • Open the env.bat file
  • If the STM32CubeProgrammer has not been installed in the default folder : C:\Program Files\STMicroelectronics\STM32Cube\STM32CubeProgrammer, the customized installation path needs to be updated.
  • Option bytes programming

The STM32CubeFW example GPIO_IOToggle used in this step by step is running in external memory and it is necessary to configure the option byte XSPI2_HSLV to make it work :

  • Open STM32CubeProgrammer
  • Connect the Nucleo board and configure the OB as follow :
  • Apply the change and disconnect STM32CubeProgrammer

1. Debug authentication configuration

This chapter explains how to start with the provisioning script.
It is used to configure the debug authentication.


1.1. Preliminary stage

  • The different steps to configure the DA are based on a script provided in the STM32CubeFW: Projects\NUCLEO-H7S3L8\ROT_Provisioning\DA\provisioning.bat.
  • The following documentation is a guide through all the steps of this script, and explains how to perform each of them.

The figure below shows where the script is located in the STM32CubeFW.

SECURITY provisioning script folder Nucleo H7S.png


  • Launch the script: provisioning.bat (double click) and keep it running during all the following steps.
    • Type the product state: CLOSED (don't use LOCKED for this tutorial, this state is used only to set a final product state)
    • Type the chosen Debug Authentication: CERTIFICATE (for explanation about certificate and password refer to intro article)
SECURITY provisioning script DA Nucleo board step1 prelim stage.png

1.2. Debug Authentication configuration

Press a key on terminal window and the script guide you to perform DA configuration :

Security H7S script configure DA.png
Warning white.png Warning
If you are using a STM32H7R device you have to modify the xml file to disable encryption as it is not supported on these devices.

Open DA_Config.xml configuration file in Projects\NUCLEO-H7S3L8\ROT_Provisioning\DA\Config with an editor as Notepad for example and set the parameter DoEncryption to 0 as it is shown below :

SECURITY Doencryption parameter.png
  • Using STM32TrustedPackageCreator
  1. Select the shield Security DA ICON STM32CubeProgrammer.png
  2. Select OBkey tab
  3. Select the DA_Config.xml configuration file in Projects\NUCLEO-H7S3L8\ROT_Provisioning\DA\Config. All the default settings for this hands-on are already filled-in .
  4. Generate OBkey
  5. A success message is displayed  : OBKey File Generation
Security H7S TPC DA config certif.png
Warning white.png Warning
In Information tab you can see if encryption option is enabled or disabled.

For the use of STM32H7S devices this option has to be enabled otherwise the board could be locked. For STM32H7R devices Encryption option must be disabled.
In order to modify the encryption option, open DA_Config.xml configuration file (or DA_Configwithpassword.xml file if you are using password method) in Projects\NUCLEO-H7S3L8\ROT_Provisioning\DA\Config with an editor as Notepad for example and set the parameter DoEncryption to 0 to disable the option, or to 1 to enable the encryption.

For a commercial product, it is important to define your own key. But for trials it is advised to use the default provided, to avoid blocked regression due to lost password.

According to the path specified in the DA_Config.xml, a DA_Config.obk file is generated in Projects\NUCLEO-H7S3L8\ROT_Provisioning\DA\Binary folder. This file will be used by the script during the provisioning step.

2. Provisioning

The step 2 corresponds to the provisioning of the OBKeys and the programming of the option bytes. This is automatically done by the script :

Security Nucleo H7S script step 2 provisioning.png

3. Images flashing

Next step is the programming of the images.

Security nucleo H7S script IMAGE FLASHING.png
Warning white.png Warning
Don't power off / on your board during this step

Check that the STM32H7RS IAR™ provided patch is correctly installed and check that your IAR Embedded Workbench™ version is recent enough.

For this step by step the 'GPIO_IOToggle code example is used. Is is executed from external memory. It is available in STM32CubeFW : Projects\NUCLEO-H7S3L8\Examples\GPIO\GPIO_IOToggle\EWARM

  • Open the project Project.eww.
  • In Project > Options > General Options > Target check that device is recognize as below, otherwise check that the patch in Utilities\PC_Software is well installed.
SECURITY Nucleo H7S device IAR options window.png
  • In Project > Options > STLINK > Setup change the Reset mode to "Software"
SECURITY Nucleo H7S IAR options window reset mode.png
  • This example is configured to download two images :
  • The application image GPIO_IOToggle installed and executed in external memory
  • The image Boot_XIP.hex that allow application image to be executed in external memory.

The parameters to download this extra image in flash are already configured in the IAR project in Project > Options > Debugger > Images  :

SECURITY Nucleo H7S IAR Boot-XIP config.png
  • Validate the modification by clicking OK
  • Perform Project > Rebuid all ,and once Build succeded select: Project > Download > Download active application
  • The two images are flashed

4. Setting the final product state and code execution

Press a key in terminal window and script sets the product state of the product to CLOSED, and code is executed.

Security H7S script end.png

You can see leds blinking on the NUCLEO board.

5. Full regression

Info white.png Information
This paragraph links to other wiki articles. The procedures described are applicable to this step by step, you only have to modify the default repository Projects\STM32H7S78-DK to Projects\NUCLEO-H7S3L8.

The product is now in closed state, but you can proceed to :

  • A full regression to recover an virgin device.

Please refer to Full regression using graphic interface or using the script provided in the STM32CubeFW

  • A debug opening

Refer to: OEMiRoT_Debug Opening

  • Download a new firmware from closed state :

Refer to this article: OEMiRoT_ Download a new firmware from a closed device