STM32WBA Build Zigbee project

Revision as of 11:46, 29 April 2024 by Registered User

1. Presentation

This page describes how to easily build and install an STM32WBA Zigbee application.
Project examples can be found in the STM32CubeWBA MCU package[1], and are available for different platforms.

The figure below shows an example of the STMicroelectronics Zigbee project structure.

STMicroelectronics Zigbee project example directory
Connectivity wba zigbee projects.png


2. Requirements

2.1. Software and hardware requirements

The following software is required:

Minimum IDE versions:

  • IAR Embedded Workbench® for Arm® (EWARM) toolchain V9.20.1, plus a patch available in the WBA firmware package (STM32Cube_FW_WBA_Vx.x.x/Utilities/PC_Software/EWARMv8_STM32WBAx_V1.2.zip)
  • RealView microcontroller development kit (MDK-ARM) toolchain V5.37, plus a patch available in the WBA firmware package (STM32Cube_FW_WBA_Vx.x.x/Utilities/PC_Software/Keil.STM32WBAx_DFP.1.0.0.zip)
  • STM32CubeIDE toolchain V1.12.0[2]

Required programmer version:

  • STM32CubeProgrammer[3], required to program the board with a previously generated binary file.

2.2. Hardware requirements

A Nucleo board[4], as illustrated in the figure below, is necessary to install the application.

Nucleo-WBA52CG board
Connectivity STM32WBA52 Board.png


3. Build and install the application

This section describes the build process using IAR Embedded Workbench® and STM32CubeIDE.

3.1. IAR IDE

Select the application that you want to build, open the dedicated IAR IDE (EWARM) directory, and launch Project.eww to open the demonstration project in the IDE.

IAR project directory
Connectivity WBA Zigbee IAR.png

Ensure that your project is correctly visible in the project explorer view.

Then either build your project or build it and program the board with it, as illustrated by the figures below.

IAR: build the application
Connectivity WBA Zigbee Build Project.png


IAR: build and program the application onto the board
Connectivity WBA Zigbee BuildProject.png

3.2. STM32CubeIDE

Select the application you want to build and open the dedicated STM32CubeIDE directory. Launch the STM32CubeIDE, and select the .project folder of the demonstration.

STM32CubeIDE project folder
Connectivity WBA Zigbee CubeIDE.png

Ensure that your project is correctly visible in the project explorer view.

Then build your project, as illustrated by the figure below.

STM32CubeIDE: build the application
Connectivity WBA Zigbee CubeIDE BUILD.png

After building, program the board with the application:

STM32CubeIDE: program the application onto the board
Connectivity WBA Zigbee Flash CubeIDE.png

3.3. Install the application from STM32CubeProgrammer

It is possible to program the previously built binary, whether with IAR Embedded Workbench® or STM32CubeIDE, by using the STM32CubeProgrammer software[3].

Select your device and connect to it:

STM32CubeProgrammer: platform connection
Connectivity WBA Zigbee CubeProgrammer.png

Once connected, the device information is displayed in the STM32CubeProgrammer interface. Click on the programming icon in the left column and select the project binary to program:

  • STM32Cube_FW_WBA_V[...]\Projects\[...]\Applications\Zigbee\Zigbee_OnOff_Server_Coord\[...]\Zigbee_OnOff_Server_Coord.bin

Set the start address to 0x08000000 and click on the Start programming button, as illustrated by the figure below.

STM32CubeProgrammer: programming the project
Connectivity WBA Zigbee CubeProgrammer steps.png

When programming is complete, STM32CubeProgrammer displays the following logs:

STM32CubeProgrammer: programming logs
Connectivity WBA CubeProg Log.png

4. References