STM32WBA Bluetooth® LE – Human Interface Device

Revision as of 16:05, 27 March 2024 by Registered User

1. Human Interface Device Over GATT Profile

Human Interface Device Over GATT Profile (HOGP) [1] is a Generic Attribute Profile (GATT) based low-energy profile defined by the Bluetooth® Special Interest Group[2]
This profile is an adaptation of the USB HID specification [3] to operate over a Bluetooth® low energy wireless link. This profile shall operate over an LE transport only.

This profile defines three roles:

  • The Human Interface Device (HID) shall be a GATT server.
  • The Boot Host shall be a GATT client.
  • The Report Host shall be a GATT client.

As Bluetooth® low energy devices are not supported in PC BIOS unfortunately, since at this point the Bluetooth® low energy stack and drivers are not yet loaded, the Boot Host role cannot be used with clients like PC, smartphone or tablet.


Bluetooth® LE HOGP: Report Host and HID Device
STM32WBA HOGP Profile


The Report Host supports the Scan Client role of the Scan Parameters Profile.

The HID Device has:

  • one or more instances of the HID Service,
  • one or more instances of the Battery Service,
  • a single instance of the Device Information Service,
  • optionally one instance of the Scan Parameters Service as part of Scan Server role of the Scan Parameters Profile,
  • optionally have single or multiple instances of other services.

This wiki page is the description of the HID Mouse project provided within the STM32CubeWBA MCU Package[4]

Bluetooth® LE HOGP Mouse Profile & STM32WBA
STM32WBA HID Mouse


The table below describes the structure of HOGP services:

Bluetooth® LE HOGP Profile specification
Service Characteristic Mode UUID size
HID Service 0x1812
Report Input: Read/Notify 0x2A4D 80
Report Output: Read/Write/Write Without Response 0x2A4D 80
Report Feature: Read/Write 0x2A4D 80
Report Map Read 0x2A4B 80
HID Information Read 0x2A4A 4
HID Control Point Write Without Response 0x2A4C 1
Device Information Service 0x180A
PnP ID Read 0x2A50 32
Battery Service 0x180F
Battery Level Read 0x2A19 1

The table below describes the HID Report characteristic descriptors:

Bluetooth® LE HID Report characteristic descriptors specification
Characteristic Name Descriptor Name UUID size
Report 0x2A4D
Client Characteristic Configuration Descriptor​ 0x2902 1
Report Reference Descriptor 0x2908 2

The table below describes the Battery Level characteristic descriptor:

Bluetooth® LE Battery Level characteristic descriptor specification
Characteristic Name Descriptor Name UUID size
Battery Level 0x2A19
Client Characteristic Configuration Descriptor​ 0x2902 1

HOGP Profile is a combination of a HID Device and a Report Host to connect and exchange data in different applications.

The GAP - Generic Access Profile defines and manages advertising and connection.

Report Host Central device and HID Peripheral device

STM32WBA55G-DK1 HOGP GAP


The GATT - Generic Attribute Profile defines and manages in/out data exchange.

Report Host GATT client device and HID GATT service device
STM32WBA55G-DK1 HOGP GATT


Examples of HID flow diagram between STM32WBA55G-DK1 & PC BLE or Smartphone BLE
STM32WBA55G-DK1 HID FLOW


1.1. STMicrolectronics Manufacturer Advertising Data

At start up, HID Device application starts Fast Advertising(80ms/100ms) including the STMicroelectronics Manufacturer Advertising Elements as described below:

HID Device STMicroelectronics Manufacturer Advertising data
0 1 2-3 4 5 6 7 8 9 10-15
Length Manufacturer ID Company BlueSTSDK Version Device ID Firmware ID Option 1 Option 2 Option 3 Device Address
HID Device 0x0F 0xFF 0x0030 STMicro 0x02 0x8B Nucleo-WBA 0x8B - HID Device 0x00 0x00 0x00 0x08E12Axxxx


Advertising is switched to Low Power advertising (1s/2.5s) after 60s

2. Requirements

2.1. Software and system requirements

The following list contains the required software as well as the required minimum IDE version:

  • IAR Embedded Workbench for ARM (EWARM) toolchain V9.20.1, plus a patch available in WBA Firmware Package: STM32Cube_FW_WBA_Vx.x.x/Utilities/PC_Software/EWARMv8_STM32WBAx_V1.3.zip
  • RealView Microcontroller Development Kit (MDK-ARM) toolchain V5.38, plus a patch available in WBA Firmware package: STM32Cube_FW_WBA_Vx.x.x/Utilities/PC_Software/Keil.STM32WBAx_DFP.1.3.0.zip
  • STM32CubeIDE toolchain V1.14.0[5].

The following programmer software is required to flash the board with an already generated binary:

  • STM32CubeProgrammer[6]

2.2. Hardware requirements

The board STM32 Discovery Kit-WBA55G-DK1 is required to install the application.

Hardware platform illustration
STM32WBA55G-DK1


2.3. Collector applications compatible

The STM32CubeWBA HID Device project is compatible with the following collectors:

3. STM32WBA55G-DK1 HID Device example description

3.1. Project directory

The "BLE_HID_Mouse" application is available by downloading the STM32CubeWBA MCU Package[7].

Refer to How to Build a Bluetooth® Low Energy project Wiki page for project directory information.

3.2. Project description

3.2.1. Structure

Below, a software project structure with the most important parts:

HID Mouse project structure
Connectivity WBA HID PROJECT.png
Connectivity yellow box.png
Main applicative part files
Connectivity dark blue box.png
Services management
Connectivity green box.png
Bluetooth® Low Energy libraries
Connectivity pink box.png
Link Layer System integration files

WARNING: Do not modify the files in Middleware folder


3.2.2. Application initialization

The different steps of the application initialization are described below:

HID Mouse project initialization
Connectivity WBA HID PROJECT INIT.png
puce1.png
  • Initialize the system (HAL, clocks, peripherals).
  • Infinite loop for run mode
puce2.png
  • Initialize the BSP, Power Mode, trace, memory manager, NVM.
  • Wait for initialization done
puce3.png
  • Initialize the Bluetooth® Low Energy Host Stack.
puce4.png
  • Initialize the Bluetooth® Low Energy GATT level.
  • Initialize the Bluetooth® Low Energy GAP level.
puce5.png
  • Reset the number of registered handlers.
puce6.png
  • Initialize the context.
  • Manage the HID Service notification.
puce7.png
  • Register Service Handler.
  • Update the services and characteristics.

3.2.3. GAP and GATT initialization and interaction

HID Mouse Device software module interaction
Connectivity WBA HID MODULE INTERACTION.png
puce3.png

and puce4.png The Bluetooth® Low Energy HID Mouse application initialization is done within app_ble.c

  • Initialize the Bluetooth® Low Energy stack - initialize the device as peripheral - configure and start advertising: ADV parameters, local name, UUID - APP_BLE_init().
  • Call the services controller initialization SVCCTL_Init() - svc_ctl.c.
  • Manage the GAP event - SVCCTL_App_Notification().
    • HCI_LE_CONNECTION_COMPLETE - provides information of the connection interval, slave latency, supervision timeout.
    • HCI_LE_CONNECTION_UPDATE_COMPLETE- provides the new information of the connection.
    • HCI_DISCONNECTION_COMPLETE - informs the application about the link disconnection and the reason.
puce5.png

The Services management is done by the service controller, svc_ctl.c

  • Initialize the number of registered handlers - SVCCTL_Init().
  • Manage events - SVCCTL_UserEvtRx()- from the Bluetooth® Low Energy Host Stack and redirect them to the gap event handler - SVCCTL_App_Notification.
puce6.png

The application level of the HID Mouse Device is done with hids_app.c:

  • Initialization of the services:
    • HID Service - HIDS_Init() - hids.c
  • Initialization of the context of the application
    • Report Map
    • HID Information - BASE USB HID SPEC VERSION
  • Receive notification from the HID Service - HIDS_Notification()
  • When Input Report characteristic is enabled by the remote, each update of the mouse position with the joystick (HIDS_APP_UpdateReport) is transfered to the remote device (collector) - HIDS_UpdateValue().
puce7.png

The HID Service hids.c manages the specification of the service:

  • Service Init - HIDS_Init()
    • Registers HID Event Handle to Service Controller - SVCCTL_RegisterSvcHandler(HIDS_EventHandler).
    • Initializes Service UUID – add HID service as Primary services.
      • Initializes Report Map characteristic.
      • Initializes HID Information characteristic.
  • Manages the GATT event from the Bluetooth® Low Energy Stack - HIDS_EventHandler().
    • ACI_GATT_WRITE_PERMIT_REQ_VSEVT_CODE
      • Reception of a Write Command: HID Control Point Characteristic Value
        • Sending of an aci_gatt_write_response() with an OK or KO status
        • Notification to the application to Suspend or Exit Suspend - HIDS_Notification(HIDS_HCP_WRITE_NO_RESP_EVT)
    • ACI_GATT_ATTRIBUTE_MODIFIED_VSEVT_CODE
      • Reception of an attribute modification - Input Report Characteristics Description Value : ENABLE or DISABLE Notification
        • Notify application of the Input Report Notification - HIDS_Notification(HIDS_NOTIFICATION_ENABLED/DISABLED)

3.2.4. Report Map and Input Report

HID Report Map characteristics should contain the USB HID descriptor specified in the USB HID specification [3].

An USB HID descriptor is a hard coded array of bytes describing the device’s data packets, including:

  • Number of packets supported,
  • Packets size,
  • Purpose of each byte and bit in the packet.

Example of USB Mouse HID descriptor for a 3 buttons Mouse with X, Y axis and a wheel:

USB Mouse HID descriptor
Connectivity WBA HID USB MOUSE DESCRIPTOR.png
3 buttons Mouse with X, Y axis and a wheel
Connectivity WBA HID 3-button mouse.png

All the hard coded bytes are described in the USB HID Usage Tables [8] document. This USB HID descriptor also defines the data structure sent in the associated Reports (Input, Output or Feature).

In this USB Mouse HID descriptor example, you can find:

  • Highlighted in green, the definition of 3 buttons represented by the 3 first bits of a byte that can have the boolean state 0 or 1.Bits 0, 1 and 2 represents the states of respectively the left, the middle and the right buttons of the mouse.The remained bits of the byte are unused.
  • Highlighted in blue, the definition of 3 bytes for the X, Y axes relative movement and wheel rotation. Each byte represents a signed integer that can take a value comprised between -127 to 127.

Example of the Input Report associated to USB Mouse HID descriptor:

3 buttons Mouse with X, Y axis and a wheel data structure
Connectivity WBA HID MOUSE INPUT REPORT.png

3.3. How to use the Bluetooth® Low Energy HID Mouse application

Once the Bluetooth® Low Energy HID Mouse application is installed on the STM32WBA55G-DK1 platform, launch a Bluetooth® Low Energy connection on a smartphone or a PC. Then, scan and connect the device called HIDS_XX (where XX is replaced by the last byte of the BD address) to the application.
As shown in the following screenshots for a ANDROID smartphone connection:

Android Bluetooth® Low Energy HID Mouse – How to
Connectivity WBA Smartphone Setting.png
Connectivity WBA Smartphone Device Connection.png
Connectivity WBA Smartphone Device Scanned.png
Connectivity WBA Smartphone Device Pairing.png
Connectivity WBA Smartphone Device Connected.png

Or for a PC connection:

PC Bluetooth® Low Energy HID Mouse – How to
Connectivity WBA HID PC SETTINGS.png
Connectivity WBA HID PC BLE DEVICES.png
PC Bluetooth® Low Energy HID Mouse – How to
Connectivity WBA HID PC ADD DEVICE.png
Connectivity WBA HID PC SCAN HID.png
PC Bluetooth® Low Energy HID Mouse – How to
Connectivity WBA HID PC CONNECT HID.png
PC HID CONNECTED
PC Bluetooth® Low Energy HID Mouse – How to
Connectivity WBA HID PC HID CONNECTED2.png

Once the Bluetooth® Low Energy connection is established and the notification enabled by the smartphone or the PC, HID Input Report is sent each time an action is performed on the STM32WBA55G-DK1 joystick .

STM32WBA55G-DK1 joystick
Connectivity WBA WBA55G-DK1 JOYSTICK.png
  • Action on Up, down, left and right direction sends an Input report containing a relative position.
  • Press on the joystick on neutral position sends an input report containing the state of the left button.

3.4. Low-power optimization

The project is delivered with the full system low-power disabled:

  • debug trace enabled
  • debugger enabled even in Low Power Mode

It is possible to enable/disable the low-power feature within app_conf.h.

/******************************************************************************
 * Low Power
 *
 *  When CFG_LPM_LEVEL is set to:
 *   - 0 : Low Power Mode is not activated, RUN mode will be used.
 *   - 1 : Low power active, the one selected with CFG_LPM_STDBY_SUPPORTED
 *   - 2 : In addition, force to disable modules to reach lowest power figures.
 *
 * When CFG_LPM_STDBY_SUPPORTED is set to:
 *   - 1 : Standby is used as low power mode.
 *   - 0 : Standby is not used, so stop mode 1 is used as low power mode.
 *
 ******************************************************************************/
#define CFG_LPM_LEVEL            (0)
#define CFG_LPM_STDBY_SUPPORTED  (0)

3.5. UART debug trace

Thanks to the debug log via UART interface , it is possible to trace the application project.

To enable the traces within the project, enable them within app_conf.h as described below:

/*****************************************************************************
 * Logs
 *
 * Applications must call LOG_INFO_APP for logs.
 * By default, CFG_LOG_INSERT_TIME_STAMP_INSIDE_THE_TRACE is set to 0.
 * As a result, there is no time stamp insertion inside the logs.
 *
 * For advanced log use cases, see the log_module.h file.
 * This file is customizable, you can create new verbose levels and log regions.
 *****************************************************************************/
/**
 * Enable or disable LOG over UART in the application.
 * Low power level(CFG_LPM_LEVEL) above 1 will disable LOG.
 * Standby low power mode(CFG_LPM_STDBY_SUPPORTED) will disable LOG.
 */
#define CFG_LOG_SUPPORTED           (1U)

/* Configure Log display settings */
#define CFG_LOG_INSERT_COLOR_INSIDE_THE_TRACE       (0U)
#define CFG_LOG_INSERT_TIME_STAMP_INSIDE_THE_TRACE  (0U)
#define CFG_LOG_INSERT_EOL_INSIDE_THE_TRACE         (0U)

/* macro ensuring retrocompatibility with old applications */
#define APP_DBG                     LOG_INFO_APP
#define APP_DBG_MSG                 LOG_INFO_APP

A debugger can also be supported by enabling it within app_conf.h as described below:

/******************************************************************************
 * Debugger
 *
 *  When CFG_DEBUGGER_LEVEL is set to:
 *   - 0 : No Debugger available, SWD/JTAG pins are disabled.
 *   - 1 : Debugger available in RUN mode only.
 *   - 2 : Debugger available in low power mode.
 *
 ******************************************************************************/
#define CFG_DEBUGGER_LEVEL           (2)
HID Mouse - Initialization phase Connected Phase
Start of CRC computation
End of CRC computation, value : 26349
Start of CRC computation
End of CRC computation, value : 26349==>> Start Ble_Hci_Gap_Gatt_Init function
  Success: aci_hal_write_config_data command - CONFIG_DATA_PUBADDR_OFFSET
  Public Bluetooth Address: 00:80:e1:2a:ff:36
  Success: aci_hal_write_config_data command - CONFIG_DATA_IR_OFFSET
  Success: aci_hal_write_config_data command - CONFIG_DATA_ER_OFFSET
  Success: aci_hal_set_tx_power_level command
  Success: aci_gatt_init command
  Success: aci_gap_init command
  Success: aci_gatt_update_char_value - Device Name
  Success: aci_gatt_update_char_value - Appearance
  Success: hci_le_set_default_phy command
  Success: aci_gap_set_io_capability command
  Success: aci_gap_set_authentication_requirement command
  Success: aci_gap_configure_whitelist command
==>> End Ble_Hci_Gap_Gatt_Init function

Services and Characteristics creation
  Success: aci_gatt_add_service command: HIDS
  Success: aci_gatt_add_char command   : INPUTREP
  Success: aci_gatt_add_char_desc command   : INPUT REP REF DESC on handle 0x10
  Success: aci_gatt_add_char command   : REM
  Success: aci_gatt_add_char command   : HII
  Success: aci_gatt_add_char command   : HCP
  Success: aci_gatt_update_char_value REM command
  Success: aci_gatt_update_char_value HII command
  Success: aci_gatt_add_service command: DIS
  Success: aci_gatt_add_char command   : PNI
  Success: aci_gatt_update_char_value PNI command
  Success: aci_gatt_add_service command: BAS
  Success: aci_gatt_add_char command   : BAL
  Success: aci_gatt_update_char_value BAL command
End of Services and Characteristics creation

==>> aci_gap_set_discoverable - Success
==>> Success: Start Advertising
>>== HCI_LE_CONNECTION_COMPLETE_SUBEVT_CODE - Connection handle: 0x0001
     - Connection established with @:65:92:b8:52:36:4b
     - Connection Interval:   45.00 ms
     - Connection latency:    0
     - Supervision Timeout:   5000 ms
>>== ACI_GAP_NUMERIC_COMPARISON_VALUE_VSEVT_CODE
     - numeric_value = 447414
     - Hex_value = 6d3b6
==>> aci_gap_numeric_comparison_value_confirm_yesno : Success

SNVMA_Write - Impacted NVM : 1
SNVMA_Write - Pending buffer : 1
FM_Write - Returned value : 0
SNVMA_Write - Flash operation started (Header write request) : 16
SNVMA_Write - Impacted NVM : 1
SNVMA_Write - Pending buffer : 1
SNVMA_Write - Impacted NVM : 1
SNVMA_Write - Pending buffer : 1
FM_BackgroundProcess - Case FM_BKGND_NOWINDOW_FLASHOP
FM_BackgroundProcess - Case FM_BKGND_NOWINDOW_FLASHOP - Write operation
FM_BackgroundProcess - Flash operation not complete yet, request a new time window
FM_WindowAllowed_Callback
>>== ACI_GAP_PAIRING_COMPLETE_VSEVT_CODE
     - Pairing Success


FM_BackgroundProcess - Case FM_BKGND_WINDOWED_FLASHOP
FM_BackgroundProcess - Case FM_BKGND_WINDOWED_FLASHOP - Time window granted
FM_BackgroundProcess - Case FM_BKGND_WINDOWED_FLASHOP - Write operation
SNVMA_FlashManagerCallback - Flash operation state : SNVMA_HEADER_WRITE
FM_Write - Returned value : 0
FM_BackgroundProcess - Case FM_BKGND_NOWINDOW_FLASHOP
FM_BackgroundProcess - Case FM_BKGND_NOWINDOW_FLASHOP - Write operation
FM_BackgroundProcess - Flash operation not complete yet, request a new time window
FM_WindowAllowed_Callback
FM_BackgroundProcess - Case FM_BKGND_WINDOWED_FLASHOP
FM_BackgroundProcess - Case FM_BKGND_WINDOWED_FLASHOP - Time window granted
FM_BackgroundProcess - Case FM_BKGND_WINDOWED_FLASHOP - Write operation
FM_BackgroundProcess - Flash operation not complete yet, request a new time window
FM_WindowAllowed_Callback
FM_BackgroundProcess - Case FM_BKGND_WINDOWED_FLASHOP
FM_BackgroundProcess - Case FM_BKGND_WINDOWED_FLASHOP - Time window granted
FM_BackgroundProcess - Case FM_BKGND_WINDOWED_FLASHOP - Write operation
FM_BackgroundProcess - Flash operation not complete yet, request a new time window
FM_WindowAllowed_Callback
FM_BackgroundProcess - Case FM_BKGND_WINDOWED_FLASHOP
FM_BackgroundProcess - Case FM_BKGND_WINDOWED_FLASHOP - Time window granted
FM_BackgroundProcess - Case FM_BKGND_WINDOWED_FLASHOP - Write operation
FM_BackgroundProcess - Flash operation not complete yet, request a new time window
FM_WindowAllowed_Callback
FM_BackgroundProcess - Case FM_BKGND_WINDOWED_FLASHOP
FM_BackgroundProcess - Case FM_BKGND_WINDOWED_FLASHOP - Time window granted
FM_BackgroundProcess - Case FM_BKGND_WINDOWED_FLASHOP - Write operation
FM_BackgroundProcess - Flash operation not complete yet, request a new time window
FM_WindowAllowed_Callback
FM_BackgroundProcess - Case FM_BKGND_WINDOWED_FLASHOP
FM_BackgroundProcess - Case FM_BKGND_WINDOWED_FLASHOP - Time window granted
FM_BackgroundProcess - Case FM_BKGND_WINDOWED_FLASHOP - Write operation
FM_BackgroundProcess - Flash operation not complete yet, request a new time window
FM_WindowAllowed_Callback
FM_BackgroundProcess - Case FM_BKGND_WINDOWED_FLASHOP
FM_BackgroundProcess - Case FM_BKGND_WINDOWED_FLASHOP - Time window granted
FM_BackgroundProcess - Case FM_BKGND_WINDOWED_FLASHOP - Write operation
FM_BackgroundProcess - Flash operation not complete yet, request a new time window
FM_WindowAllowed_Callback
FM_BackgroundProcess - Case FM_BKGND_WINDOWED_FLASHOP
FM_BackgroundProcess - Case FM_BKGND_WINDOWED_FLASHOP - Time window granted
FM_BackgroundProcess - Case FM_BKGND_WINDOWED_FLASHOP - Write operation
FM_BackgroundProcess - Flash operation not complete yet, request a new time window
FM_WindowAllowed_Callback
FM_BackgroundProcess - Case FM_BKGND_WINDOWED_FLASHOP
FM_BackgroundProcess - Case FM_BKGND_WINDOWED_FLASHOP - Time window granted
FM_BackgroundProcess - Case FM_BKGND_WINDOWED_FLASHOP - Write operation
SNVMA_FlashManagerCallback - Flash operation state : SNVMA_BUFFER_WRITE
Start of CRC computation
End of CRC computation, value : 48382
FM_Erase - Returned value : 0
FM_BackgroundProcess - Case FM_BKGND_NOWINDOW_FLASHOP
FM_BackgroundProcess - Case FM_BKGND_NOWINDOW_FLASHOP - Erase operation
FM_BackgroundProcess - Flash operation not complete yet, request a new time window
FM_WindowAllowed_Callback
FM_BackgroundProcess - Case FM_BKGND_WINDOWED_FLASHOP
FM_BackgroundProcess - Case FM_BKGND_WINDOWED_FLASHOP - Time window granted
FM_BackgroundProcess - Case FM_BKGND_WINDOWED_FLASHOP - Erase operation
SNVMA_FlashManagerCallback - Flash operation state : SNVMA_RETRY_WRITE
FM_Write - Returned value : 0
FM_BackgroundProcess - Case FM_BKGND_NOWINDOW_FLASHOP
FM_BackgroundProcess - Case FM_BKGND_NOWINDOW_FLASHOP - Write operation
FM_BackgroundProcess - Flash operation not complete yet, request a new time window
>>== HCI_LE_CONNECTION_UPDATE_COMPLETE_SUBEVT_CODE
     - Connection Interval:   7.50 ms
     - Connection latency:    0
     - Supervision Timeout:   5000 ms
>>== HCI_LE_CONNECTION_UPDATE_COMPLETE_SUBEVT_CODE
     - Connection Interval:   45.00 ms
     - Connection latency:    0
     - Supervision Timeout:   5000 ms
HIDS_REP_NOTIFY_ENABLED_EVT

4. References