1. Introduction
To check in this pre-version: OEM secrets/OEM data -> shall we speak of OEM OBK? Check also TBU/TBD/images to be updated. Also specificity of H7RS: all loaded in RAM and then launch SFI without any interaction between host and RSSe.
Hereafter, STM32H7RS refers to STM32H7Rx/7Sx lines.
The STM32H7RS supports Secure Firmware Install thanks to a dedicated RSSe (Secure firmware extension).
STMicroelectronics provides the SFI solution to perform the preparation and installation flows.
2. SFI for STM32H7RS
The SFI procedure on the STM32H7RS is similar to the SFI procedure applied on other platforms. The main difference is that interaction between host and STM32H7RS is not possible during SFI.
Follow SFI Step-by-step on STM32 boards to run the SFI procedure on the STM32H7RS.
SFI on external flash (SFIx) is not supported on STM32H7RS.
2.1. Preparation flow
2.1.1. Overview
The purpose of this step is to:
- prepare the encrypted firmware image to install, called SFI image. It is composed of the OEM application and the additional components (OEM secrets and OEM option bytes).
- provision the OEM key within an HSM.
2.1.2. SFI image
2.1.2.1. Overview
Here is an overview of the SFI image creation flow.
2.1.2.2. SFI image generation
Once the OEM application has been developed, the OEM must prepare and test the SFI image to be installed during manufacturing.
For that purpose, the OEM must use the STM32 Trusted Package Creator tool. This allows to correctly generate the SFI image and test it before manufacturing.
The output of the STM32 Trusted Package Creator is the tested SFI image, ready to be installed during manufacturing.
2.1.2.3. Description of the SFI image inputs
The OEM must provide the following inputs, described below:
- the OEM application: The OEM must provide its application binary.
- the OEM secrets: The OEM secrets are the OEM data and the OEM keys. The OEM secrets are described in detail in the TBD.
During the SFI procedure, the OEM must set its secrets, paying specific attention to the following:
- TBU: OBK provisioning: DA first with dbg_auth config then IROT OBK provisioning (optional)
- Option Bytes: The OEM must set carefully the STM32H7RS Product state.
The STM32H7RS Flash Memory configuration to install via the SFI procedure must be the same than the one used during the OEM application development.
2.1.2.4. SFI image output description
The Trusted Package Creator encrypts the SFI image inputs with the OEM key, and generates the SFI image.
The SFI image is then an encrypted image containing the OEM application, the OEM secrets and the OEM option bytes.
2.1.3. OEM key provisioning
The OEM must provide its OEM key to the Contract Manufacturer (CM) in a way the OEM key cannot be read or extracted clearly by the CM. Only STM32 can handle the OEM key.
In SFI for STM32H7RS, to provide the OEM key to the CM:
- The OEM provisions its OEM key, using the Trusted Package Creator, in one HSM.
Then:
- Only the STMicroelectronics STM32 microcontrollers can securely install the SFI image.
- Authenticity, integrity, and confidentiality of the SFI image content is ensured.
When using the HSM, the number of STM32 chips to program can be counted.
2.2. Installation flow
The installation procedure is similar to the generic SFI installation procedure, deployed on other STM32 products supporting SFI.
3. References