How to start with certificate linked to SOC class and ID on STM32H5

Revision as of 19:58, 8 February 2024 by Registered User

How to start with certificate linked to SOC class and ID on STM32H5


Target description

The generation of a root certificate and a certificate chain and how to use it to open the debugger through a debug authentication are explained in the two following articles:

The purpose of this article is to explain how to generate a certificate and a certificate chain valid only for one specific MCU product and for one specific sample.


Introduction

It is advised to read the following article: Debug Authentication STM32H5 How to Introduction.
Read the chapter about the root certificate and the certificate chain included in one of the "How to start" mentioned previously.


Prerequisites

  • Hardware
    • STM32H573 discovery board: the STM32H573 devices have all the available security features, including the HW crypto accelerator. (Note that for the STM32H56x devices, the HW crypto is not available)
    • Discovery MB1677- STM32H573 (need USBC cable)


  • Required tools
    • STM32Cube_FW_H5_V1.0.0 or later
    • STM32CubeProgrammer_rev2.13.0 or more recent (with trusted package creator (TPC) selected at installation).
    • IAR Embedded Workbench® rev 9.20.1 or later.
    • Tera Term / Putty or equivalent terminal emulator.
Info white.png Information
The TPC installed together with CubeProgrammer in the bin folder located in default STM32CubeProgrammer path : C:\Program Files\STMicroelectronics\STM32Cube\STM32CubeProgrammer\bin You can pin this tool to the taskbar to simplify the "STiRoT Getting started" process :
Security PinToTask.png


  • STM32Cube Firmware
    • Download the STM32CubeFW_H5 Cube firmware (Place it as close as possible to the C: root, to avoid long windows path)
    • A directory STM32H573I-DK is included in the “Projects” directory
    • If the STM32CubeProgrammer has not been installed in the default folder:C:\Program Files\STMicroelectronics\STM32Cube\STM32CubeProgrammer, the customized installation path needs to be updated in the environment variable: env.bat
    • Check that the selected application path is correct: for the following tutorial the STiRoT fully secured example is described => The STiROT_Appli must be active.


  • Check that the selected application path is correct, as shown in the figure below: for the following tutorial, the STiRoT fully secured example is described => The STiROT_Appli must be active.


Literature


Step by step instructions

  • The different stages to configure and use the STiRoT are based on a script provided in the STM32CubeFW (provisioning.bat)
  • The following documentation is a guide through all the steps of this script, and explains how to perform each of them.


No categories assignedEdit