1. Literature
2. Target description
The purpose of this article is to explain step by step how to use the STM32CubeFW example provided by ST, for OEMiRoT, using the Nucleo-STM32U083RC board.
- How to use the script provided by ST and perform all the required steps.
- How to install and run the user application example which is provided.
- How to perform a regression to retrieve an empty board with initial settings.
Based on this STM32CubeFW example, additional exercises are proposed
- To perform a firmware upgrade using the bootloader
3. Introduction
- Start by reading the zzzzzz article.
- For more details and to get an overview on OEMiRoT, read the zzzzzzzz articles.
One example of OEMiRoT is provided in the STM32Cube_FW that is used in this "getting started".
Through this practical example you will learn:
- What OEMiRoT is and how to use the STM32CubeFW example which is provided.
- How to configure the OEMiRoT and the debug authentication for this example.
- What is the iLoader and its role.
- How to generate an encrypted and signed image for the user application firmware and user data.
- What the device provisioning is and how to perform the setup of the device.
- How the user application and user data are installed.
- How to perform a debug authentication and reopen the debugger.
- How to read the installed user application firmware using the STM32CubeProgrammer
- How to attach an IDE on a running target and execute step by step, the secure user application
- How to perform a regression to retrieve an empty board
- The principle of certificate chain.
4. Prerequisites
- Hardware
- STM32U083 Nucleo board: the STM32U083 devices have all the available security features, including the HW crypto accelerator (the HW cryptographic acceleration is not supported for STM32U07x devices).
- USB-C cable
- STM32U083 Nucleo board: the STM32U083 devices have all the available security features, including the HW crypto accelerator (the HW cryptographic acceleration is not supported for STM32U07x devices).
- Required tools
- STM32Cube_FW_U0_V1.0.0 or later
- STM32CubeProgrammer_rev2.16.0 or more recent.
- IAR Embedded Workbench® rev 9.20.1 or later.
- Tera Term / Putty or equivalent terminal emulator.
- STM32Cube Firmware
- Download the STM32Cube_FW_U0 Cube firmware (advise is to place it close form the C: in order to avoid long paths)
- A directory NUCLEO-U083RC is included in "STM32Cube_FW_U0_V1.x.x\Projects"
- Open the env.bat file in ROT_Provisioning sub-folder
- 1- If the STM32CubeProgrammer has not been installed in the default folder:
- 1- If the STM32CubeProgrammer has not been installed in the default folder:
C:\Program Files\STMicroelectronics\STM32Cube\STM32CubeProgrammer, the customized installation path needs to be updated.
- 2- Check that the OEMiRoT_Appli path is OK
5. Example with PASSWORD configuration
This chapter explains how to start with the provisioning script.
It is used to configure the OEMiRoT and the debug authentication.
5.1. Preliminary stage
- The different steps to configure and use the OEMiRoT are based on a script provided in the STM32CubeFW:
Projects\STM32H7S78-DK\ROT_Provisioning\OEMiROT\provisioning.bat
- The following documentation is a guide through all the steps of this script, and explains how to perform each of them.
- The figure below shows where the script is located in the STM32CubeFW.
- Launch the script: provisioning.bat (double click) and keep it running during all the following steps.
- Type the product state: CLOSED (don't use LOCKED for this tutorial, this state is used only to set a final product state)
- Type the chosen Debug Authentication: PASSWORD (for explanation about certificate and password refer to intro article)
- Launch the script: provisioning.bat (double click) and keep it running during all the following steps.
5.2. OEMiRoT configuration
The next step indicated by the script is to open the OEMiROT_Config.xml file, update to the wanted configuration and to generate the OBk file.
- Open STM32TrustedPackageCreator.
- Select the shield
- Select OBkey tab
- Select the OEMiRoT_Config.xml configuration file. All the default settings for this hands-on are already filled-in and it is not needed to regenerate the encryption and authentication keys. In case these keys are regenerated, the firmware image needs to be regenerated (in case this image is already available)
- Generate OBkey
- The confirmation window is displayed
- According to the path specified in the OEMiROT_Config.xml, an OEMiROT_Config.obk file is generated in Projects\STM32H7S78-DK\ROT_Provisioning\OEMiROT\Binary folder. This file will be used by the script during the provisioning step.
5.3. Debug Authentication configuration
The Debug Authentication (DA) configuration is the next step of the script.
- Using STM32TrustedPackageCreator
- Select the shield
- Select OBkey tab
- Select the DA_Config.xml configuration file. All the default settings for this hands-on are already filled-in .
- Generate OBkey
- A success message is displayed for the password file password.bin generation
- The confirmation window is displayed
- Warning: for a commercial product, it is important to define your own key. But for trials it is advised to use the default provided, to avoid blocked regression due to lost password.
- According to the path specified in the DA_Config.xml, a DA_Config.obk file is generated in Projects\STM32H7S78-DK\ROT_Provisioning\DA\Binary folder. This file will be used by the script during the provisioning step.
5.4. Image generation
Check that the STM32H7R IAR™ provided patch is correctly installed and check that your IAR Embedded Workbench™ version is recent enough.
Two code examples for IAR Embedded Workbench™ are provided:
- OEMiROT_Boot corresponds to the Secure Boot.
It performs authenticity and integrity checks of the project firmware and data images.
- OEMiROT_Appli is an example of application managed by OEMiROT
OEMiROT_Boot project configuration
The step 3 of the scripte is the generation of the OEMiROT_Boot and OEMiROT_Appli applications firmware images.
- Open the Project.eww located in the EWARM directory: Projects\STM32H7S78-DK\Applications\ROT\OEMiROT_Boot\EWARM
Number of code images and Data images is defined in
flash_layout.h file in the ./Projects\STM32H7S78-DK\Applications\ROT\OEMiROT_Boot\Inc folder.
This example is configured by default for one application image and no data image. You can check these default parameters in file flash_layout.h as shown in figure below :
OEMiROT_Boot project compilation
- Open Project -> Option -> General Options: The device and CPU core should be automatically recognized and you should see the following windows:
If the device is not recognized, check that the STM32H5 IAR™ provided patch is correctly installed, and check that your IAR Embedded Workbench™ version is recent enough.
- Perform: Project -> Rebuild all (don’t upload the code, only perform a compilation)
The following binary is created: Projects\STM32H7S78-DK\Applications\ROT\OEMiROT_Boot\Binary\OEMiROT_Boot.bin
OEMiROT_Appli project compilation
- Open the Project.eww located in the EWARM directory:
Projects\STM32H7S78-DK\Applications\ROT\OEMiROT_Appli\EWARM
- Open Project -> Option -> General Options
The device and CPU core should be automatically recognized.
- Perform: Project -> Rebuild all (don’t upload the code, only perform a compilation)
The following image is created: Projects\STM32H7S78-DK\Applications\ROT\OEMiROT_Appli\Binary\rot_app_enc_sign.hex Don’t close the EWARM project.
5.5. Board programming
In the next steps the script will automatically perform
- The provisioning of the Option Byte
- Flash the previously generated image in the downloads area
- Perform the needed reset to install the code
- Set the final state of the product
- If all the steps have been executed successfully, a confirmation is displayed as shown in the figure above.
5.6. OEMiRoT application execution
- Close the script
- Launch the Teraterm (or equivalent)
- File => New connection
- The COM port number should be the same as indicated by your Windows device manager and also written in the env.bat file (see Prerequisites chapter)
- Setup => Serial port -> update to 115200 (and see the figure below for other configurations) -> New Setting
- Press the reset button (black button of the discovery board)
- The OEMiRoT application is executed (figure below)
5.7. Full regression
- There are two ways to perform a regression
- Using the graphic interface of the STM32CubeProgrammer.
- Using the regression script provided in the STM32CubeFW
5.7.1. Full regression using the script provided in the STM32CubeFW
- Launch the script as shown in the figure below
- You need to specify if the Debug Authentication provisioning as been done with Certificate or Password.
- Type "Password" for this example
- The script is executed and indicate that the regression has been performed successfully.
5.7.2. Full regression using the graphic interface of the STM32CubeProgrammer
- Click
in STM32CubeProgrammer
- Select Debug Authentication.
- Click “Discover”
- The information window will be filled:
- Enter the file password.bin path and click Regression
6. Example with CERTIFICATE configuration
6.1. OEMiRoT and debug authentication configuration
This chapter explains how to start with the provisioning script. It is used to configure the OEMiRoT and the debug authentication (in this case a configuration using a certificate)
6.2. Preliminary stage
- The same provisioning script is used as for the example for a Debug Authentication configuration with Password.
- Script located at: STM32CubeFW: STM32H7S78-DK\ROT_Provisioning\STiROT\provisioning.bat
- The following documentation is a guide through all the steps of this script, and explains how to perform each of them.
- Launch the script: provisioning.bat (double click) and keep it running during all the following steps.
- Type the product state: CLOSED (don't use LOCKED for this tutorial, this state is used only to set a final product state)
- Type the chosen Debug Authentication: CERTIFICATE (for explanation about certificate and password refer to intro article)
6.3. OEMiRoT configuration
The next step indicated by the script is to open the OEMiROT_Config.xml file, update to the wanted configuration and to generate the OBk file.
- Open STM32TrustedPackageCreator.
- Select the shield
- Select OBkey tab
- Select the OEMiRoT_Config.xml configuration file. All the default settings for this hands-on are already filled-in and it is not needed to regenerate the encryption and authentication keys. In case these keys are regenerated, the firmware image needs to be regenerated (in case this image is already available)
- Generate OBkey
- The confirmation window is displayed
- According to the path specified in the OEMiROT_Config.xml, an OEMiROT_Config.obk file is generated in Projects\STM32H7S78-DK\ROT_Provisioning\OEMiROT\Binary folder. This file will be used by the script during the provisioning step.
6.4. Debug Authentication configuration
The Debug Authentication (DA) configuration is the next step of the script.
- Using STM32TrustedPackageCreator
- Select the shield
- Select OBkey tab
- Select the DA_Config.xml configuration file (file for the DA configuration with Certificate). All the default settings for this hands-on are already filled-in and a default Debug Authentication root key is provided.
- Generate OBkey
- The confirmation window is displayed
- Warning: for a commercial product, it is important to regenerate your own Debug Authentication root key. But for trials it is advised to use the default provided, to avoid blocked regression due to lost key.
- According to the path specified in the DA_Config.xml, a DA_Config.obk file is generated as shown in the figure below.
- This file will be used by the script during the provisioning step.
- According to the path specified in the DA_Config.xml, a DA_Config.obk file is generated as shown in the figure below.
6.5. Image generation
Check that the STM32H5 IAR™ provided patch is correctly installed and check that your IAR Embedded Workbench™ version is recent enough.
Two code examples for IAR Embedded Workbench™ are provided:
- OEMiROT_Boot corresponds to the Secure Boot.
It performs authenticity and integrity checks of the project firmware and data images.
- OEMiROT_Appli is an example of application managed by OEMiROT
OEMiROT_Boot project configuration
The step 3 of the scripte is the generation of the OEMiROT_Boot and OEMiROT_Appli applications firmware images.
- Open the Project.eww located in the EWARM directory: Projects\STM32H7S78-DK\Applications\ROT\OEMiROT_Boot\EWARM
Number of code images and Data images is defined in
flash_layout.h file in the ./Projects\STM32H7S78-DK\Applications\ROT\OEMiROT_Boot\Inc folder.
This example is configured by default for one application image and no data image. You can check these default parameters in file flash_layout.h as shown in figure below :
OEMiROT_Boot project compilation
- Open Project -> Option -> General Options: The device and CPU core should be automatically recognized and you should see the following windows:
If the device is not recognized, check that the STM32H5 IAR™ provided patch is correctly installed, and check that your IAR Embedded Workbench™ version is recent enough.
- Perform: Project -> Rebuild all (don’t upload the code, only perform a compilation)
The following binary is created: Projects\STM32H7S78-DK\Applications\ROT\OEMiROT_Boot\Binary\OEMiROT_Boot.bin
OEMiROT_Appli project compilation
- Open the Project.eww located in the EWARM directory:
Projects\STM32H7S78-DK\Applications\ROT\OEMiROT_Appli\EWARM
- Open Project -> Option -> General Options
The device and CPU core should be automatically recognized.
- Perform: Project -> Rebuild all (don’t upload the code, only perform a compilation)
The following image is created: Projects\STM32H7S78-DK\Applications\ROT\OEMiROT_Appli\Binary\rot_app_enc_sign.hex Don’t close the EWARM project.
6.6. Board programming
In the next steps the script will automatically perform
- The provisioning of the Option Byte
- Flash the previously generated image in the downloads area
- Perform the needed reset to install the code
- Set the final state of the product
- If all the steps have been executed successfully, a confirmation is displayed as shown in the figure above.
6.7. OEMiRoT application execution
- Close the script
- Launch the Teraterm (or equivalent)
- File => New connection
- The COM port number should be the same as indicated by your Windows device manager and also written in the env.bat file (see Prerequisites chapter)
- Setup => Serial port -> update to 115200 (and see the figure below for other configurations) -> New Setting
- Press the reset button (black button of the discovery board)
- The OEMiRoT application is executed (figure below)
6.8. Full regression
- There are two ways to perform a regression
- Using the graphic interface of the STM32CubeProgrammer.
- Using the regression script provided in the STM32CubeFW
6.8.1. Full regression using the script provided in the STM32CubeFW
- Launch the script as shown in the figure below
- You need to specify if the Debug Authentication provisioning as been done with Certificate or Password.
- Type "Password" for this example
- The script is executed and indicate that the regression has been performed successfully.
6.8.2. Full regression using the graphic interface of the STM32CubeProgrammer
- Click
in STM32CubeProgrammer
- Select Debug Authentication.
- Click “Discover”
- The information window will be filled:
- Enter the paths for the key and the certificate (example with a certificate chain will be shown later, in this example only a single certificate is used (ROOT)):
- Select Full regression
- Click Execute, and the following success Message is displayed: