How to start with OEMiSB on STM32U0

Revision as of 17:22, 17 January 2024 by Registered User

1. Using the example

To ease the example generation and loading, a script is provided in the STM32Cube package. The script called “provisioning” is available in \Projects\NUCLEO-U083RC\ROT_Provisioning\OEMiSB.
The script execution is following steps:

  1. Configuration management
  • RDP selection
    • 0: In this case the development mode is enabled
    • 1: Production mode is enabled, and debug is possible
    • 2: Production mode is enabled, and debug is not possible
  • Data size selection
  1. Image generation
  • Compilation of the application and generating binary file.
  • Editing boot header files automatically.
  • Computing application HASH and generating hash area binary.
  • Compilation of the boot.
  1. Provisioning
  • Remove old protections and initialize option bytes.
  • Perform mass erase.
  • Download application, boot and hash.
  • Hardening by enabling HDP and WRP.

The script is useful to automate hash generation, which would have to be manually imported into the binary on each build.

No categories assignedEdit