Matter certification process

Revision as of 11:22, 10 January 2024 by Registered User

1. Introduction

One of the key features of the Matter protocol is that its software code is open source, which means that anyone can develop devices that are compatible with it. However, in order to ensure that these devices are fully compliant with the Matter standard and support all of its security mechanisms, they must be certified by the Connectivity Standards Alliance (CSA).
The certification process involves testing and validation by a third-party testing lab to ensure that the device meets all the necessary hardware and software requirements for full compliance with the Matter standard. Only devices that have received official certification from the CSA are allowed to carry the Matter logo.

2. Matter certification types

CSA defines two types of certification:

  • Matter HW solution
    • Matter HW solution certification includes whole Matter SW and underlying Transport layer (Thread/BLE)
  • Matter SW component
    • Matter SW component certification only includes a subset of Matter HW solution and is only applicable to Software Components that run within the context of a Supported Operating Environment (SOE).
      SOE shall support, at minimum, all the mandatory requirements for a Matter Software Component.


Connectivity Matter Cerification.png

3. Transport Layer Certification

Matter protocol runs over various technologies such as Thread, Wi-Fi, or Ethernet. To obtain Matter certification, devices must be certified according to these technologies. STMicroelectronics provides a Matter over Thread end device. Matter over Thread requires BLE for Commissioning as per Matter standard. Matter SDK runs on top of a Thread/BLE Dynamic Concurrent mode protocol stack. To get Matter certification, underlying Transport Layer shall also be certified. This means that below certifications are required:

  • Thread with Thread Group (Thread certification process wiki page)
  • BLE (Bluetooth SIG)

4. Matter certification process

Whatever the type of Matter certification, the process is the following:

  1. Become a member of the CSA
  2. Select an Authorized Test Provider (ATL) and submit testing. The list of ATLs can be found on the CSA website.
  3. ATL delivers a final test report to the applicant and the CSA
  4. Submit certification application to the CSA
  5. CSA review application (Processing)
  6. CSA approves certification
    • Public visibility of certified products on CSA website
    • Matter certified logos
Matter certification process
Connectivity Matter certification Process.png

5. Test Harness for Matter Certification

As mentioned previously, the ATL will run the test harness for the specific candidate. Candidate also may conduct in-house testing to detect any possible issues that may arise during formal certification testing. This approach can be beneficial in terms of time and cost savings.
The list of tests requested by the CSA depends on the product to be certified. You can find all the necessary instructions and guidelines for CSA membership on their website.
To certify Matter Dimmable Light device, with SDK1.1, STMicroelectronics perform:

  • 75 tests for Core including OTA and device discovery tests
  • 56 tests for Clusters including On/Off, Level Control and Access Control clusters tests

6. Certification application documents for Matter

The four required documents for certification are:

  • Document of Conformity (DoC)
  • PICS (Protocol Implementation Conformance Statements), which is an XML file containing the mandatory and the optional functions supported by the product under certification. It can be generated using the CSA’s PICS Tool.
  • Network Transport Attestation, which is an attestation confirming that you have obtained certification for the transport platform being used for your Matter component. This attestation is required for technologies such as Bluetooth, Thread, and Wi-Fi. The network transport attestation is not necessary for Matter SW component certification.
  • Security Attestation, which provides detailed information about the security level of the Matter component.

7. Acronyms and definitions

Term Definition
ATL Authorized Test Lab
FTD Full Thread Device
MTD Minimum Thread Device
PICS Protocol Implementation Conformance Statements
SOE Supported Operating Environment



No categories assignedEdit