Matter certification process

Revision as of 12:43, 21 December 2023 by Registered User (→‎Acronyms and definitions)

1. Introduction

One of the key features of the Matter protocol is that its software code is open source, which means that anyone can develop devices that are compatible with it. However, in order to ensure that these devices are fully compliant with the Matter standard and support all of its security mechanisms, they must be certified by the Connectivity Standards Alliance (CSA).
The certification process involves testing and validation by a third-party testing lab to ensure that the device meets all the necessary hardware and software requirements for full compliance with the Matter standard. Only devices that have received official certification from the CSA are allowed to carry the Matter logo.

2. Matter certification types

CSA defines two types of certification:

  • Matter HW solution
    • Matter HW solution certification includes whole Matter SW and underlying Transport layer (Thread/BLE)
    • That is the certification we are targeting with a dynamic concurrent mode BLE/Thread MTD
  • Matter SW component
    • Matter SW component certification only includes a subset of Matter HW solution and is only applicable to Software Components that run within the context of a Supported Operating Environment (SOE).
      SOE shall support, at minimum, all the mandatory requirements for a Matter Software Component.


Connectivity Matter Cerification.png

3. Matter certification process

Whatever the type of Matter certification, the process is the following:

  1. Become a member of the CSA
  2. Obtain a Vendor ID code from the CSA
  3. Similar to Zigbee and Thread certifications, Matter certification is preceded by an in-house testing phase. Each company that intent to get certification should test its product using the CSA provided Test Harness.
  4. Select an Authorized Test Provider (ATL) and submit testing. The list of ATLs can be found on the CSA website.
  5. ATL delivers a final test report to the applicant and the CSA
  6. Submit certification application to the CSA
  7. CSA review application (Processing)
  8. CSA approves certification
    • Public visibility of certified products on CSA website
    • Matter certified logos
Matter certification process
Connectivity Matter certification Process.png

Products with Thread, Wi-Fi, or Bluetooth need certification according to relevant standards. In our case, STMicroelectronics is in the process of certifying as a Matter Thread device solution, so we must certify:

  • Matter
  • Bluetooth by the Bluetooth SIG
  • Thread with Thread Group (Thread certification process wiki page)

4. Certification application documents for Matter

The four required documents for certification are:

  • Document of Conformity (DoC)
  • PICS (Protocol Implementation Conformance Statements), which is an XML file containing the mandatory and the optional functions supported by the product under certification. It can be generated using the CSA’s PICS Tool.
  • Network Transport Attestation, which is an attestation confirming that you have obtained certification for the transport platform being used for your Matter component. This attestation is required for technologies such as Bluetooth, Thread, and Wi-Fi. The network transport attestation is not necessary for Matter SW component certification.
  • Security Attestation, which provides detailed information about the security level of the Matter component.

5. Acronyms and definitions

Term Definition
ATL Authorized Test Lab
FTD Full Thread Device
MTD Minimum Thread Device
PICS Protocol Implementation Conformance Statements
SOE Supported Operating Environment



No categories assignedEdit