1. Introduction
This implementation can be seen as a base to implement home sensors that can be extend to thermostat or others.
Test and verify various functionality and ensure proper functioning.
2. Getting started
From the Wiki: Zigbee RUC Lighting network [1], this project adds new ZR and ZED for measurement sensors features.
2.1. Hardware requirements
P-NUCLEO-WB55 pack [2] with its USB Dongle are required to set up the demonstration.
For more information, please visit STM32WB Development ecosystem
P-NUCLEO-WB55 | USB Dongle |
---|---|
Additionally, its uses two different sensors integrated:
- The BME680 sensor, directly connected to the base station (Nucleo board [2] used as ZR), provides real-time data for temperature, pressure, and humidity by SPI control
- The SCD41 sensor, connected to the autonomous sensor (Nucleo USB-Dongle [2] used as ZED) by I2C control. For future upgrades, the sensor measurement could be programmed as SED with the Low-Power programming.
Finally, the data are displayed by the base station. For this purpose, an e-Paper display is used by SPI control.
Black and white e-paper with a size of 4.2 inches (300 x 400 pixels) from Pervasive Displays.
Total screen refresh time: approximately 2 seconds.
2.2. Software and system requirements
For more information to build Zigbee application, please visit STM32WB Build Zigbee Project
To check messages from the board, use any convenient terminal software via the UART Interface, please visit Wiki: Zigbee Log via UART
One driver is available for each sensor and display, these could be found with source example.
2.3. Install the Zigbee network
To install the RUC example, please follow the HowTo Join a Zigbee Network and HowTo bind devices.
3. Zigbee implementation
This example will use several Measurement clusters with the following topology:
- a base station as ZR with client clusters to collect data sensors
- three or more sensors device as ZED with multiple server clusters by device
Several clusters Measurement are mixed for sensors, like Temperature, Water content and concentration.
- Temperature Measurement cluster [3], is the basic cluster for the weather station.
- Water Content Measurement [4], which includes three subclusters. The one used in the application is the Relative Humidity Percentage.
- Concentration Measurement, a collection of 33 subclusters [5]. The one used in the application is the CO2 cluster.
3.1. Sensors
The ZED sensor is based on Nucleo USB Dongle [2].
Each ZED uses several Server Measurement clusters as Temperature and humidity to connect (bind) to the base station.
3.2. Base station
The base station is a ZR but also the client for all measurement clusters available.
4. Acronyms and definitions
Term | Definition |
---|---|
ZC | Zigbee Coordinator |
ZR | Zigbee Router |
ZED | Zigbee End Device |
SED | Sleepy End Device |
RUC | Realistic Use Case |
GPIO | General Purpose Input Output |
PWM | Pulse Width Modulation |