This message will disappear after all relevant tasks have been resolved.
Semantic MediaWiki
There are 1 incomplete or pending task to finish installation of Semantic MediaWiki. An administrator or user with sufficient rights can complete it. This should be done before adding new data to avoid inconsistencies.1. Introduction
This implementation can be seen as a base to implement home sensors that can be extend to thermostat or others.
Test and verify various functionality and ensure proper functioning.
2. Zigbee implementation
For this example, form the basic topology it
several clusters Measurement are mixed for sensors, like Temperature, Water content and concentration.
- Temperature Measurement cluster [1], is the basic cluster for the weather station.
- Water Content Measurement [2], which includes three subclusters. The one used in the application is the Relative Humidity Percentage.
- Concentration Measurement, a collection of 33 subclusters [3]. The one used in the application is the CO2 cluster.
Two different sensors are integrated to implement the weather station:
- The BME680 sensor, directly connected to the base station ZR (Nucleo board), providing real-time data for temperature, pressure, and humidity. SPI control
- The SCD41 sensor, connected to the ZED sensor (Nucleo USB-Dongle). Control by I2C. For future upgrades, it can be used as SED.
Additionally, the data needs to be displayed on a support, and for this purpose, an e-paper from Persuasive display with 4.2" inch size (300x400 pixel).
The ePaper offers two colors (black and white) and has total refresh screen time of approximately 2 seconds.
3. Acronyms and definitions
Term | Definition |
---|---|
ZC | Zigbee Coordinator |
ZR | Zigbee Router |
ZED | Zigbee End Device |
RUC | Realistic Use Case |
GPIO | General Purpose Input Output |
PWM | Pulse Width Modulation |